Classical Food, Alternative Proteins and Cultivated Meat: A Wide Product Range

Scale Up with Sartorius—From Research and Lab to Pilot and Manufacturing

Sartorius has a long and successful experience supporting the pharma and biotech industries. This has sharpened our expertise, fine-tuned our products and now puts us in prime position to support food tech and food production. Particularly in the area of novel foods like cultivated meats from animal slaughter-free stem cells including seafood, and new dairy where microorganisms and mammalian cells are key. As a supplier, we are a one-stop shop for this rapidly developing and highly competitive market. We are also leaders in protein purification in the baby food market.

Partnering a one-stop shop with ultra-high standards and deep regulatory knowledge puts you in prime position. With time to market and optimization both vital, Sartorius will get you there not only faster but also more cost-effectively:

  • Expertise in cultivation and purification technology required for microorganisms and mammalian cell cultures
  • Data analytics software to ensure fastest development and, later on, optimal processes and actionable insights
  • Complete range of crossflow technologies to separate and concentrate the protein of interest
  • Leader in protein purification

Contact Our Experts   Download Product Portfolio eBook

Cultivated Meat

The development of powerful cell culture media strategies has dramatically changed the way cultivated meat is produced. Sartorius is ideally placed to support your cell banking project by preserving the stem cells and enabling their repartition. Our proven instrumentation technology has been implemented in cell-culture labs and pilot plants. What’s more, our product portfolio covers upstream and downstream processes—from initial research all the way to full-scale manufacturing up to 2,000 L per bioreactor, and even more in parallel.

Other important highlights:

All with the support of a team of experts to help you define and design your ideal process.

Contact Our Experts

Simplify Your Cultivated Meat Process

Research Phase (15 mL to 250 mL)
Benchtop Development Phase (1 L to 10 L)
Pilot Phase (50 L to 200 L) Single-Use Technologies
Manufacturing (200 L)

Plant-Based Food and Mycoproteins

The market for tasty, healthy, and nutritious vegan food is a competitive one, especially when price and speed to market are also critical. To help customers face the challenge and address their plant-based and mycoprotein research needs, Sartorius delivers process characterization thanks to Ambr® 250 and Biostat® B & B-DCU. You also get the benefit of our wide experience in aseptic transfers that can safeguard your process and limit the risk of contamination.

Other important highlights:

All with the support of a team of experts to help you define and design your ideal process.

Contact Our Experts

Fermentation-Based Dairy

The challenge for many industries using fermentation of lactobacillus to provide new dairy alternatives is to be price competitive with regular animal-based dairy products. However, Sartorius can help you develop more efficient processes thanks to our deep knowledge and experience.

Other important highlights:

All with the support of a team of experts to help you define and design your process.

Contact Our Experts

Food Ingredients

When you supply classical ingredients like aromas, textures, colors, flavors, and yeast to the food industry, you want to be first on the market, develop the best products and set an attractive price.
Which, in turn, demands more efficient and cost-effective processes—as well as more sustainable solutions that are increasingly demanded.

Sartorius can help you develop the ideal process thanks to our deep knowledge and experience.

Other important highlights:

All with the support of a team of experts to help you define and design your process.

Contact Our Experts

Sartorius F&B @ LinkedIn

Join our community, get the latest Industy news and discuss with the experts.

Visit & Follow Us

Resources

User Guide

Classical Food, Alternative Proteins and Cultivated Meat - A Wide Product Range

PDF | 20.7 MB
User Guide

Venting Filters for Food and Beverage Applications

PDF | 6.9 MB
Brochure

Filtration Solutions - For Food and Beverage Applications Only

PDF | 936.7 KB

Food Quality Control: Tips and Tricks for Your Lab

There are a lot of steps that can optimize your food workflow process in your lab. Get to know these great tips and tricks today.

Download Poster
 


The implementation of a Design of Experiment (DOE) strategy will allow you to optimize the development of your final product (texture, taste, quality, and yield) and assure consistency and reproducibility while reducing time to market. Implementing data analytics software can help you answer the following questions: Can you meet cost and quality metrics? What will be the approximate cost of your finished product? How will your current recipe react to raw material variations? What variables will most affect your finished product?

Learn More

Ambr® 250 Modular is an innovative, easy-to-use, expandable benchtop system that incorporates 2 to 8 fully integrated single-use 100-250 mL mini bioreactors. It has a wide range of applications in process optimization and process characterization.

Learn More


Cell-cultured meat production requires scalable multi-use or single-use bioreactors for every stage of development, from clone selection and process development to pilot and full commercial production, including perfusion processing. Scalable, multi-parallel systems based on your needs help you quickly move from the early stages of clean meat discovery and development to mass production. In addition to high throughput systems and scalability, you need an easy-to-use platform that will automate much of the process to control oxygen levels, pH, temperature, in addition to advanced PAT such as Raman, cell capacitance, off-gas concentrations and higher-level recipe control.

Learn More

The Soxhlet method is a well-established procedure for extracting lipids from food samples. The method is relatively simple and can operate without constant supervision. It involves drying and grinding the food, then placing it in a special porous container called a thimble. The apparatus consists of three main parts: a flask, an extraction chamber, and a condenser. The process starts by heating the flask, which causes the solvent to evaporate and rise to the condenser. Here, it cools down and drips into the extraction chamber, where it permeates the sample in the extraction thimble, dissolving the lipids. These lipids are then carried back into the flask. The cycle repeats for 6 to 24 hours, depending on the sample and the extent of extraction required.

The Soxhlet method necessitates three distinct weight measurements: the initial weight of the sample, the weight of the empty flask, and the weight of the flask after the extraction is complete. These measurements are crucial for determining the mass of lipids extracted from the sample.

The Cellulose thimbles are more appropriate for the use in fast and reliable analytics in the field of food control and environmental monitoring. Commonly nuts & seeds, animal or plant butters, animal feeds, flour products, chocolate. In contrast to the glass fiber thimbles they will be typically used for fluid extraction. Glass fiber is recommended for filtration and the determination of dust and aerosols from air and gas streams. Their strength lies in:

  • Extraction with solvents incompatible with cellulose fibers
  • Extraction or particle retention at temperatures up to 500°C and in highly acidic media
  • Gravimetric determination of dust particles or aerosols from hot air and gas streams.
  • Extraction for specific biochemical analyses.

Shop Thimbles Now

It is important that the outer diameter (=inner diameter + 2x wall thickness) of the thimble fits into the extractor with a suitable pitch.

For example, an extractor with an NS 45/40 pitch (the 2nd number (40) is the inner diameter of the extractor) matches a slightly smaller inner diameter of the thimble, in this case 35mm ID.

And the length of the tube should be a little higher (0.5 - 1 cm) than the overflow siphon on the main body of the extractor, but lower than the bypass that goes into the main body above the siphon.

Download Datasheet

Related Blog Articles

Applied Industries
Jun 19, 2024 | 7 min read

Plant-Based Foods: Time to Put Yourself in Prime Position

With the global economy adding new challenges to the plant-based foods and animal-free protein industry, Sartorius is here to help with solutions and support

Applied Industries
Oct 05, 2023 | 10 min read

Cultivated Meat: Are We at the Tipping Point?

Cultivated meat is here to stay – and only going to get bigger. Find out about the latest important steps forward, the challenges that remain, and how Sartorius can help you address them. 

Applied Industries
Aug 23, 2023 | 7 min read

Is Precision Fermentation the Future of Food?

Precision fermentation is a game-changer in developing animal-free foods and alternative proteins. But to deliver on its potential, we first need to address the current challenges limiting its use

Applied Industries
Jan 31, 2023 | 4 min read

Get the Support You Need to Develop a New Food Product

The market for new food products is incredibly competitive. And any gains during R&D and manufacture can be decisive—not least being quick to market. You need support and technology you can trust.

Applied Industries
Sep 07, 2022 | 10 min read

Why Adoption of Single-Use Technologies Makes Sense in the Food & Beverage Industry

Single-use equipment for food and beverage production solves common issues and offers important benefits. Read our new article.

Applied Industries
Jan 24, 2022 | 5 min read

The Critical Role of Data Analytics & Design of Experiment (DOE) in Alternative Meat & Dairy...

For manufacturers of plant-based proteins and cultured meat and dairy products, this is a critical time in product development and manufacturing. Companies that can create delicious-tasting meat and d...

Applied Industries
Sep 28, 2021 | 8 min read

Reducing Time-to-Market Challenges for Alternative Meat & Dairy Products

Plant-based and alternative meat and dairy consumption has risen dramatically in the last several years throughout the world. 

Applied Industries
Jul 29, 2021 | 4 min read

Why Venting Filter Size Matters in Food & Beverage Production

Any scientist can tell you that microbes are abundant in the air we breathe every day. They are in the air inside your home, outdoors, and in your workplace. Some of these microbes are harmless, but o...

Consult Our Experts

Consult Our Experts

Related Topics

Bioreactors and Fermenters from 100 mL up to 2,000 L.

Bioreactors & Fermenters

Sartorius offers a complete scalable bioreactor platform from cell and strain line development to commercial manufacturing.

Fluid Management

With over 20 years of experience in manufacturing single-use solutions, we are your best partner for running your future manufacturing facilities.

Choose Sartoclear® for Depth Filtration That Delivers

Unlock efficient harvest clarification with Sartoclear® depth filters—engineered for superior clarity and reliable performance.

Sartoflow® Advanced: A Modular Benchtop TFF System

Flexible TFF from process development and clinical trials to small-batch cGMP production.

Microcarriers

Six types of SoloHill® animal protein-coated and animal componentfree microcarriers are available to support adherent cell culture growth.