Antibody Drug Conjugates (ADCs)

Antibody Drug Conjugates (ADCs) are a transformative class of next generation biopharmaceuticals that are redefining the landscape of cancer treatment and other difficult to treat indications. ADCs represent a synergistic combination of the targeting capabilities of monoclonal antibodies with the cell-killing power of cytotoxic drugs, the payload. Researchers are currently developing novel design of ADCs to further improve their efficacy and reduce off tumor toxicities.

The latest generation of ADCs show promising therapeutic outcomes and have led to the rapid growth of this precision immunotherapeutic class. New advancements in conjugation and linker technologies are at the forefront of next-generation ADC development, broadening the scope of oncology with targeted drugs for difficult-to-treat cancers like solid tumors, ovarian, pancreatic, glioblastoma, prostate cancer and beyond.

  • Faster, smarter ADC lead selection
  • Comprehensive ADC profiling
  • Linking binding data to functional activity
     

Request Information

Current development challenges include:

  • Complexity: The complex makeup and combination of Mechanism of Action (MoA) of ADCs require orthogonal in vitro characterization and cell-based assays with high accuracy and precision
  • Linker Stability: Developing chemically stable linkers that are cleavable within target cells is essential to ensure the selective release of the cytotoxic payload
  • Cytotoxic Payload: The potency and tolerability of the cytotoxic drugs used in ADCs must be optimized to improve the therapeutic index and reduce side effects.

Sartorius is addressing these challenges with innovative analytical techniques, cell-based assays, and 3D advanced cell models that streamline the research and development of ADC candidates:

  • Critical quality attributes (CQAs) with combined platforms
  • In-depth analysis of ADC activity and specificity
  • Insightful assessment of different mechanism of action (MoA)

ADCs Mechanism of Action

Researchers aim to create powerful workflows for ADC characterization that can uncover differences in binding and functional Mechanism of Action (MoA), which can inform and enhance antibody discovery processes. The MoA for most FDA-approved and pre-/clinical ADC drug candidates typically follows these steps:

Targeting: The ADC circulates in the bloodstream until it encounters a cancer cell with the appropriate antigen on its surface. The antibody component of the ADC binds to the antigen.

Internalization: After binding to the antigen, the ADC-antigen complex is internalized by the cancer cell through a process called receptor-mediated endocytosis.

Release of Payload: Inside the cell, the linker is cleaved, often in response to the acidic environment of the lysosomes or by specific enzymes, releasing the cytotoxic drug.

Cell Death: The released drug then interferes with a critical cellular process, such as DNA replication or protein synthesis, leading to the death of the cancer cell.

ADC R&D Workflow

Take a closer look at how Sartorius' research instruments and equipment alongside single-use solutions and services support both research & development and production scale. Achieve robust, efficient, and flexible operations that bring compliant ADCs to market faster.

   

Featured Products for Antibody Drug Conjugates (ADCs)

iQue® High-Throughput Screening (HTS) Cytometry Platform

The iQue® HTS Cytometry Platform is a high-throughput, suspension cell and bead analysis platform for multiplexed analysis of cell phenotype and function in a single well allowing for streamlined workflow and highly informed date sets. The iQue® 21 CFR Part 11 Software Module ensures easy transitions from research lab towards regulated laboratories.

Comprehensive functional profiling: Antibody-Dependent Cellular Cytotoxicity (ADCC) studies including quantification of critical Natural Killer (NK) cell activation markers

  • Complement-Dependent Cytotoxicity (CDC) assay
  • Live-cell antibody binding potency assay
  • ADC cytotoxicity, quantification of cell death
  • Quantification of cytokines involved in NK killing mechanism
  • High-throughput analysis of bystander activity

Explore High-Throughput Screening (HTS) by Cytometry Read Application Note

Octet® Label-Free Protein Analysis Platforms

Octet® Biolayer Interferometry (BLI) and Surface Plasmon Resonance (SPR) platforms measure protein-protein interactions in parallel, without the use of detection agents. These robust approaches enable fast, real-time characterization of binding and activity of ADC to target receptors, even in complex and unpurified samples. 

  • Rapid analysis of ADCs binding to target antigens, i.e. HER2
  • In-depth characterization of kinetic analysis of target and FcγR binding
  • Direct quantitation of cytokines

View The Data

 Explore BLI Explore SPR


Incucyte® Live-Cell Analysis System

The Incucyte® Live-Cell Analysis System is designed to efficiently capture cellular changes where they happen - in the incubator. It enables in-depth functional and phenotypic assessment of several cell types and cellular interactions such us immune cell activation, cell health and proliferation.

Incucyte® 21 CFR Part 11 Software Module offers comprehensive security and electronic record keeping functionality.

  • ADC internalization
  • Target cell killing
  • Cell proliferation, health, apoptosis,
  • Cell cycle analysis
  • ADC cytotoxicity and ADCC /ADCP activity assays - also in spheroid models
  • Bystander killing - also in spheroid models

Build a comprehensive in vitro functional and phenotyping profile of ADCs candidates with combined live-cell and biolayer interferometry platform.

Explore Live Cell Imaging & Analysis

Learn more about evaluating ADCs in vitro using 3D tumor spheroid models

Get in touch

CellCelector CLD Platform

The CellCelector CLD Platform is a fully automated cell imaging and picking system developed for high-throughput screening, selection and isolation of single cells, clones, clusters and adherent colonies specifically in cell line development workflows. The CellCelector CLD uniquely combines a powerful high-content imaging system with a fully automated cell-picking platform. It can process hundreds of thousands of cells in parallel to identify and select optimal clones that secrete high levels of the desired antibody, typically within 8 hours.

Simplifying Antibody Discovery with Automation:

  • Single Cell Cloning for CLD
  • High-throughput secretion screening and recovery of producer cells
  • Automated CHO and other production clone picking
     

Learn More

Lab Filtration and Purification

Fast and easy macromolecule purification for your R&D projects, using process-ready Sartobind® membranes.

Sartobind Protein A Lab

Rapid affinity purification for IgGs and mAbs, with a process-ready protein A membrane.

Sartobind IEX Lab

Rapid, economical IEX for parallel screening and small-scale contaminant removal after affinity chromatography.

  • Out-of-the-Box Flexibility Connect directly to a syringe, pump or FPLC system with no need to order expensive adapters separately – everything you need is already included.
  • High Yields in Seconds Rapid transport of even the largest molecules to the functionalized surface through convective flow, reduce cycle times and maximize productivity.
  • Process-Ready Technology Based on the industry-leading Sartobind® platform to eliminate uncertainty and minimize optimization requirements when transitioning to production.

Learn More



Sartorius Antibody Drug Conjugates (ADCs) Solutions Offer:

Enhanced Traceability

Incucyte®, iQue®, and Octet® BLI instruments all include 21 CFR Part 11 Software Module enable electronic record keeping and traceability, user management as well as electronic signatures. This supports the easy transition of assay from the R&D phase towards clinical pipelines and commercial manufacturing.

Optimized Workflows for Complementary Results

Combination of optimized workflows allow for data generation across multiple platforms with ease, facilitating broader profiling of many different ADC characteristics. For example, in addition to ADCC activity, the iQue® also quantifies other critical activation markers and cytokines (CD25, CD69, IFNγ. and Granzyme B), which, when combined with Octet® binding affinity data, can provide researchers with useful biophysical and functional information during ADCs development.

Improving Productivity

Enjoy walk-away convenience as images are automatically acquired and analyzed. Multiplex measurements in 96- and 384-well assay formats.

Upgrade Your Technology Today With Flexible Leasing Options

Take advantage of our leasing options to ensure financial flexibility, predictable costs, and the freedom to upgrade as your needs evolve.

Explore Leasing Options

Biologics Discovery and Development Resources

View All Resources
Antibody Drug Conjugates (ADCs) 3D Illustration
eBook

Creating Confidence in Antibody Drug Conjugates (ADCs) Characterizatio...

A Combined and Orthogonal Analytics Approach to ADCs Using Ligand Binding and Live-Cell Analysis

The Path from Traditional Monoclonal Antibodies to Next-Generation Constructs
eBook

The Path from Traditional mAbs to Next-Generation Constructs

Explore next-generation therapies such as ADCs and bsAbs for oncology

Webinar

Characterizing Anti-HER2 Antibodies with Cytometry & BLI Label-Fre...

High-throughput analysis of live-cell antibody binding, competitive binding, and Fc function

An antibody drug conjugate is pictured in purple with a cytotoxic payload
Application Note

Characterizing Trastuzumab ADCs with Biolayer Interferometry and High-...

This app note demonstrates the characterization of the drug trastuzumab to the trastuzumab-containing reference medicinal products (RMPs) Kadcyla® and...

Monoclonal antibody illustration in black and yellow for sartorius
Webinar

From Molecule to Market: Simplifying the Characterization of ADCs

Simplifying the Characterization of the drug trastuzumab to Kadcyla® and Enhertu®

Frequently Asked Questions

ADCs are targeted cancer therapies that combine the specificity of monoclonal antibodies with the potency of cytotoxic drugs. They are designed to selectively deliver these potent agents to cancer cells, thereby minimizing the systemic toxicity associated with traditional chemotherapy.

An ADC consists of three main components:

Antibody: The antibody is selected for its ability to bind specifically to an antigen that is expressed on the surface of cancer cells. The antigen should ideally be unique to cancer cells or at least be significantly overexpressed on them compared to normal cells. This ensures that the ADC targets and binds to the cancer cells with high specificity.

Cytotoxic Drug (Payload): The drug attached to the antibody is typically a highly potent cytotoxic agent that can kill cancer cells. These drugs are often too toxic to be used alone, but when delivered directly to cancer cells by the antibody, they can be used effectively at lower, less toxic doses.

Linker: The linker is a chemical or peptide bond that connects the cytotoxic drug to the antibody. It is designed to be stable in the bloodstream to prevent premature release of the drug, which could cause toxicity to healthy tissues. However, once the ADC is internalized by the cancer cell, the linker is cleaved by cellular processes, releasing the cytotoxic drug to exert its cell-killing effects.

ADCs are indeed considered biologics. Biologics are a category of drugs that are derived from living organisms or contain components of living organisms. ADCs are complex molecules composed of an antibody linked to a biologically active drug or cytotoxic compound. The antibody part of the ADC is a protein that is produced using biotechnological methods in living cells, which classifies it as a biological product.

The U.S. Food and Drug Administration (FDA) regulates ADCs under the Center for Drug Evaluation and Research (CDER) as biologics, and they are subject to the regulatory pathways that apply to biological products, including the Biologics License Application (BLA) process.

ADCs combine the targeting capabilities of monoclonal antibodies (which are a type of biologic) with the cancer-killing ability of cytotoxic drugs, allowing for more precise targeting of cancer cells while minimizing the impact on healthy cells. This makes them a powerful tool in the treatment of certain types of cancer.

ADCs are complex pharmaceuticals designed to deliver cytotoxic drugs specifically to targeted cancer cells. The production of ADCs involves several key steps:

Antibody Production:

The process begins with the generation of monoclonal antibodies (mAbs) that are specific to antigens expressed on the surface of cancer cells. These antibodies are produced by immune cells that have been cloned from a single parent cell, ensuring specificity and uniformity.

The production of mAbs typically involves the use of mammalian cell culture systems, such as Chinese hamster ovary (CHO) cells, which are engineered to produce the desired antibody.

Cytotoxic Drug and Linker Synthesis:

The cytotoxic drug, also known as the "payload," is a potent agent that can kill cancer cells. It is usually too toxic to be administered alone.

A linker molecule is chemically synthesized to connect the cytotoxic drug to the antibody. The linker must be stable in the bloodstream to prevent premature release of the drug but should release the drug once inside the targeted cancer cell.

Conjugation:

The antibody is chemically conjugated to the cytotoxic drug via the linker. This step is critical and requires precise control to ensure that the correct number of drug molecules are attached to each antibody molecule. This ratio is known as the drug-to-antibody ratio (DAR).

Conjugation methods vary, but common approaches include the use of cysteine or lysine residues on the antibody to form a stable chemical bond with the linker.

Purification:

After conjugation, the ADC mixture contains species with different DARs, as well as unconjugated antibodies and free drugs. The mixture is purified to isolate the ADC with the desired DAR and to remove impurities.

Techniques such as hydrophobic interaction chromatography (HIC), size-exclusion chromatography (SEC), or affinity chromatography may be used for purification.

Quality Control and Characterization:

The final ADC product undergoes rigorous quality control testing to ensure its purity, stability, and biological activity. This includes tests for aggregation, free drug content, and the functionality of the antibody.

Characterization techniques such as flow cytometry, mass spectrometry, high-performance liquid chromatography (HPLC), and Enzyme-Linked Immunosorbent Assay (ELISA) may be used to analyze the ADC's properties.

Formulation and Packaging:

The purified ADC is formulated into a stable pharmaceutical preparation, which may involve the addition of stabilizers or excipients.

The final product is filled into vials or other suitable containers under aseptic conditions and is then packaged for distribution.

Yes, ADCs are considered a form of targeted therapy. They are designed to specifically target and kill cancer cells while sparing healthy cells, which is a hallmark of targeted cancer therapies. The monoclonal antibody component of an ADC selectively binds to antigens that are typically overexpressed on the surface of cancer cells, delivering the cytotoxic drug directly to the tumor. This targeted approach aims to improve the efficacy of the treatment and reduce the side effects associated with traditional chemotherapy.

ADCs have been developed to treat a variety of cancer types. The applicability of an ADC to a specific cancer depends on the presence of a targetable antigen that is expressed on the surface of the cancer cells. Some of the cancer types that ADCs have been approved for or are being investigated to treat include:

  • Breast Cancer: ADCs such as trastuzumab emtansine (Kadcyla) target HER2-positive breast cancer.
  • Lymphoma: Brentuximab vedotin (Adcetris) is used to treat Hodgkin lymphoma and systemic anaplastic large cell lymphoma.
  • Leukemia: Gemtuzumab ozogamicin (Mylotarg) targets CD33-positive acute myeloid leukemia (AML).
  • Bladder Cancer: Enfortumab vedotin (Padcev) is used for urothelial carcinoma, the most common type of bladder cancer.
  • Lung Cancer: There are ADCs in development for non-small cell lung cancer (NSCLC) targeting specific antigens.
  • Gastric Cancer: Trastuzumab deruxtecan (Enhertu) is used for HER2-positive gastric or gastroesophageal junction adenocarcinoma.
  • Multiple Myeloma: There are ADCs being investigated for multiple myeloma, targeting antigens such as BCMA (B-cell maturation antigen).

The development of ADCs is an active area of research, and many more ADCs are in clinical trials for a range of other cancers. The success of an ADC in treating a particular type of cancer depends on the identification of suitable antigens that are highly expressed on cancer cells and the ability to target those antigens with an antibody that can deliver a cytotoxic payload effectively.

Publications

A Novel Dual-Payload ADC for the Treatment of HER2+ Breast and Colorectal Cancer

“Moreover, in order to observe the cytotoxic effect of the ADC, cell images were captured using Incucyte® ZOOM Live-cell Analysis prior to the addition of any sample and  after a 72 hour observation as shown in Figures 4 and 5. The Incucyte® cytotox green dye from Sartorius was used in the study to monitor the cytotoxic effect of the dual antibody-drug conjugate on cancer cells. This product enables real-time visualization and quantification of cell toxicity by labeling dead or dying cells, which helps researchers assess the efficacy of the conjugate”

Source:
https://doi.org/10.3390/pharmaceutics15082020
Pharmaceutics 2023, 15, 2020

Cite: 
Mckertish, C.M.; Kayser, V. A Novel Dual-Payload ADC for the Treatment of HER2+ Breast and Colon Cancer. Pharmaceutics 2023, 15, 2020. https://doi.org/10.3390/pharmaceutics15082020

Preclinical Development of MGC018, a Duocarmycin-Based Antibody-Drug Conjugate Targeting B7-H3 for Solid Tumors

“In the "Bystander killing assay" section of the document, the Incucyte® NucLight Red Lentivirus from Sartorius was used to generate cells stably expressing a red fluorescent protein (Hs700T/B7-H3 KO/RFP). These cells were then used in an assay to test the ability of MGC018 to kill not only B7-H3-positive tumor cells but also neighboring B7-H3-negative tumor cells through the so-called "bystander effect". Cell viability was measured after 5 days using an Incucyte® Live-Cell Analysis System from Sartorius.”

Source:
doi: 10.1158/1535-7163.MCT-20-0116
2020 American Association for Cancer Research

Cite: 
Scribner JA, Brown JG, Son T, Chiechi M, Li P, Sharma S, Li H, De Costa A, Li Y, Chen Y, Easton A, Yee-Toy NC, Chen FZ, Gorlatov S, Barat B, Huang L, Wolff CR, Hooley J, Hotaling TE, Gaynutdinov T, Ciccarone V, Tamura J, Koenig S, Moore PA, Bonvini E, Loo D. Preclinical Development of MGC018, a Duocarmycin-based Antibody-drug Conjugate Targeting B7-H3 for Solid Cancer. Mol Cancer Ther. 2020 Nov;19(11):2235-2244. doi: 10.1158/1535-7163.MCT-20-0116. Epub 2020 Sep 23. PMID: 32967924.

Characterization of human anti-EpCAM antibodies for the development of an antibody-drug conjugate

In the "Cell staining" section of the document, the Incucyte® S3 Live Cell Analysis System from Sartorius was used. It was used to analyze the internalization of antibodies by scanning the stained plates.

Source:
https://doi.org/10.1038/s41598-023-31263-x
Scientifc Reports, 2023

Cite:
Satofuka, H., Wang, Y., Yamazaki, K. et al. Characterization of human anti-EpCAM antibodies for developing an antibody–drug conjugate. Sci Rep 13, 4225 (2023). https://doi.org/10.1038/s41598-023-31263-x

Fc Antigen-Binding Fragment-Drug Conjugates as a Novel Antibody-Based Format for Targeted Drug Delivery

“The Cell Imaging Reader, Incucyte® S3 was used to investigate the receptor-mediated cellular uptake of Fcabs. The reader was equipped with DAPI and RFP filter cubes and was used together with a BioSpa 8 automated incubator. Images were acquired every two hours over a 24-hour period in the brightfield and RFP channels. Shortly before the end of the 24-hour measurement, a Hoechst 33342 dye was added for additional DAPI nuclear staining. Images were processed using BioTek gen5 data analysis software to normalize the fluorescence intensity of the pHAb dye and calculate the intracellular accumulation rate.”

Source:
DOI:10.26083/tuprints-00020360
Hunter, Sebastian Michael (2022)

Antibody-Mimetic Drug Conjugate with Efficient Internalization Activity Using Anti-HER2 VHH and Duocarmycin

The following unit was used: Vivaspin Turbo 15 PES, 50,000 MWCO; Sartorius, Gottingen to increase the concentration of the refolded anti-HER2 VHH-Cupid protein. This is an important step in the process of protein purification and concentration to achieve the desired protein concentration for subsequent experiments.

Source:
https://doi.org/10.1016/j.pep.2023.106375
1046-5928/© 2023 The Authors

Cite:
Juri Sakata, Toshifumi Tatsumi, Akira Sugiyama, Akihiro Shimizu, Yuya Inagaki, Hiroto Katoh, Takefumi Yamashita, Kazuki Takahashi, Sho Aki, Yudai Kaneko, Takeshi Kawamura, Mai Miura, Masazumi Ishii, Tsuyoshi Osawa, Toshiya Tanaka, Shumpei Ishikawa, Masanobu Tsukagoshi, Michael Chansler, Tatsuhiko Kodama, Motomu Kanai, Hidetoshi Tokuyama, Kenzo Yamatsugu, Antibody-mimetic drug conjugate with efficient internalization activity using anti-HER2 VHH and duocarmycin, Protein Expression and Purification, Volume 214

Generation and Characterization of SORT1-Targeted Antibody-Drug Conjugates for the Treatment of SORT1-Positive Breast Tumors

In section "4.4. Affinity Measurement", an Octet® instrument from Sartorius was used to measure the affinity. The anti-human FC sensors from Sartorius were loaded with antibodies to analyze the binding properties. The instrument was used to determine the equilibrium dissociation constant (KD) and data analysis was performed using Sartorius Data Analysis 12.0 software.

Source:
https://www.mdpi.com/1422-0067/24/24/17631
Int. J. Mol. Sci. 2023, 24, 17631

Cite:
Zhuang, W.; Zhang, W.; Xie, L.; Wang, L.; Li, Y.; Wang, Z.; Zhang, A.; Qiu, H.; Feng, J.; Zhang, B.; et al. Generation and Characterization of SORT1-Targeted Antibody–Drug Conjugate for the Treatment of SORT1-Positive Breast Tumor. Int. J. Mol. Sci. 2023, 24, 17631.
https://doi.org/10.3390/ijms242417631

Site-Specific Antibody Conjugation Using Modified Bisected N-Glycans: Method Development and Potential for a Tunable Effector Function

The Biolayer Interferometry system used in the study is the Octet® RED96 system from Sartorius. It was used to measure the binding affinity of the antibodies and antibody-drug conjugates.

In the "EXPERIMENTAL PROCEDURES" section, the Incucyte® system from Sartorius was also used to monitor the internalization of test antibodies and antibody conjugates. It was used to read out the fluorescence every 30 minutes to monitor the internalization process of the antibodies/conjugates in HER2-expressing SKBR3 cells.

Source:
https://pubs.acs.org/doi/10.1021/acs.bioconjchem.3c00302
Bioconjugate Chem. 2023
 

Evaluation of the Physicochemical Properties of ADC and Their Influence on Pharmacokinetics in huFcRn Transgenic Mice

The Sartorius Octet® system was used to analyze and acquire data. It is a biophysical analytical instrument that is often used to study binding kinetics and affinities between molecules. In this context, it was probably used to evaluate the binding properties of the antibody-drug conjugates (ADCs), especially in terms of their interaction with the human neonatal Fc receptor, which is an important aspect for predicting the pharmacokinetics and therapeutic efficacy of the ADCs.

Source:
Doi: 10.26083/tuprints-00021848
Approved dissertation by Anna Kaempffe, M.Sc.
Darmstadt 2022

Request a Quote, Demo, or More Information

What other areas are you interested in? (select all that apply)

Request More Information

Innovations to Advance Key Biologics Research

Computer-generate image of therapeutic proteins floating

Monoclonal Antibodies Discovery & Development

Information-rich solutions for development of traditional monoclonal antibody therapeutics.

Line of clear capsules encasing biosimilars

Biosimilar Development

At the heart of all biosimilar development is a comprehensive comparability study. See how we can support your robust analytical data package.

Bispecific Antibody (bsAb) with receptor sites on two cell surfaces - CGI image

Bispecific Antibodies (BsAbs)

Advanced analytical techniques to ensure bsAbs are developed with the desired quality and specificity.

Abstract 3D Cell for Cell Line Development

Cell Line Development

A Perfect Fit, From Start to Finish: Cell line development with intelligent tools, services, and solutions for your unique needs.