icon-education

Chromatography Glossary

Do you have some gaps in your chromatography knowledge? Here, you’ll find simple definitions of key terms and additional resources covering everything you need to know.

A

affinity chromatography

Affinity chromatography is a mode of chromatography with an immobilized ligand that exhibits specific or highly selective binding recognition for a target. It is a powerful purification approach that can serve as part of a platform for the industrial manufacturing of biomolecules. Examples include immobilized protein A for mAbs and oligo dT matrices for mRNA.

Related Articles:
How do Molecular Attributes and Sample Properties Affect Chromatography?

Related Pages:
Affinity Chromatography

Downloads: 
Purification of His₆-Tagged Proteins - Metal Chelate Chromatography With Sartobind® Membrane Adsorbers

Extraction of mRNA From IVT Mixtures With CIMmultus® Oligo dT Column

Advanced therapy and medicinal products (ATMPs) are medicines based on genes, tissues, or cells. They offer groundbreaking new opportunities for the prevention or treatment of disease and injury. For example, they might contain genes that lead to a therapeutic, prophylactic, or diagnostic effect and work by inserting recombinant DNA into cells.

Related Pages:
Cell and Gene Therapy

B

Bind & elute is the most typical application mode of chromatography. Solutes, especially the target, bind to the chromatography matrix. Impurities are washed out by changing the composition of the mobile phase (eluent) to discourage their binding (desorption), and the target is recovered. Desorption (elution) can be with a linear gradient or a step-change in conditions.

Breakthrough is the point in a chromatography run where a target or impurity first appears in the effluent. Breakthrough often represents a limit beyond which a chromatography matrix volume or device size is unable to handle more incoming target or impurity (see also dynamic binding capacity).

C

Capture is a chromatography stage where the focus is on target binding. It is usually an early unit operation. Ideally, capture chromatography will achieve high levels of purity so that subsequent unit operations are only required for particular safety concerns or polishing (e.g., removing viruses, leakage contaminants, and trace HCPs).

Related Articles:
How do Molecular Attributes and Sample Properties Affect Chromatography?

A contaminant is an impurity arising from an unintended source. Contaminants might include ligand leakage from an affinity matrix, endotoxins from unwanted bacterial infection, viruses, or other materials introduced due to the bioburden.

Related Articles:
How do Molecular Attributes and Sample Properties Affect Chromatography?

Downloads: 
Robust Parvo Virus (MVM) Clearance on Sartobind® Membrane Adsorbers

Continuous chromatography describes any chromatography with continuous sample application and target recovery. It can consist of automated separation of a sample into target and impurities, or a multi-column arrangement (see also SMB). Continuous chromatography assures maximum use of the matrix, minimum use of eluents, and short operation time while retaining purification performance.

Related Pages:
Continuous Chromatography

Downloads: 
BioSMB Process System - Scale-up of Multi-Column Chromatography

In with the New: Embracing Multicolumn Chromatography

Protein A Resin Reduction Achieved With Process Transfer From Batch to BioSMB

Infographic: 5 Reasons to Switch to Multi-Column Chromatography

Convective chromatography descrives any type of chromatography in which the matrix contains large pores or channels instead of small micropores. Mass transport to the ligands takes place purely by convective flow, so separation of components is achieved without the need for diffusion into small pores. Capacity and resolution are generally unaffected by flow rate since there is no limitation due to diffusion.

Related Pages:
Monolithic Chromatography

Critical quality attributes (CQAs) are defined characteristics of the purification target that are demanded and monitored in the final product.

Related Articles:
How do Molecular Attributes and Sample Properties Affect Chromatography?

D

Dynamic binding capacity (DBC) describes the capacity of a chromatography matrix to bind a target or impurity under operating conditions (i.e., with a flowing mobile phase - eluent - containing the target/specific impurity with or without other impurities present). It is usually defined for a device of specified dimensions, eluent flow rate, and target|impurity composition. The results are expressed as mass (of target or impurity) per device unit/column volume at a % (typically 1% or 5%) of maximum effluent concentration of the target or impurity.

E

The effluent is the mobile phase (eluent) that leaves the chromatography column or device.

The eluent is the mobile phase that flows through a chromatography matrix. It is frequently used to describe the mobile phase at any stage in chromatography, whether entering, passing through, or leaving the matrix during sample application or desorption (elution).
 

Elution is the flow of eluent through a chromatography matrix. It is often used to describe the desorption phase when the target is recovered in bind & elute mode.

Exosomes are membrane-bound extracellular micro-vesicles (EVs) that are often produced in the endosomal compartment of eukaryotic cells. Exosomes can contain proteins, lipids, or nucleic acids.  They are currently being developed as potential therapeutics with the ability to elicit cellular responses in vitro and in vivo.
 

F

Flow-through is a mode of chromatography where the target flows through the matrix without binding, or with little retention, and impurities are bound (negative chromatography). This mode is especially useful when the target has a high concentration in the sample, and the impurities are present in relatively small amounts (scavenging).

Flow velocity is an expression of flow rate, typically expressed in a scalable unit such as centimeters per hour (cm/hr). It is most often calculated by dividing the volumetric flowrate by the column cross-sectional area.

Format refers to the chromatography device - whether it is a column (either pre-packed or self-packed), a monolithic matrix device, or a membrane cartridge. A wide range of materials is available, including empty glass, plastic, or stainless steel columns for packing beaded resins, columns that allow automatic packing, pre-packed columns of all sizes, radial flow devices, and membrane cartridges for small lab applications to large-scale production.

Related Pages:
Chromatography Consumables
 

H

Particularly important when the target sources are mammalian cells, host cell proteins (HCPs) refer to all protein impurities present in the initial feed. Commonly, assays are developed and employed to track the removal of these impurities without defining individual components.

Related Pages:
Anti-CHO HCP Detection Kit

Hydrophobic interaction chromatography (HIC) is a type of chromatography with a hydrophobic ligand and aqueous mobile phase. Binding of the target and/or impurities is achieved with a high salt concentration in the sample and initial mobile phase. Desorption from the matrix is achieved by decreasing the ionic strength and in some cases by additives that discourage hydrophobic interaction 

Related Articles:
How do Molecular Attributes and Sample Properties Affect Chromatography?

Related Pages:
Hydrophobic Interaction Chromatography (HIC)

Downloads: 
Comparison of HIC Monolithic Support for Sample Displacement Chromatography of pDNA

Single-Use Membrane Chromatography in ADC Production

High-performance liquid chromatography (HPLC) is a type of chromatography where high resolution is achieved through the use of very fine particles or beads (often <10 microns in diameter). HPLC is widely used with dedicated equipment that tolerates the high pressures and the use of organic solvents. It is generally avoided at large scales due to high costs for explosion-proof environments, high-pressure equipment, and organic solvents. Nevertheless, HPLC forms an essential step in purifying many organic molecules, peptides, and polypeptides (including insulin).

Downloads: 
Combining the Sensitivity of the PATfix® HPLC Platform With the Resolution of Ultracentrifugation for AAV Characterization

Using PATfix® Analytical HPLC Platform to Optimize Lysis Conditions in pDNA Downstream Processing

I

Ion exchange chromatography (IEX) is one of the most widely applied chromatography modes in which solutes are separated due to their different ionic properties. IEX can be used in both bind & elute and flow-through modes. Binding and elution are modulated by changes in mobile phase ionic strength, pH, or both. A wide range of matrices, including salt-tolerant, is available.

Related Articles:
How do Molecular Attributes and Sample Properties Affect Chromatography?

Related Pages:
Ion Exchange Chromatography (IEX) 

Downloads:
Endotoxin Removal - Ion Exchange Chromatography With Sartobind® Membrane Adsorbers

Isolation of DNA Fragments From Agarose Gels Using Sartobind D Ion Exchanger

Impurities are unwanted solutes or other materials that originate from the target source. For instance, impurities from bacterial fermentation, cell-culture supernatant, synthetic sample, or tissue extract.

Intermediate purification is a stage of chromatography between target capture and polishing. Typically, the selected chromatography mode is different from the mode used in capture and polishing. In an ideal scenario, an intermediate purification step would not be required.

L

Laminar flow is a smooth type of liquid flow in which the fluid behaves as a system of orderly parallel layers with no eddies or irregular regional fluctuations in velocity and pressure. Laminar flow is gentle for molecules that are sensitive to shear stress, such as mRNA. Monolithic chromatography matrixes that have regular-sized interconnected channels offer good laminar flow properties. Beaded resins or irregular particle resins tend to have irregular flow with eddies and turbulence.

A chromatography ligand describes any functional group attached to the matrix that helps to isolate a target or impurity. Commonly used ligands include amine groups, protein A, oligo dT, and enzyme substrates.

Related Articles:
How do Molecular Attributes and Sample Properties Affect Chromatography?

M

The backbone material used as the support for chromatography is called the matrix. The chromatography matrix typically consists of beaded resin particles packed in a column, layers of membranes arranged in a cartridge, or a monolithic structure of interlinked channels.

Mixed-mode chromatography (MMC) describes chromatography on a matrix that exhibits several binding mechanisms for targets and impurities. These include ion exchange, hydrophobic interaction, and hydrogen bonding. MMC is useful for difficult polishing applications or for salt-tolerant IEX. However, binding and elution conditions require extensive optimization.

Related Articles:
How do Molecular Attributes and Sample Properties Affect Chromatography?

Related Pages:
Mixed-Mode Chromatography

Downloads:
Method for High Throughput Screening of MEP, HEA, PPA, and CMM HyperCel Mixed-Mode Chromatography Resins Using 96-Well Plates  

Benefits of Mixed-Mode Cation Exchange Chromatography: CMM HyperCel Resin Used for Monoclonal Antibody and Other Recombinant Protein Purification

The liquid that flows through the chromatography matrix is called the mobile phase. Initially carrying the sample feed, the mobile phase is typically followed by washing out non-bound solutes. Then, the eluent conditions are changed to desorb bound solutes.

Modality is the term used to describe all types of purification targets. These include protein biomolecules, nucleic acids, vectors, viruses, vesicles, exosomes, and other ATMPs.

A chromatography mode is a group term that describes different separation mechanisms such as ion exchange, hydrophobic interaction, affinity, multi-modal, and reversed-phase chromatography. It is also used to describe flow-through and bind & elute techniques.

Related Articles:
How do Molecular Attributes and Sample Properties Affect Chromatography?

Monoclonal antibodies (mAbs) are important biopharmaceuticals, and are made by culturing a clonal population of white blood cells. mAbs are most often created by hybridoma technology (although other technologies exist) and can be purified by affinity chromatography using a protein A ligand.

Related Pages:
Monoclonal Antibodies

Downloads:
Benefits of Mixed-Mode Cation Exchange Chromatography: CMM HyperCel Resin Used for Monoclonal Antibody and Other Recombinant Protein Purification   

DNA Removal Using Sartobind® Q in mAb Purification - Ion Exchange Chromatography With Sartobind® Membrane Adsorbers

BioSMB for Increased Productivity at the mAb Capture Step

Monolith Purification Visual

Monoliths are chromatography devices with a layer of interconnected channels (different channel diameters are available). Mass transport occurs due to the convective flow of the mobile phase (eluent) through the channels. Devices are pre-packed and can be used as single-use or multi-use columns.

Related Pages:
Monolithic Chromatography

Downloads:
CIMmultus® Monolithic Columns - Pre-Packed Preparative Columns for Purification of Large Biomolecule  

CIMac™ Analytical Columns  

Chromatographic Separation of Full and Empty AAV8 Capsids

O

Oligo dT is a short fragment of single-stranded DNA consisting of thymine (T) bases. The sequence can bind the poly(A) tail present in mRNA molecules. Oligo dT is frequently used as the ligand in affinity purification of mRNA.

Related Articles:
How do Molecular Attributes and Sample Properties Affect Chromatography?

Related Pages:
Affinity Chromatography

Downloads:
Extraction of mRNA From IVT Mixtures With CIMmultus® Oligo dT Column

P

Polishing is a chromatography stage that typically removes small amounts of remaining impurities and contaminants following earlier purification steps that have removed the bulk of the impurities. Polishing chromatography demands a chromatography matrix with high efficiency and selectivity to achieve the required level of purity of the target product. It is usually the final chromatography unit operation and is often needed to assure safety and efficacy. 

Related Articles:
How do Molecular Attributes and Sample Properties Affect Chromatography?

Related Pages:
mAbs

Protein A was originally derived from the cell wall of the bacteria Staphylococcus aureus. Now frequently genetically engineered, Protein A is a widely used ligand in affinity chromatography for the purification of monoclonal antibodies (mAbs), as it exhibits highly specific binding to the Fc region of IgG.

R

In rapid cycling chromatography (RCC), a relatively small amount of media is used to perform many short cycles instead of a large amount of media employed to perform one or a few cycles. RCC offers significant productivity increases (10-15x) compared to traditional chromatography. 

Related Pages:
Rapid Cycling Chromatography

A resin is a solid, usually organic, polymeric structure (sometimes it refers to inorganic materials such as silica or hydroxyapatite) that forms the backbone of particulate and beaded chromatography matrixes. Such matrices are most commonly porous with a stationary liquid phase within pores. Mass transport (exchange) of substances from the mobile phase, which flows past resin particles to the pores, mainly occurs by diffusion.

Related Pages:
Chromatography Resins

Downloads:
Benefits of Mixed-Mode Cation Exchange Chromatography: CMM HyperCel Resin Used for Monoclonal Antibody and Other Recombinant Protein Purification

Efficient Contaminant (HCP, DNA) Removal Using MEP HyperCel Chromatography Resin for Monoclonal Antibody Purification

Reversed-phase chromatography (RPC) is a chromatography mode based on a hydrophobic stationary phase. The matrix often consists of alkyl chains covalently bonded to silica or might be a matrix with inherently hydrophobic properties, such as various plastic polymers. Solutes bind due to their hydrophobic or non-polar properties. They can be eluted according to differences in these properties using a gradient containing an organic solvent, such as acetonitrile or ethanol. RPC is most often used in the lab as HPLC to separate and analyze organic molecules or closely similar peptides. At large scales, it is used in the production of certain peptides and polypeptides (notably insulin), where it requires an explosion-proof environment and high-pressure stainless steel equipment.

Related Articles:
How do Molecular Attributes and Sample Properties Affect Chromatography?

S

Salt tolerant describes a form of mixed-mode ligand and - when attached to a matrix - chromatography, where the binding characteristics allow ion exchange at an elevated ionic strength. This is accomplished by mixed-mode ligands with both ion exchange and additional binding mechanisms that support and enhance the ionic binding of targets and/or impurities, despite elevated concentrations of salts in the sample and mobile phase.

Related Pages:
Ion Exchange Chromatography (IEX)

Downloads:
DNA Binding On Sartobind STIC® PA Compared to Sartobind® Q - Salt Tolerant Membrane Chromatography 

Membrane Chromatography Cassettes for Bind & Elute Applications of Viruses and Large Proteins

Size-exclusion (SEC) is a chromatography mode that separates molecules purely on their size. The components of a mixture do not bind to the stationary phase in SEC. Instead, they pass through the stationary phase at different rates depending on their size. 

Related Articles:
How do Molecular Attributes and Sample Properties Affect Chromatography?

Simulated moving bed (SMB) is a form of continuous chromatography that uses several columns (or other chromatographic devices) with valves on the inlet and outlet sides. The sample is applied continuously to the columns in sequence so that it appears that the bed is moving past the sample inlet. As with simpler arrangements of continuous chromatography, SMB reduces matrix and eluent consumption and can allow major cost and time savings compared with batch chromatography. However, it puts high demands on in-process control and valve performance.

The stationary phase describes stationary regions in a column or other device where partitioning of solutes occurs with the mobile phase. In beaded and particulate resins, the partitioning region is inside the liquid-containing micropores of the chromatography matrix. Mass transfer of solutes and exchange with fresh, incoming eluent occurs by diffusion from the mobile phase to the micropores, rather than convective flow. Solutes that have diffused into the micropores can then bind to groups attached to the stationary matrix. In monoliths and membrane matrixes,  solutes in the mobile phase have direct access to the stationary phase binding sites, and mass transfer is by convection.

T

The purification target is the molecule, particle, vesicle, virus, viral particle, or vector which requires purification. 

The target product profile (TPP) is a description of the product containing the defined target of the purification and other components. These might include its solvent environment or lack of specified, harmful impurities.

Turbulent flow is the fluid motion characterized by chaotic changes in pressure and flow velocity. This is in contrast to laminar flow, which occurs when a fluid flows smoothly with no disruption between parallel layers. Turbulent flow increases with flow rate, especially when the liquid has to follow irregular paths, for example, around resin beads. Turbulent flow can damage shear-sensitive purification targets such as mRNA and leads to zone broadening and loss of resolution.

More about Sartorius

Sartorius Single-Use Bioreactors and Single-Use Platform

Applications

Products

Services