Improve Your Chemical Manufacturing

Innovative Solutions for Efficient and Simplified Chemical Analysis

More of it, only the very best of it, and keep it eco-friendly.

When it comes to chemical and consumer care solutions, our motto is simple: More of it; only the very best of it; and keep it eco-friendly.

Efficient and economical solutions are paramount to lasting success in an evolving market driven by innovations and regulations. An effective process that meets all requirements must be designed carefully from beginning to end to increase productivity and quality while saving time. 

We are here to simplify chemical analysis and consumer care needs with easy-to-handle and quick-to-clean solutions that maintain the highest durability and resilience. Our flexible, modular and versatile products help drive innovation and adapt to new trends, technologies and regulations in your pursuit of sustainable chemistry – doing more with less. Whether in research, process development or quality control (QC), our innovation helps achieve stability, safety and efficacy every step of the way.

Let Sartorius provide the tools you need for maximized results in:

  • Cosmetics and Personal Care
  • Fine and Specialty Chemicals 
  • Bulk Chemicals

Consumers are becoming increasingly aware of products’ potential impact on the environment. So are we. As the responsibility grows to embrace industrial sustainability, we are working hard to provide clients and partners with future-proof, resource-saving technologies.

Applications we are happy to support you with:

  • Chemical Composition Analysis
  • Sample preparation for analytical testing
  • Microbiological testing for raw materials and finished goods
  • Data Analytics

Sustainability begins right on our doorstep, leading our team to act responsibly towards the future and the environment – for our employees, for our clients and for society. 

fine and specialty chemicals

Fine & Specialty Chemicals: Make Superior Performance

Flexible Solutions for Advanced Development and Testing of Fine Chemicals

bulk chemicals

Bulk Chemicals: Rough Enough to Be Up to the Task?

Durable Solutions for Safe and Sustainable Work With Bulk Chemicals

Contact an Expert

Featured Resources

Application Guide

Fundamental PreAnalytics for Compliant Flexibility

Lab essentials for tailored sample preparation

Analytical Samples, Standards & Calibration Curves
Application Guide

Analytical Samples and Standards

Collection of technical documentation to effectively limit interferences.

Enzymatic Degradation of Plastic: Recent Methods, Applications, and Solutions for the Recycling of Polymers
White Paper

Enzymatic Degradation of Plastic

Recent Methods, Applications, and Solutions for the Recycling of Polymers

Measurement Uncertainty During Weighing: Top 8 Contributors to Watch Out For
White Paper

Measurement Uncertainty During Weighing

Top 8 Contributors to Watch Out For - created together with Chemical & Engineering News

White Paper

Analytical Testing of Cosmetics

An overview of the most common active ingredients and harmful substances in cosmetics and summary of sample preparation.

Discover Sustainable Solutions

Sustainability is an integral part of our corporate strategy and one of our corporate values

To us, sustainability means operating responsibly over the long term –with respect to customers, employees, investors, business partners and society as a whole. Likewise, it entails handling natural resources responsibly.

Good health and well-being are at the core of our business.

icon-recycable-waste

Learn more about the corporate responsibility of Sartorius

See how Sartorius operates responsible over the long term - with respect to business partners, employees, society and natural resources

Explore More
icon-processcontrol_dataanalysis

Improve your Sustainability with Sartorius Data Analytics Software

Use the Umetrics® Suite to reduce cost and decrease emissions in heat and power generation

Explore More
View All Chemical & Consumer Care Resources

Chemical & Consumer Care Featured Products

Cubis III Family - product line perspective view - white

Cubis® III: Connect, Comply, Simplify

Direct integration and built-in compliance—no middleware, no hidden costs

SIMCA® Multivariate Data Analysis Software

Advanced data analytics solution able to keep full control over your processes from raw material to finished product

Frequently Asked Questions

Contact your Sartorius representative for further information on our products' chemical compatibility.

Explore Pipettes

The liquid attached to the outside of the tip is extra and not part of the set volume. To avoid picking up extra liquid on the outside of the tip, insert the pipette tip only 3-5 mm below liquid surface, or slightly deeper for very large volumes. Touch the tip on to the vessel wall after aspiration to remove excess liquid from outside the tip. Do not wipe the tip on a tissue cloth as it can contaminate the sample, or absorb liquid from inside the tip.

Explore Pipettes

If the pipette tip cone comes into contact with corrosive liquids, clean it with alcohol and a soft tissue. You can minimize the risk of corrosion by using Safetyspace™ Filter Tips that protect the pipette's tip cone and other internal parts. You can also protect the insides of the pipette by installing Safe-Cone plus filters into the tip cone.

Explore Pipette Tips

We recommend using pipettes with tips that are validated for fit and performance on those pipettes. For example, Sartorius pipettes are designed to be used with Sartorius pipette tips, which are a perfect fit together. While other manufacturer’s tips might be compatible, it is the user's responsibility to validate the pipette and tip combination for compatibility and performance. Check the ISO 8655 standard on how to determine pipette and tip combination performance. Also, be sure to calibrate your pipettes with the tips you plan to use.  

Explore Pipettes

The maintenance interval is affected by various factors, including pipetting frequency, liquids dispensed, and the age and model of the pipette. For example, more frequent maintenance is required if you dispense a lot of volatile liquids or solvents. At minimum, a maintenance interval of one year is suggested, with calibration done annually or more often, such as every 3 – 6 months. 

Explore Pipetttes

Industries that need a record of water quality data must select a system that has this capability. There are different options for saving water quality data. Depending on the system, it can either be saved electronically (via USB or SD-card) or printed as a hard copy. Using a printer ensures data cannot be manipulated or falsified.

Explore Water Purification

Regular check-ups help ensure high water quality and purity, as well as system and consumables quality. Customers can maintain their system to some degree. However, to avoid risk of losing high-quality water or damaging the system - and to reduce downtime and ensure error free operation - it is recommended that maintenance is done by qualified service technicians. Look into the service contract options with the manufacturer at the time of purchase. 

Explore Water Purification


There are different opinions on this topic. In theory, it's better not to use desiccant. Desiccants cause a difference between the internal and external balance environments. They reduce the humidity in the balance, which causes static electricity when weighing glassware. Thus, it gives inaccurate readings. Electronic balances are particularly susceptible to these effects for the low, 0.01mg accuracy readings. Presence of desiccant causes a slight air flow in the balance, which makes the balance unstable. 

Explore Laboratory Balances

The infrared moisture meter (or Moisture Analyzer) has applications in many industries. The infrared moisture meter is used in weighing of water, milk, dew, cream, powder, soap, oil, plastic, and more. the table we listed is the actual measurement: nail polish, nitro alkali solution, makeup remover, talcum powder / prickly heat powder, shaping spray, antibacterial soap, body milk, after shower gel, etc. According to your local regulations (if applicable), the moisture reference comes from a defined method in a related norm. Typically, the oven method is the reference, and the Moisture Analyzer needs a Homologation SOP.

Explore Moisture Analyzers

Our customers use the Sartolab® P20 Plus large-volume positive pressure filter. Since the filter volume is large, it is often used in the R&D phase. There are different membrane pore sizes to choose from, and we normally recommend a pore size of 0.2 µm. The benefit of the Sartolab® P20 Plus is the fast and efficient filtration. At least 5 liters of water sample can be filtered by combining with a peristaltic pump. Many of our customers also use Tangential Flow ultrafiltration membrane to pack a Vivaflow® cassette to concentrate hyaluronic acid and remove impurities.

Explore Pressure Filters

It depends on which process step the balance is used in, and how critical the step is. In the cosmetics industry, calibration is typically performed annually, unless there are deviations in the daily verification or when earlier calibration is recommended by a service technician. For internal/external calibration, we recommend using the Internal calibration program with a calibration weight to ensure adjustment by time and by temperature deviations.

Explore Instrument Services | Calibration

We supply balances that are resistant to solvents by using PBT housing and parts. We recommend using isopropyl alcohol for deep cleaning. Chlorine is not recommended because it can cause micro-corrosion.

Explore Laboratory Balances

You can perform research to find the typical moisture content values for the samples (if available) to get a rough idea of how much moisture they contain and then work backwards to determine an optimal sample size. Conversely, you can start with a very small sample size, knowing that the moisture content will be a percentage of the overall sample. Then, correlate the amount of moisture found with the measurement sensitivity of the moisture analyzer to make sure that you are within the effective measuring range of the instrument based on the sample size selected.

Explore Moisture Analyzers

Moisture analyzers can generally provide accurate and repeatable results within just a few minutes. These times can be optimized by adjusting measurement parameters, like sample size, temperature and other settings.

Explore Moisture Analyzers

It depends on a number of factors, including the sample size and the degree of fluctuation in the measuring environment. To determine the exact amount of potential fluctuation, you should experiment and compare results against measurements taken when complete acclimatization has taken place.

Explore Laboratory Balances

For microbiology testing, disposable devices are ideal as they reduce the risk of cross-contamination. The Microsart® filter is the best suited for microbiology testing, as long as the assay is chemically compatible with the plastic. The Microsart® filter can be used in conjunction with the Microsart® media or the Nutrient Pad sets depending on the assays requirements.

Shop Now

The fastest way to test lipid-based cosmetics is to emulsify the cosmetic to break up the lipids. This allows for filtration using the Microsart® filter. It is also helpful to pre-wet the membrane to minimize lipid binding and pass through.

Shop Now

This can be done using the Cubis® III density kits and proper accessories. The exact accessories will depend on the nature of the cream and how it behaves - liquid, solid or paste.

Explore Laboratory Balances

We recommend glass microfiber filters, which are depth filters. They can easily capture particles in the structure of the filter or on its surface. Therefore, they combine flow rates with high load capacity and retention of very fine particles. Glass microfiber filters without binders are biologically inert and are resistant to most chemicals.

Explore Glass Fibers

Yes, with a LIMS system you can capture data in any number of ways, but the exact options depend on your specific LIMS system. Most LIMS systems allow the user to document data in internal or external storage devices and databases, as well as networked printers.

Explore Laboratory Balances

Yes. However, precautions are needed in extremely dry environments as they increase the chances of static electricity, which can negatively influence the performance of your balance. Countermeasures against static include anti-stat mats, ionizers, and other devices. 

Explore Laboratory Balances

Regular verification and adjustment by using internal, external or automatic calibration ensures precision.

Explore Laboratory Balances

Weighing low sample quantities is common in analytical labs. In the area of chemical analysis, such as quantitative gravimetric analysis, thermogravimetry or elemental analysis, accuracy plays an essential role. During the weighing processes sample spillage may be difficult to detected due to the very small sample quantities. The Sartorius YSH48 Anti Spilling Weighing Pan has a reduced surface design to prevent spilled sample from landing on the weighing pan and affecting your weighing results. Any spilled substances land outside the weighing pan, ensuring reliable and highly accurate measurement.

Explore Application Highlight

Big data refers to extremely large or complex datasets that must be analyzed using advanced statistical methods and tools. These tools reveal patterns, trends, and associations, especially relating to processes, behavior, and interactions. Chemical manufacturers use advanced data analytics to compare and measure the effect of various production inputs, such as coolant pressure, temperature, or carbon dioxide flow on yield – often finding surprising and unexpected dependencies that impact output.

Learn How Manufacturers Are Using Big Data Analytics to Improve Processes

Data and analytics can have hugely beneficial effects in the chemical industry:

  • Select the right raw materials by predicting properties of compounds and reducing the number of experiments
  • Optimize production processes by visualizing data and providing guidance on process adjustments
  • Keep processes under control by enabling corrective actions to reduce scrap and increase yield

Explore Fine Specialty Chemicals

Request a Quote, Demo, or More Information

What other areas are you interested in? (select all that apply)

Request More Information

Explore Sartorius

icon-fermentation-bioreactors

Biopharmaceutical Manufacturing

Explore More
icon-scientist

Life Science Research

Explore More
icon-testing

Quality Control & Testing

Explore More