T cell releases antibodies, binding to virus

Protein-Protein Interactions (PPI)

Overview of Protein–Protein Interactions

Protein-Protein Interactions (PPIs) play a vital role in maintaining biological systems. Strong interactions ensure structural integrity and function, while weaker interactions provide flexibility, allowing cells to adapt to changing conditions. Understanding PPIs is fundamental to advancing research in cell biology and drug development.
 

Explore Biolayer Interferometry for PPIExplore Surface Plasmon Resonance for PPI

Protein-Protein Interaction Assays

The protein-protein interaction assays can be broadly classified into three main categories:

In Vitro - This method involves conducting the entire procedure outside the cell in a controlled laboratory environment. Techniques include affinity chromatography, protein fragment complementation, X-ray crystallography, NMR, phage display, spectroscopy, protein assays, and biomolecular interaction analysis.

In Vivo - These techniques are applied directly to living cells or organisms, allowing for the observation and analysis of biological processes in their natural context.

In Silico - These techniques are performed using computer simulations and computational models. They encompass sequence and structure-based approaches, in-silico two-hybrid approaches, gene expression-based methods, chromosome proximity and gene fusion techniques, phylogenetic profiling, or tree-building techniques.

 

Types of Protein-Protein Interactions

PPIs are classified based on factors such as stability, duration, and the types of proteins involved. 

Protein-protein interactions can be classified in several ways: 

Based on affinity, they can be classified as obligate (in case one or more of the proteins is unstable in vivo unless interacting and forming a specific protein complex) and non-obligate interactions (in case the proteins can exist independently).

Non-obligate interactions can be classified based on the stability of the complex they form, as permanent or transient, and transient interactions as weak or strong.

As most obligate interactions are permanent, and most non-obligate interactions are transient, obligate and permanent are sometimes used interchangeably in the literature.

The majority of cellular processes are regulated by transient PPI, and thus a large part of the research on PPI concentrates on this type of interaction.

Dynamic processes like signal transduction and metabolism rely on weaker, transient interactions regulated by conditions like phosphorylation or conformational changes. These weak interactions help assemble multi-enzyme complexes or shape cellular morphology and motility.

In contrast, strong PPIs lead to stable, multi-subunit complexes, with dissociation constants typically in the nanomolar range or lower. RNA polymerase is a well-studied complex with strong interactions between its multiple subunits. Another example is the interaction between the anti-apoptotic protein Bcl-2 and the pro-apoptotic protein Bax, which balances cell survival and death. Disruption of this balance is a key factor in cancer development.

 

Protein-Protein Interactions as Drug Targets

Many drugs target PPIs to either disrupt or enhance specific interactions, providing therapeutic benefits in diseases like cancer. Small molecules, peptides, and monoclonal antibodies (mAbs) are examples of interaction modulators developed through various screening and optimization techniques. 

For example, monoclonal antibodies targeting the PD-1/PD-L1 pathway have revolutionized cancer immunotherapy by blocking this immune checkpoint, boosting anti-tumor responses. Similarly, Nutlin-3 inhibits the interaction between MDM2 and p53, preventing p53 degradation and allowing its tumor-suppressive functions to operate. This small molecule is undergoing clinical testing and shows promise in cancer treatment.

 

Methods for Analyzing Protein-Protein Interactions

There are end-point and real-time methods for analyzing PPIs. End-point assays provide information about a single timepoint and are ideal for detecting an interaction. However, for capturing dynamic interactions and detailed kinetics, real-time methods provide the most complete picture of the PPI.

  • Affinity-based methods like co-immunoprecipitation (co-IP) and pull-down assays isolate proteins and their binding partners from complex mixtures like cell lysates. Enzyme-linked immunosorbent assay (ELISA) is a widely used labeled, end-point assay that measures steady-state binding affinities of purified proteins but cannot capture the dynamics of the interaction, i.e., the kinetics of how fast the interaction formed or dissociated provided by on- and off-rates.
  • Yeast two-hybrid is a genetic method that detects PPIs by activating a transcription factor when two proteins interact.
  • Real-time, label-free biophysical methods such as surface plasmon resonance (SPR), biolayer interferometry (BLI), and isothermal titration calorimetry (ITC) provide insights into binding rates and affinities, helping researchers understand interaction mechanisms and optimize therapeutic targeting. These methods are also label-free, which simplifies workflows and eliminates the risk of interference from labeling.

The choice of method depends on factors like target size, sample usage, and throughput requirements. It is also crucial to consider the interaction type, as weak or transient interactions may be lost in certain protocols. In some applications, an ELISA provides sufficient yes/no information about the interaction of interest. However, for a deeper understanding of dynamic interactions, label-free, real-time data is often needed.

Related Products

The Octet® BLI is an easy-to use, real-time analytical tool that rapidly screens critical quality attributes.

2-Channel System: Octet® R2

Grows with your biomolecule characterization needs

Octet R4 label free detection system

4-Channel System: Octet® R4

The perfect balance between cost and throughput with given leeway

Octet R8 label free detection system instrument

8-Channel System: Octet® R8

Unmatched flexibility and versatility in protein analysis

Octet RH16 ultra high throughput label free detection system

16-Channel High Throughput Octet System: Octet® RH16

Ideal for high-throughput applications that demand high sensitivity and low sample volume requirements

Octet® BLI rapidly determines recombinant protein concentration as a control parameter in cell line development.

96-Channel Ultra High Throughput Octet System: Octet® RH96

Monitors up to 96 biosensors simultaneously, enabling label-free detection for protein quantitation and kinetic characterization at unmatched speed

Octet N1 label free detection system

Personal Assay Octet® N1 System

Affordably priced label-free analysis for individual researchers on any budget

Octet® SF3 SPR

Octet® SF3 SPR 

Generate high-quality kinetics and affinity data in a fraction of the time compared to standard multi-cycle kinetics using the Octet® SF3.

Frequently Asked Questions

PPIs occur when two or more proteins physically interact, driving nearly all biological processes. Examples include enzyme-substrate interactions, receptor-ligand signaling cascades, cell cycle regulation, and structural assemblies like the cytoskeleton.

Yes, proteins interact with other proteins. These interactions are crucial for many biological processes, including signal transduction, cellular structure, and metabolic pathways.

Breaking protein-protein interactions can be achieved through several methods:

  • Small Molecules: Designing or using small molecules that can bind to one of the proteins and disrupt the interaction.
  • Peptides: Using peptides that mimic the interaction site to competitively inhibit the protein-protein interaction.
  • Mutagenesis: Altering amino acids at the interaction site through genetic engineering to prevent binding.
  • Antibodies: Antibodies that specifically bind to one of the proteins block the interaction.
  • Environmental Changes: Altering conditions such as pH, temperature, or ionic strength to destabilize the interaction. This is often used to regenerate biosensor to re-use them in binding assays.
  • Protein Degradation: Using techniques like targeted protein degradation to remove one of the interacting proteins.

These methods are often used in research and drug development to study protein functions and develop therapeutic interventions.

Testing for PPIs involves several steps and can be achieved using various techniques. 

First, choose the appropriate method based on the nature of the proteins, the type of interaction, and the information needed, such as binding affinity, kinetics, or structural details.

Next, prepare protein samples. If required, label the proteins with fluorescent or other suitable tags to facilitate detection, especially for techniques like FRET or MST.

After conducting the experiment depending on the chosen method, analyze the data. Finally, validate the results by confirming findings using complementary techniques or repeating experiments to ensure reliability and reproducibility.

Common techniques used to study protein-protein interactions (PPI) include:

  • Co-immunoprecipitation (Co-IP): A method to detect physical interactions between proteins using specific antibodies.
  • Yeast Two-Hybrid (Y2H) Screening: A genetic approach to identify protein interactions by detecting the activation of reporter genes in yeast.
  • Biolayer Interferometry (BLI): A label-free technique for measuring binding kinetics, affinity and analyte concentration in real-time without the need for microfluidics.
  • Surface Plasmon Resonance (SPR): Another label-free technique to measure binding kinetics and affinity in real-time.
  • X-ray Crystallography: Used to determine the 3D structure of protein complexes at atomic resolution.
  • Nuclear Magnetic Resonance (NMR) Spectroscopy: Provides information on the structure and dynamics of protein complexes in solution.
  • Fluorescence Resonance Energy Transfer (FRET): A technique to study interactions by measuring energy transfer between two fluorescently labeled proteins.
  • Mass Spectrometry (MS): Used to identify and quantify proteins in complexes, often combined with cross-linking or affinity purification.
  • Isothermal Titration Calorimetry (ITC): Measures the heat change during protein binding to determine interaction thermodynamics.
  • MicroScale Thermophoresis (MST): Measures the movement of molecules in temperature gradients to study binding affinities and kinetics.

Biolayer Interferometry (BLI) is a technique used to study protein-protein interactions. It measures binding events in real-time by detecting changes in the interference pattern of light reflected from a biosensor surface. One protein is immobilized on the sensor, and the other is in solution. BLI provides information on binding kinetics, affinity, and specificity without the need for labeling, making it a valuable tool for analyzing protein interactions. 

The BLI technology allows a fluidic-free design. Unlike other techniques that require complex microfluidic systems, BLI uses a simple dip-and-read format eliminating the risk of clogging and cross-contamination and simplifying the experimental setup.

Additionally, BLI is capable of measuring interactions in crude samples, such as cell lysates or unpurified protein mixtures. This capability is particularly beneficial for early-stage research and high-throughput screening.

For Biolayer Interferometry (BLI) experiments, the amount of protein required can vary depending on the specific assay and the proteins involved. BLI utilizes a plate-based format, which allows for non-destructive measurement. This means that the sample plate can be reused for further experiments after the initial BLI analysis. This feature not only conserves valuable samples but also enables subsequent analyses or assays, enhancing the efficiency and versatility of the experimental workflow. It's important to optimize the concentration and amount based on preliminary experiments to ensure reliable and reproducible results.

Generally, for the experiment you need:

  • Immobilized Protein: Typically, a few micrograms (µg) of the protein are needed to immobilize on the biosensor. The exact amount depends on the protein's molecular weight and the immobilization strategy.
  • Analyte Protein: For the protein in solution (analyte), concentrations in the range of nanomolar (nM) to micromolar (µM) are commonly used.

Surface Plasmon Resonance (SPR) is a technique used to study protein-protein interactions. It allows researchers to measure the binding affinity, kinetics, and specificity of interactions between proteins in real-time without the need for labeling. In SPR, one protein is immobilized on a sensor chip, and the other protein is flowed over the surface. Changes in the refractive index near the surface are measured, which occur when the proteins interact. This provides valuable data on how proteins interact, including the strength and duration of the interaction.

The amount of protein required for Surface Plasmon Resonance (SPR) experiments can vary depending on the specific setup and the proteins involved. Generally, you need:

  • Immobilized Protein: Typically, a few micrograms (µg) of the protein are needed to immobilize on the sensor chip. The exact amount depends on the protein's molecular weight and the immobilization method.
  • Analyte Protein: For the protein in solution (analyte), concentrations in the range of nanomolar (nM) to micromolar (µM) are commonly used. The total volume required can range from a few hundred microliters (µL) to a few milliliters (mL), depending on the experimental design and the number of replicates.

It's important to optimize the concentration and amount based on preliminary experiments to ensure reliable and reproducible results. 

References

Acuner Ozbabacan, S. E., Engin, H. B., Gursoy, A., & Keskin, O. (2011). Transient protein–protein interactions. Protein Engineering, Design and Selection, 24 (9), 635–648. https://doi.org/10.1093/protein/gzr025

Berggård, T., Linse, S., & James, P. (2007). Methods for the detection and analysis of protein-protein interactions. Proteomics, 7(16), 2833–2842. https://doi.org/10.1002/pmic.200700131 

Goncearenco, A., Li, M., Simonetti, F. L., Shoemaker, B. A., & Panchenko, A. R. (2017). Exploring Protein-Protein Interactions as Drug Targets for Anti-cancer Therapy with In Silico Workflows. Methods in molecular biology (Clifton, N.J.), 1647, 221–236. https://doi.org/10.1007/978-1-4939-7201-2_15

Lu, H., Zhou, Q., He, J., Jiang, Z., Peng, C., Tong, R., & Shi, J. (2020). Recent advances in the development of protein-protein interactions modulators: mechanisms and clinical trials. Signal transduction and targeted therapy, 5(1), 213. https://doi.org/10.1038/s41392-020-00315-3

Request a Quote, Demo, or More Information

What other areas are you interested in? (select all that apply)

Request a Quote, Demo, or More Information

Related Content

icon-octet-family

Biologics Characterization Tools

Explore More
icon-instrument-service

Octet® System Service and Support

Explore More
icon-supplement

Octet® BLI Resources

Explore More

Follow Octet® on LinkedIn

Get the Latest Updates, Trends and Developments on Label-free, Stress-Free Solutions for Drug Discovery, Biologics Development and Biomanufacturing.

Follow Us Now