Pharmaceutical Microbiology Quality Control
In a pharma QC microbiology laboratory, the primary objective is to identify viable microorganisms at every stage of the production process: in the air, raw materials, water and finished products. This enables lot release with the assurance of safety, efficacy and purity. To achieve this, regulatory compliant equipment and consumables are required and help to promote safe handling while minimizing the risk of false positives and false negatives.
Sartorius supports your contamination control strategy (CCS) with consumables and hardware for:
- Microbial enumeration - USP <61>, <62> and <1231>, Ph.Eur. 2.6.12, JP 4.05
- Growth-based sterility testing - USP <71>, EP 2.6.1, JP 4.06
- Rapid PCR sterility testing - EP 5.1.6, EP 2.6.27
- Microbial air monitoring – EN ISO 17141, EU GMP Annex 1
- Rapid PCR mycoplasma detection - EP 2.6.7
Product Highlights
Microbial Enumeration | Bioburden Testing | Growth-based method
To ensure the safety of pharmaceutical products, it is crucial to monitor for and eliminate microbiological contaminants from laboratory and manufacturing environments. While membrane filtration is the preferred method for microbial enumeration, transferring the filter to the media can lead to contamination and false positives.
Microsart® filters provide a solution by combining a sterile filter unit with pre-filled agar media plate, enabling touch-free membrane transfer, and reducing the risk of secondary contamination. This innovative approach enhances the accuracy and reliability of microbial enumeration/bioburden testing, meeting regulatory requirements such as USP <61>, <62> and <1231>, Ph.Eur. 2.6.12, JP 4.05. Don't compromise when it comes to patient safety - choose Microsart® filters for reliable and accurate microbial enumeration.
- Touch-free membrane transfer
- Easy colony enumeration and picking
- Filter base and gridded membrane comes combined with a sterile 100 mL or 250 mL funnel
- Media comes pre-filled, sterile packaged, and ready-to-use
Download Application Note: Filtration of Viscous Samples for Microbiology QC
Explore Microbial Enumeration | Bioburden Testing
Sterility Testing | Compendial Growth-Based Method
Testing for sterility is required for sterile pharmaceutical, medical, and cosmetics products such as aqueous solutions, soluble solids, ointments, creams, parenteral preparations, and ophthalmics. According to USP <71>, EP 2.6.1, or JP 4.06, membrane filtration can be used for filterable aqueous preparations, alcoholic or oily preparations, and preparations that are miscible with or soluble in aqueous or oily solvents. To ensure accurate results, the test environment must be kept aseptic.
The Sterisart® family provides a range of closed, compatible, and cost-effective systems for sterility testing. These systems protect samples from secondary contamination and lab personnel from hazards associated with handling spikes and needles. The Sterisart® solution is more than just a product; it is a comprehensive customer solution:
- 20 different types of filtration units, canisters Sterisart® NF with specific adapters to best fit your specific product
- One system for the entire testing procedure, including Sterisart® Universal Pump | Gen 4
- Designed for use in laminar flow and isolators
- Backed by a global network of highly qualified service engineers and accredited local service centers
Watch Sterisart Testing Video Guide
Watch Sterile Sample Extraction & Rapid Release Webinar
Alternative Rapid Sterility Testing | Real-Time PCR method
Compendial microbiological methods may be considered as slow, making proactive corrective action difficult at times. Alternative sterility testing methods offer near real-time results and an opportunity for earlier corrective action, improving testing quality for small volumes or non-filterable new cell-based therapeutics like ATMPs or CAR-T cells. These methods can be used for in-process samples or final product release. Even if methods described in the Pharmacopoeia are still reference methods, validation of new, rapid methods is described in EP 5.1.6, USP <1223> or USP <1071>, as they increase patient safety and reduce the need for prophylactic medication with antibiotics.
Microsart® ATMP Sterile Release Kit, a combination of Microsart® ATMP Bacteria and of Microsart® ATMP Fungi, detects bacterial and fungal contamination within three hours, using the proven real-time PCR method.
- Developed in close cooperation with authorities, and validated according to EP 5.1.6 and USP <1223> for sensitivity, specificity, and robustness
- TaqMan® probes ensure the highest level of qPCR specificity
- Lyophilized, inactivated or non-viable validation standards for required bacterial and fungal species
Download Rapid Sterility Poster
Microbial Air Monitoring
Monitoring air ambient in cleanrooms, isolators, or filling lines (i.e. RABS or BFS) for viable microorganisms is a routine task in the pharmaceutical, medical and cosmetics industries. Continuous monitoring of airborne viruses, bacteria, yeasts, and fungi permit trends to be recognized early. This helps in determining the root cause when contamination results are Out Of Tolerances (OOT), as a key requirement of standards and guidelines, such as the EN 17141 and the revision of the EU GMP Annex 1.
With MD8 Airscan®, you can continuously monitor the air environment for a minimum of 8 hours using just one gelatin membrane filter. However, gelatin filters have the retentive capacity of a depth filter (e.g. HEPA H14 filter) and facilitate near complete retention of microbes and viruses, due to the sieving and diffusion effect, with no loss of recovery.
- Agar-free gelatin membrane filters do not dry out during long-term sampling nor influence microbial growth
- Adaptable sampling head based on your requirements: installation in your production lines and in lab isolators or stand-alone benchtop unit
- Optional aseptic transfer of gelatin membrane filters in isolators or RABS with single-use Biosafe® Bags
Download EU GMP Annex 1 Application Note
Watch Impacts on Microbial Air Monitoring Webinar
Rapid Mycoplasma Detection | Real-Time PCR method
Mycoplasmas are small bacteria that can reproduce independently and cause problems in cell cultures. Routine QC and in-process testing are required for master cell bank (MCB), working cell bank (WCB), as well as for cell substrates that are used in the manufacture of biotechnological/biological products. Nucleic acid amplification techniques (NAT) alternative methods can provide faster results than traditional methods and are well described in USP, JP and EP. They must detect 10 CFU/mL of Mycoplasma, when viable but non-culturable (VBNC) Mycoplasma may go undetected even after 28 days of culture with the traditional method of mycoplasma, risking false-negative results.
Microsart® Mycoplasma qPCR detection kits offer a method for early detection of Mycoplasma contamination. The easy-to-follow protocol is aided by color-coded reagents that are both clear and concise. Additionally, the lyophilized reagents guarantee consistent quality without requiring freezer storage.
- Validated according to EP 2.6.7and USP 63 for sensitivity, specificity, and robustness
- TaqMan® probes ensure the highest level of qPCR specificity
- Lyophilized, non-infectious Mycoplasma validation standards, each containing 10 CFU of the chosen Mycoplasma species
- Applicable on any qPCR cycler suitable to detect FAM™ and ROX™ dyes
Download Microsart® AMP Mycoplasma Kit Application Note
Download Detection and Prevention of Mycoplasma Contamination in Cell Cultures Infographic
Sartorius Pharmaceutical Features
Broad range of solutions to support your Contamination Control Strategy and batch release decisions, with compendial growth-based and rapid NAT methods.
Validated solutions and services to comply with the main international regulations and standards.
German-engineered manufacturing of microbiology membranes, consumables, and hardware for over 50 years and continuous improvement to serve our customer needs in highly regulated environments.
Cell-based Therapies - Be on the Safe Side
Watch how Microsart® ATMP Sterile Release and Mycoplasma Kits detect bacteria, fungi and mycoplasma in your cell therapy products in only 3 hours.
Frequently Asked Questions
Bioburden testing counts the viable microorganisms in or on a material before sterilization or further processing. It is required at raw material receipt, at in-process hold points, on water systems, and immediately before sterilization or sterile filtration.
Since 1 December 2025, USP <1119> - Bioburden Monitoring* and <1119.1> - Bioburden Test have governed this testing, replacing chapter <1229.3>. They exist to correct a common error: USP <61> is not interchangeable with bioburden testing. USP <61> covers release testing of non-sterile products, while <1119> covers process monitoring and extends to sterile products, in-process material, containers, and pharmaceutical water. Unlike USP <61>, it is risk-based sampling sites, frequencies, and limits must be scientifically justified. Ph. Eur. 2.6.12 and JP 4.05 apply outside the US.
Sterility tests must detect aerobic bacteria, anaerobic bacteria, yeasts, and molds. Fluid Thioglycollate Medium is incubated at 30-35°C for anaerobes; Soybean Casein Digest Medium at 20-25°C for aerobes and fungi. Incubation runs 14 days.
Growth promotion testing confirms the media support these organisms. FTM is challenged separately with Clostridium sporogenes, Pseudomonas aeruginosa, and Staphylococcus aureus; SCDM with Aspergillus brasiliensis, Bacillus subtilis, and Candida albicans, each at no more than 100 CFU. The test is read visually and is pass/fail: any macroscopic growth within the 14 days fails and triggers a sterility failure investigation before batch disposition. USP <71> and Ph. Eur. 2.6.1 have been harmonized since 2002.
A sterility test confirms the absence of any viable microorganism in finished sterile product: a pass/fail release assay under USP <71>. A bioburden test counts the organisms present before sterilization: a quantitative process control under USP <1119> series.
Products with antimicrobial activity are filtered through a 0.45 µm membrane and rinsed with sterile diluent to remove inhibitory residue before incubation. Oily preparations are first dissolved in a sterile, non-inhibitory solvent such as isopropyl myristate.
The rinse is the step most often under-validated. USP <71> permits up to five 100 mL portions per membrane, with three a common starting point. Fluid A is the general-purpose rinse; Fluid D adds polysorbate 80 for oils and poorly wettable matrices; beta-lactams require penicillinase alongside rinsing rather than instead of it. Rinse volume, rinse fluid, and any inactivator must be fixed by the method suitability test, not adjusted per batch. Closed systems such as Sterisart perform these steps through a sealed fluid path, reducing exposure during the longer handling these matrices require.
A MST proves your product does not inhibit microbial growth under your test conditions. This was formally called the bacteriostasis and fungistasis (B&F) test. Without conducting this test, one cannot tell whether nothing grew because nothing was there, or because the product suppressed it. It also must be conducted on every new or reformulated product.
Requirements changed in 2026. Ph. Eur. 2.6.7 version 12.2 came into force on 1 April 2026, and USP <77> becomes official on 1 October 2026. Both recognize NAT methods as equivalent to culture and indicator cell culture, rather than as alternatives requiring comparability. In Ph. Eur. 2.6.7, there is more emphasis on the workflow.
The sensitivity criterion is now a limit of detection of 10 CFU/mL or <100 genomic copies/mL, introducing genomic copies as a standardized unit for the first time. Validation material must have CFU determined at harvest without prior freezing, with a GC/CFU ratio not exceeding 10. Testing should cover both cells and supernatant, defined controls including an external positive control are mandatory, and emphasis has shifted from method comparison toward whole-workflow validation.
VBNC mycoplasmas are metabolically active but will not form colonies under standard culture conditions, so a 28-day culture test can return a clean result on a contaminated batch. Ph. Eur. 2.6.7 now explicitly requires detection of both culturable and non-culturable mycoplasmas.
That effectively ends culture-only strategies: a method blind to the non-culturable fraction no longer satisfies the chapter on its own. qPCR, RT-qPCR, and digital PCR are the recognized route and may replace culture, indicator cell culture, or both when properly validated. Exposure is highest in cell and gene therapies, where shelf life is shorter than a 28-day test, and in any process using serum-derived raw materials.
USP <62> is a qualitative absence test rather than a count. It requires specified organisms to be absent from a defined sample quantity, with the organism panel set by the product's route of administration.
Note that "objectionable" may extends beyond the listed organisms as the FDA has taken enforcement action over Burkholderia cepacia complex (BCC) in aqueous non-sterile products so compliance to USP <62> result is a floor rather than a ceiling. Results are read alongside USP <61>: USP <61> tells you how much, USP <62> tells you what.
Closed systems keep the fluid path sealed from sample introduction through to incubation, removing the manual membrane transfer that is the largest single source of laboratory-induced contamination.
The cost of a false test result is easy to underestimate. One false positive triggers a full sterility failure investigation for that batch; while one false negative triggers a full sterility failure investigation since the last validation of the test method. Under EU GMP Annex 1, that investigation must produce a defensible root cause; if it cannot conclusively demonstrate laboratory error, the batch cannot be released. Open canister methods require an operator to open the system and transfer the membrane by hand in the critical zone. Closed systems such as Sterisart eliminate that step.
Inspectors assess microbiology laboratories against 21 CFR 211.194, EU GMP Annex 1, and ICH Q10. The recurring finding is rarely a missing document, it is broken traceability, where records exist but cannot be linked back to a result.
Expect requests for validated SOPs and method validation packages; current per-product method suitability tests; IQ/OQ/PQ, calibration, and maintenance records for incubators, autoclaves, isolators, and cabinets; media preparation records with lot traceability and growth promotion testing of every lot; reference cultures within five passages of the reference lot; analyst training and aseptic qualification; environmental and personnel monitoring with trending; and ALCOA+ raw data with audit trails. A sterility result should trace to its medium lot, analyst, qualification status, session monitoring, and equipment without anyone having to reconstruct it.
USP <63> defines what a mycoplasma test must achieve. USP <77> - Mycoplasma Nucleic Acid Amplification Tests, official 1 October 2026, defines how to prove a NAT method achieves it. USP <77> does not replace <63>; it closes a gap <63> left open.
USP <63> prescribes two compendial procedures: Method A, the agar and broth media procedure, and Method B, the indicator cell culture procedure. It permits a validated NAT or enzymatic method to be used instead, but it never sets out how that validation should be conducted only that the method must be shown comparable to Method A or B. Molecular method development ran well ahead of the chapter, and laboratories were left interpreting comparability for themselves.
USP <77> supplies the missing criteria: validation design, definition of intended use, control strategy, and specificity demonstrated across more than 100 mollicute species. It formalizes the GC-to-CFU ratio as an accuracy metric, aligning with the 10 CFU/mL or <100 genomic copies/mL sensitivity requirement in Ph. Eur. 2.6.7 v12.2 and JP 18 G3. In practice, if you run NAT for release testing, USP <63> remains the reference your method is measured against and USP <77> becomes the yardstick for your validation package.