Front of the iQue 5 Platform on transparent background

Streamline Your Antibody Discovery and Screening with Sartorius Solutions

Antibody Discovery and Screening Workflows

Therapeutic antibodies are one of the fastest-growing classes of drugs with the promise of better specificity and safety. Successful antibody discovery campaigns take advantage of technologies that allow for rapid identification and characterization of candidate molecules with superior target reactivity and optimized functionality.

The iQue® High-Throughput Screening (HTS) by Cytometry Platform saves you time, resources, and cost across the biologics discovery workflow.

  • Screen antibodies generated from hybridomas and primary B-cell cultures as well as arrayed libraries from display technologies
  • Identify candidates with the desired biological outcome by evaluating cell health, function and cytokine release in the same assay
  • Rapidly identify lead clones by simultaneously evaluating suspension CHO cells and quantifying their secreted proteins

Click below to see how the iQue® High-Throughput Screening Cytometry Platform streamlines the three biologics discovery workflow steps antibody screening, functional profiling, and bioprocessing.
 

Request More Information

icon-webcast

Webinar: Effective Cell Line Development

Reducing Risk, Decreasing Timelines, and Optimizing Outcomes

Watch Now

Explore Solutions for Antibody Discovery Workflows

icon-ique5

Antibody Screening

Get fast and timely access to antibody specificity and species cross reactivity during primary screening.

View Details
icon-assay

Functional Profiling

Easily go from high content functional assays to actionable information that helps you select candidates with desirable biological activity.

View Details
icon-bioprocess

Bioprocessing

Select antibody clones upstream of cell line development by simultaneously detecting IgG titer, cell health and viability.

View Details

Antibody Discovery & Screening Platforms

The iQue® 5 High-Throughput Screening (HTS) Cytometer being prepared for use.

iQue® HTS by Cytometry Platform

Meet the iQue® HTS cytometry platform, which focuses on speed from setup to acquisition and analysis.

Two laboratory technicians in a lab viewing information from the Octet RH96 N1 on an iPad.

Octet® BLI Detection Systems

Analyze titer & concentration in crude samples, do real-time flexible epitope binning, and screen for CQAs at early stage CLD with Octet® BLI.

Octet SF3 with Lab Technician

Octet® SPR Detection 

Generate the most accurate binding kinetics data in the shortest timeframe imaginable with the Octet® Surface Plasmon Resonance (SPR) system.

Video Testimonial

How the iQue® High-Throughput Screening Cytometry Platform is Changing the Way We Obtain Compelling Data

“In-solution, cell-based assays are the way forward and the ability to do so with the iQue® Screener in a 384-well high-throughput format has been extremely useful to us. We can now use one third of the materials and screen 4 times more antibody clones in the same amount of time, obtaining more compelling data for ourselves and our clients. – Andrea Gorlani, PhD, Scientist ModiQuest Research

The Benefits of Antibody Discovery with the iQue® HTS Platform

The iQue® High-Throughput Screening Platform utilizes a unique and rapid, air-gap-delimited sampling technology paired to a no-adjustment, flow-based detection engine and powerful, easy-to-use iQue Forecyt® Software for assay management and analysis.
 

More Data Than ELISAs

Unlike ELISAs, which can only report on binding to single antigens and require large amounts of the target protein to coat entire wells, the iQue® HTS Platform is able to simultaneously acquire data on multiple biological readouts and with much less protein. Using differential fluorescent labeling, multiple cell types and a range of cellular parameters can be assessed all in the same well, quickly generating a rich, highly-informative data set. And because multiple target proteins can be presented on beads or on the cell surface, precious reagents are conserved, reducing costs.
 

Assays in More Relevant, Native Environments

Because the iQue® HTS Platform supports cell-based assays, target proteins can be presented on the cell surface instead of coated on the wells of a plate. By placing the target in its native conformation, results are more likely to be biologically relevant and better indicators of what will happen in vivo.
 

Faster than Traditional Flow

By sampling only microliters from each well and delivering an air-gap-delimited flow of samples to the detectors, the iQue® High-Throughput Screening (HTS) by Cytometry Platform converts the traditional low throughput, time-consuming flow cytometry approach into a high throughput process capable of rapidly driving the antibody screening process forward. The end result is a data-rich snapshot of the molecular events occurring in each well that can take less than five minutes for a 96-well plate and under 20 minutes for a 384-well plate.
 

Get More Relevant Data on your Antibodies Faster with the iQue® High-Throughput Screening (HTS) by Cytometry Platform

  • Gain more relevant insights by screening targets in their native conformations on the cell surface.
  • Expand what each assay tells you by assessing binding against multiple targets simultaneously.
  • Increase the scale of your screens through the ability to use much less of each target protein.
  • Amplify what you learn by combining binding assays with functional assays.

Request a Quote, Demo, or More Information

What other areas are you interested in? (select all that apply)

Request a Demo, Literature, or More Information