Cell and gene therapy illustration containing stem cells and DNA

Gene Therapy Development

Reduce Time, Effort and Cost in Bioprocessing for Cell and Gene Therapy

Cell and gene therapy (CGT) is a new and promising immunotherapy for patients suffering from certain types of cancer. CGT is among the treatments of Advanced Therapy Medicinal Products (ATMP) transforming how biopharma companies treat and potentially cure certain diseases.

Genes are used to treat, prevent or cure a disease or medical disorder. Often, gene therapy works by adding new copies of a gene that is broken, or by replacing a defective or missing gene in a patient’s cells with a healthy version. With adeno-associated viruses (AAVs) - the viral vector of choice for in vivo treatment - along with a growing interest in gene therapies, there is an increasing need for cost-effective vector manufacturing technologies and viral vector production platforms for human gene therapy products.

Rapid Quantitation of AAV Capsids in Bioprocess Development for Gene Therapy Using Octet® BLI

Rapid Quantitation of AAV Capsids in Bioprocess Development for Gene Therapy Using Octet® BLI

Adeno-associated virus (AAV), with low immunogenicity and toxicity, has become one of the most promising viral vectors used for delivery of genetic material in gene therapy. AAV vector development and production at industrial scale requires an efficient method for accurate quantitation of viral capsids in both upstream and downstream bioprocessing.

Octet® Bio-Layer Interferometry (BLI) systems in combination with the Octet® AAVX Biosensors offer a rapid, label-free, and high-throughput method for quantification of AAV capsids. This video compares the Octet® AAVX biosensor workflow to that of ELISA at various stages in bioprocess development.

Featured Applications

Rapid and Direct Quantitation of AAV Capsids

To meet increased throughput and safety demands, scientists at BridgeBio Pharma, Inc. and REGENXBIO Inc. are making use of the novel approach of AAV capsid titer quantification with label-free biosensor assays, which offers a robust alternative to conventional ELISA approaches.

Octet® BLI instruments are eliminating hands-on steps that come with running a traditional immunoassay. Time and human error are significantly decreased, both factors that adversely impact assay reproducibility and team productivity.

Read Application Note

Fast Measurement of AAV Serotypes in Crude and Purified Samples

A rapid and robust method for AAV capsid quantitation is essential for AAV bioprocess development and manufacturing. Conventional ELISA, HPLC and ddPCR methods for AAV titer measurement are time-consuming and labor intensive.

The Octet® Bio-Layer Interferometry (BLI) Platform - using the Octet® AAVX Biosensors - provides a label-free approach with a broad dynamic range from 8.5 x 108 to 1.0 x 1013 vp/mL for all serotypes tested. It also shows high precision and accuracy for capsid quantitation of both purified and crude AAV samples and can be regenerated and re-used up to 20 times providing an efficient and cost-effective solution for high-throughput AAV quantitation applications. 

Read Technical Note

Featured Resources

Imagery of adeno-associated vector genome. Two capsids are present one empty the other full, with DNA cargo. For AAV empty/full ratio assay in gene therapy.
Technical Note

Still Analyzing AAV Empty/Full Ratio the Hard Way?

Experience a novel, rapid, and high-throughput approach for determining AAV empty/full ratio in as little as 30 minutes.

cell visualisation
Webinar

A New Wave Biosensor Approach for AAV Process Development

REGENXBIO Inc. shares their experience in finding a high-throughput technique for AAV capsid concentration quantification.

Octet® AAVX Biosensors for Rapid and Direct Quantitation of AAV Capsids
Application Note

Measure AAV Titer in as Little as 15 Minutes

Rapid Quantitation of AAV Capsids for Various Serotypes for Bioprocess Development and Quality Control in Gene Therapy

app note cover
Application Note

Biomolecular Binding Kinetics Assays on the Octet® Platform

Explore advantages of label-free binding assessment in therapeutics development and life sciences research.

A compendium for successful BLI and SPR assays
Application Guide

A Compendium for Successful BLI and SPR Assays

A comprehensive guide for designing and performing label-free biomolecular interaction analysis.

AAV capsid 3D model in combination with the Octet BLI biosensor icon
Webinar

Reduce Cycle Times for AAV Quantification

See the Octet® AAVX Biosensor in comparison to an in-house assay on the Octet BLI platform.

Instant Access

Octet® AAVX Biosensors: For Quantitation of AAV Capsids
Datasheet

Octet® AAVX Biosensors: For Quantitation of AAV Capsids

PDF | 727.5 KB
Octet AAVX Biosensors for Quantitation of AAV Capsids
Technical Note

Octet® AAVX Biosensors for Quantitation of AAV Capsids

PDF | 2.0 MB
Octet RH16 with Lab Tech
Application Note

Converting ELISA Assay Into Octet® Quantitation Assay

PDF | 207.5 KB
application guide thumbnail
Application Guide

Quality Control Of Biotherapeutics Using Octet® Systems

PDF | 1.9 MB

Related Products

Octet® BLI rapidly determines recombinant protein concentration as a control parameter in cell line development.

96-Channel Ultra High Throughput Octet System: Octet® RH96

Monitors up to 96 biosensors simultaneously, enabling label-free detection for protein quantitation and kinetic characterization at unmatched speed

Octet RH16 ultra high throughput label free detection system

16-Channel High Throughput Octet System: Octet® RH16

Ideal for high-throughput applications that demand high sensitivity and low sample volume requirements

Octet R8 label free detection system instrument

8-Channel System: Octet® R8

Unmatched flexibility and versatility in protein analysis

Request a Quote, Demo, or More Information

What other areas are you interested in? (select all that apply)

Request a Quote, Demo, or More Information

Related Content

icon-octet-family

Biologics Characterization Tools

Explore More
icon-instrument-service

Octet® System Service and Support

Explore More
icon-supplement

Octet® BLI Resources

Explore More

Follow Octet® on LinkedIn

Get the Latest Updates, Trends and Developments on Label-free, Stress-Free Solutions for Drug Discovery, Biologics Development and Biomanufacturing.

Follow Us Now