On-Demand Webinar: Treasure Hunting with Octet®  | A New-Wave Biosensor Approach for Direct, Fast and High-Throughput AAV Process Development

Last updated: February 2024


This webinar will highlight REGENXBIO’s experience in finding a high-throughput technology for AAV capsid concentration quantification including comparisons between Octet® AAVX Biosensors and other analytical methods. We will also present an assessment on reliability of % full capsid data generated using various methods including Octet® AAVX Biosensors, as well as case studies making use of the quantification information generated from this technology.

Overview

Gene therapies are designed to deliver functional genes to address genetic defects in cells, enabling the production of therapeutic proteins or antibodies that are intended to impact disease. While the global pipeline for adeno-associated virus (AAV) gene therapy continues to expand, there are key challenges, such as characterization data to better understand AAV, that still need to be addressed. One of the fundamental characterization datasets that should be assessed, especially in a high-throughput format, is AAV capsid concentration in solution.


  • Document type: Webinar
  • View time: 53 minutes


Complete the Form to Access the Webinar

Key Takeaways

Topics discussed:

  • Reasons explaining why it is necessary to quantify total AAV capsids
  • Evaluation summary of different methods for capsid quantification
  • Comparison data package for calculated % full capsid using Octet® data and other methods
  • Real life datasets showing the usefulness of the capsid titer data and packaging efficiency (%full) data generated on Octet® BLI Platform

Webinar Speakers

Amanda Zhang, MS

Senior Scientist Scientific Project Manager
REGENXBIO

Amanda Zhang is a Senior Scientist and Scientific Project Manager with REGENXBIO who has been in the downstream field working on purification and characterization of antibodies and adeno-associated virus (AAV) for 15 years.

She has developed numerous downstream processes that led to IND filings and has set up technologies for the early characterizations of antibodies and AAV. At REGENXBIO, she is responsible for production of recombinant AAV vectors in support of pre-clinical and IND enabling studies.

In addition, she plays a key role in bridging R&ED and Process Development functions by providing early phase knowledge on process, product, and manufacturability to relevant teams. She also takes part in facilitating and streamlining operations to maximize impact on early phase pipeline and platform development.

Follow Octet® on LinkedIn

Get the Latest Updates, Trends and Developments on Label-free, Stress-Free Solutions for Drug Discovery, Biologics Development and Biomanufacturing.

Follow Us Now
Imagery of adeno-associated vector genome. Two capsids are present one empty the other full, with DNA cargo. For AAV empty/full ratio assay in gene therapy.
Technical Note

Still Analyzing AAV Empty/Full Ratio the Hard Way?

Experience a novel, rapid, and high-throughput approach for determining AAV empty/full ratio in as little as 30 minutes.

Access Tech Note

Request a Quote, Demo, or More Information

What other areas are you interested in? (select all that apply)

Please Complete the Form to Access the Webinar

icon-shopping-cart
Ready to Buy?