tacta mechanical pipette

ISO 8655: 2022 Frequently Asked Questions

Most Frequently Asked Questions About New Revision of the ISO 8655 Standard

Overview

ISO 8655 standard addresses the needs of pipette manufacturers and test houses. Also it gives good basis for end users to set up pipette quality control program.

  • Document Type: Flyer
  • Page count: 4
  • Read time: 8 minutes
  • Last updated: August 2022

 Read these FAQs below or
 

Download the Flyer

The new ISO 8655:2022 Piston Operated Volumetric Apparatus FAQ flyer cover

This FAQ flyer covers the following:

  1. Key changes in 8655 new revision
  2. Pipette reference- and alternative test methods
  3. In use testing routine for pipettes

ISO 8655 Frequently Asked Questions

ISO 8655:2022 contains requirements for producing and in use control of piston-operated volumetric apparatus (POVA). This includes testing methods, testing environment, testing equipment, reporting requirements, requirements for measurement uncertainty, and general requirements for how POVAs work. The ISO 8655:2022 is applicable to pipettes, burettes, dilutors, dispensers and manually operated precision laboratory syringes.

ISO 8655:2022 consists of nine parts total, which is two more parts then in the previous version. There are major and minor changes to all parts. Part 9 of the new ISO 8655:2022 describes a new instrument class - manually operated precision laboratory syringes.

The ISO 8655:2022 describes two different reference measurement procedures for the determination of volume (a gravimetric procedure in part 6 and a photometric procedure in part 8). In addition to the reference measurement procedures, part 7 (new chapter) describes alternative procedures.

Unlike laws, standards are only legally binding when stipulated in legislation or in contracts. For an accredited calibration laboratory, the ISO 8655:2022 becomes binding when this standard is named in the accreditation certificate. However, even where standards are not expressly named in a contractual agreement or law, they are used to settle legal disputes, especially in product liability cases. In this way, standards provide legal certainty. Therefore, it is recommended to follow the new ISO 8655:2022 after it is officially published in a country.

In former versions of the ISO 8655 the gravimetric measurement procedure for volume determination has been described as the “gold standard”. The gravimetric procedure (Part 6 in the ISO 8655:2022) is now losing this unique position. The photometric procedure (Part 8 in the ISO 8655:2022) is now given equal status as the second reference measuring procedure.

Currently, the ISO does not favor one method over the other.

Following a reference measurement procedure, calibrations and tests must be performed following strict requirements. Deviations from these requirements when referring to part 6 (gravimetric reference procedure) or part 8 (photometric reference procedure) are not permitted.

However, it is not always possible to fulfill the environmental requirements described in Parts 6 and 8, especially when calibrating or testing a POVA on the customer site. The alternative measurement procedure allows deviations from these strict requirements within limits.

Calibrations and tests under Part 7 require specific environmental conditions, repetitions and test volumes.

Tests and calibrations under Part 7 A.2 allow use of the gravimetric reference measurement procedure according to Part 6 of the ISO 8655:2022, when all deviations from the reference measurement procedure are recorded and reported. This allows for example to vary the test liquid, the tested volumes, the replicates or the tip changes.

Calibrations and tests done under ISO 8655 Part 7 can also be used as a metrological confirmation of POVA if at least 10 replicate measurements are performed per selected volume and the measurement procedures are validated by comparison to one of the reference measurement procedures.

A metrological confirmation can be done by both a calibration or test and should be performed according to one of the reference measurement procedures described in ISO 8655 Part 6 and ISO 8655 Part 8, or according to an alternative measurement procedure described in ISO 8655 Part 7.

Both calibration and test are defined as a set of operations that establish the relationship between the delivered volume and the corresponding selected volume of the apparatus. While the estimate of measurement uncertainties is required for a calibration, this is optional when testing a POVA.

The ISO states that a metrological confirmation of all POVA shall be performed regularly to ensure that the apparatus meets the requirements for its intended use.

The recommended frequency is based on the risks associated with using the POVA. The maintenance interval is affected by such factors as pipetting frequency, liquids dispensed and the age/model of the pipette. A minimum maintenance interval of one year is suggested, with calibration done annually or more often, such as every 3 – 6 months. In some circumstances, such as when dispensing volatile liquids or solvents, more frequent maintenance is advised.

The following factors should be considered:

  • Risk of application
  • Frequency of use 
  • Number of users
  • Type of liquid to be delivered and its vapors
  • Acceptable maximum permissible errors
  • Manufacturer information
  • Liquid handling process requirement

The ISO 8655:2022 clearly states that an as-found calibration or test should be carried out and a metrological confirmation should be considered before and after the maintenance or repair of a POVA. Maintenance or repairs can affect the performance of a POVA and the as-found calibration is needed to interpret results obtained beforehand.

Calibration and test under the ISO 8655:2022 can be done against the ISO 8655, manufacturer or customer/user tolerances. A test against the ISO 8655 tolerances is necessary to prove that the ISO standard is fulfilled. If the manufacturer or customer/user tolerances are stricter or equal to the ISO 8655 tolerances, then the standard is fulfilled. Deviations that are not within the ISO 8655 tolerances do not prove that the ISO standard is fulfilled.

Calibration and test according to ISO 8655 Part 6, Part 7 and Part 8 require tolerances for the nominal volume, 50 % of the nominal volume and 10 % of the nominal volume (or the lower limit if the min is > 10 % of the nominal volume). If no manufacturer or customer/user tolerances for these volumes are available, only a test according to ISO 8655 Part 7 A.2 is possible.

Calibration and testing under ISO 8655 Part 6, Part 7 and Part 8 must be done with at least 10 repetitions per tested volume and at three points, minimum. They must be set to the nominal volume, 50 % of the nominal volume and 10 % of the nominal volume (or the lower limit if min is > 10 % of the nominal volume).

Only the ISO 8655 Part 7 A.2 allows for the calibration or testing of the POVA with other, or less calibration volumes, and less than 10 repetitions.

Some POVA require the use of exchangeable parts during typical use (e.g., disposable pipette tips). The new ISO 8655 describes the POVA and the exchangeable part as a system and requires that these exchangeable parts constitute an integral part of the POVA under test. Therefore, the calibration results are only valid for the tip type used during the calibration. In case the POVA is used with different tip types, a separate calibration should be performed with each tip type.

The new ISO 8655:2022 clearly describes that the maximum permissible errors apply to the total system of pipette and tip. Before a pipette tip is placed on the market, the tip manufacturer must prove that the whole system, pipette and tip, fulfills the requirements and maximum permissible errors of the new ISO 8655. Using the tip is not recommended if the manufacturer of a third-party tip has not provided this validation.

According to ISO 8655 Part 6, Part 7 and Part 8 the tip must be changed at least once per calibrated volume when performing calibration or testing, in order to detect damaged or incorrectly manufactured tips. When performing the calibration under ISO 8655 Part 7 A.2, the tip does not need to be changed mandatorily.

Measurement results can only be compared if they are taken under the same conditions. Common laboratory conditions fluctuate and are never completely standard. To enable comparison of results from different calibration laboratories, all variables that affect liquid properties, such as temperature, humidity and air pressure, must be controlled.

In short, ISO 8655 describes how the calibration of a POVA is performed, while ISO 17025 entitled “General requirements for the competence of testing and calibration laboratories” defines the requirements that a calibration laboratory must meet to work competently and achieve valid calibration results. Within the accreditation process, the calibration laboratory must prove to an independent accreditation body that it is complying with the corresponding national and international standards, laws and guidelines and therefore is operating at a globally comparable level.

One important section within the ISO 17025 describes the traceability of the test equipment. This means that all test equipment that is used for calibration or as part of a calibration must be traceable to international standards. This ensures that an accredited calibration certificate alone is always recognized as proof of traceability.

The following requirements need to be fulfilled following ISO8655:2022

Nominal Volume of the POVA

Resolution (d)
(mg)

Repeatability (s)
(mg)

Expanded Uncertainty in use (Ugl[W])
(mg)

0.5 μL ≤ V < 20 μL

0.001a
0.01b

0.006a
0.03b

0.012a
0.06b

20 μL ≤ V < 200 μL

0.01

0.025

0.05

200 μL ≤ V ≤ 10 mL

0.1

0.2

0.4

10 mL < V ≤ 1,000 mL

1

2

4

1,000 mL < V ≤ 2,000 mL

10

10

40

a single-channel balance
b Multi-channel balance (to be used below 20 µL only if the expanded uncertainty in use is less than ¼ of the maximum permissible systematic error of the apparatus)

Do you need support regarding the new ISO8655 norm?

Contact an Expert

Related Educational Resources

Application Guide

How to Set Up a Pipetting Quality Control Program for Your Lab

Calibration, maintenance, and regular control of tools are essential to ensure the highest quality standards of laboratory work.

Application Note

Best Practices for Pipetting 3D Cell Culture Hydrogels

Three-dimensional (3D) cell culture preparation can be a difficult process. Learn some best practices.

application note cover
Application Note

Are You GLP/GMP Compliant When it Comes to Pipetting?

This application note introduces principles that can help you with demanding requirements when it comes to your pipetting practices.

Related Products

Tacta® Mechanical Pipette, Single Channel

Tacta® Mechanical Pipette, Single Channel

Most advanced mechanical pipettes, which do not only provide accurate and repeatable results, but also are nice to use.

Tacta® Mechanical Pipette, 8 Channel

Tacta® Mechanical Pipette, 8 Channel

Most advanced mechanical pipettes, which do not only provide accurate and repeatable results, but also are nice to use.

Optifit Racked Pipette Tips

Choose only the best tips to match your pipettes.

Request a Quote, Demo, or More Information

What other areas are you interested in? (select all that apply)

Request a Quote, Demo, or More Information

New Products and Promotions

Light Pack Pipette Tip Box key campaign visual

The Wait is Over! Introducing the Responsible Pipette Tip Box

Sartorius Light Pack: Less plastic, fully foldable, same performance. ACT® certified and 2026 Red Dot Award winner. Try it today!

New

Revolutionizing pipette calibration with the new Cubis® II MPS116S

Designed for fast, reliable, and compliant calibration of 95% of all single channel pipette volumes, from 2 µL to 5 mL.  

Pipette Trade-In Program | Up to 40% Discount on Pipette Products

Trade in your old pipettes for the most ergonomic electronic or mechanical pipettes available – all while receiving up to 40% off.

Order Your Free Sample of Tips

Request a free pipette tip sample today and optimize your pipetting system.

Shopping cart with various lab products inside
Sale

Shop More, Save More: Get Up to 10% Off Lab Products

Get 5% off orders $0 to $3,000 and 10% off orders above $3,000. Use code SAVEMORE26 at checkout.

icon-shopping-cart
Ready to Buy?