Essential Regulatory Requirements for Laboratory Weighing

Weighing is a crucial step in analytical procedures, making lab scales indispensable in QC labs. Explore this page to understand how the essential requirements for lab balances are described in different chapters of international pharmacopeias like USP 1251, USP 41, Eur.Ph. 2.1.7, JP 9.62, ChP 9032, FDA requirements for electronic records and data integrity as described in 21 CFR part 11 and general guidelines like the calibration guide no. 18 (EURAMET cg18) published by the association of European metrology institutes.

Learn about the essential requirements for electronic balances in QC labs, including good practices, international compliance, minimum weight and smallest net weight, and data integrity.

 

Get in Touch With an Expert

Introducing the Cubis® III and Cubis® II for Connectivity & Compli...

Cubis® III and Cubis® II by Sartorius ensures precise results, regulatory compliance, and seamless connectivity with modern IT environments.

Enhance your laboratory's efficiency and data integrity with Cubis® III and Cubis® II's intelligent functions, comprehensive audit trails, and customizable workflows, designed to meet the demands of Lab 4.0.
 

Step-by-step illustration of the easy Cubis III configurator.

Build Your Balance with the Cubis® III Configurator

Cubis® III lab balance are 100% configurable. Build your custom balance for your specific needs and submit an easy quote request.

Configure Your Cubis® III Balance Now

Updated Requirements for Balances in the Pharmaceutical Industry

The pharmaceutical industry is undergoing significant changes in balance requirements, driven by international harmonization efforts. Major pharmacopoeias—USP, Ph.Eur., JP, and ChP—have revised their guidelines to ensure precise regulations. These updates highlight the importance of reliable balances in achieving accurate analytical results. 

Download the white paper to learn more about how major pharmacopoeias are aligning laboratory balance regulations, and what it means for pharmaceutical quality control.

Access the White Paper

 

USP 41 vs USP 1251

Compare USP 41 and USP 1251 to understand the differences between weighing performance requirements and balance qualification guidelines.

 

Topic

USP 41 : Weighing on an Analytical Balance

USP 1251 : Balance Qualification

Focus / PurposeDefines performance requirements for accurate weighing. Provides guidance on qualification, calibration and verification of  balances. 
ScopeSpecifies how the balance must perform during weighing activities.Specifies how the balance must be qualified to ensure it is fit for its intended use.
Key Requirements
  • Accuracy
  • Repeatability
  • Metrological traceability
  • Use of calibrated test weights
  • Installation Qualification (IQ)
  • Operational Qualification (OQ)
  • Performance Verification (PV)
  • Risk-based qualification
Performance ChecksRequires accuracy and repeatability tests using calibrated weights.Provides guidance on defining intervals and procedures for calibration and checks.
Minimum WeightClarifies how to determine minimum weight based on repeatability results.Refers to minimum weight but focuses on ensuring qualification supports accurate minimum weight.
Environmental ConditionsEmphasizes environmental factors that affect weighing accuracy (temperature, drafts, vibration).Emphasizes environmental controls during installation and qualification.
Safety FactorNot addressed or required.Introduces the safety factor concept (optional, not mandatory).
TraceabilityRequires weights traceable to SI units.Strengthens metrological traceability expectations.
Effective DateUpdated chapter effective February 2026.Revised chapter aligned with modernization; effective February 2026.

Current Revision Status and Regulatory Framework

  • USP: The USP has revised its chapters on balances, with updates effective from February 2026. These revisions are enforced by the Federal Food, Drug, and Cosmetic Act (FDCA).
  • Ph.Eur: Expected revisions to Chapter 2.1.7 will be published by late 2026, enforced by EU Directive 2001/83/EC and EU Regulation 2019/6.

  • JP: New chapters on balances will be implemented by the end of 2025, under the Pharmaceutical and Medical Device Act (PMD Act).
  • ChP: Introduced new guidelines in early 2025, enforced by the Drug Administration Law of the People's Republic of China.

Key Requirements for Compliant Laboratory Weighing

Explore the essential requirements that ensure accurate, reliable, and compliant weighing in laboratory environments, including environmental control, calibration practices, performance checks, minimum weight definitions, and support tools that enable consistent regulatory compliance.

 

All pharmacopoeias emphasize environmental control in balance operation:

  • Temperature: Stable, avoiding direct sunlight.
  • Humidity: 40% to 60% RH.
  • Air Currents: Minimize drafts.
  • Vibration: Use anti-vibration tables.
  • Static Electricity: Use antistatic devices.
  • Electromagnetic Fields: Avoid RF/magnetic sources.
  • Cleanliness: Maintain a clean area.

Calibration ensures metrological traceability to the International System of Units (SI):

  • USP: Emphasizes periodic calibration.
  • Ph.Eur. and ChP: Similar requirements.
  • JP: Provides background on traceability.

Performance checks focus on accuracy and repeatability:

Accuracy

  • Sensitivity: Check using a weight >5% of the balance’s maximum capacity.
  • Calibrated Weight: Use a weight with uncertainty <1/3 of the acceptance criterion.

Repeatability

  • Weight: Use a weight ≤5% of the balance’s maximum capacity.
  • Procedure: Zero balance, place weight, record indication, repeat 10 times.

Clarification of "minimum weight" and "smallest net weight":

  • Smallest Net Weight (msnw): User-defined smallest sample quantity.
  • Minimum Weight (mmin): Calculated from performance checks.

Sartorius offers recommendations and assets to support compliance:

  • Environmental Conditions: Check and improve as necessary.
  • Device Features: Utilize features like IsoCal function.
  • Performance Checks: Define intervals based on risk analysis.
  • Calibration: Define intervals and tolerances.

Supporting Assets

  • White Paper Bundle: Guides on compliant weighing practices.
  • Generic Operating Procedures: Harmonized procedures for performance checks.
  • Service Certificates: Ensuring reliable measurement results.

Regulatory Landscape for Compliant Lab Weighing

Performance Checks for Compliance with Pharmacopeia requirements

Generic operating procedure for a performance check according to USP 41, Ph.Eur. 2.1.7, JP 9.62 and ChP 9032

Download our detailed USP 41, Ph.Eur. 2.1.7, JP 9.62 and ChP 9032 generic operating procedure.

United States Pharmacopeia 1251 - Weighing on an Analytical Balance

USP general chapter 1251 offers best practices for laboratory weighing, including selecting the right balance for accuracy, proper placement and installation, calibration and verification, routine testing and maintenance, correct weighing techniques, and documentation and traceability of procedures.

Download the Infographic for an optimal use of your lab balances in Pharma industry

European Pharmacopeia General Chapter 2.1.7 – Balances for Analytical Purposes

EP 2.1.7 provides comprehensive guidelines for the use and maintenance of analytical balances, covering principles of mass determination, installation considerations, and the use of appropriate weighing vessels. It emphasizes the importance of calibration, repeatability, sensitivity, and adherence to the minimum weight requirement in performance checks.

Download a detailed EP 2.1.7 compliance guide

EURAMET Calibration Guide No. 18 – Guidelines on the calibration of Non-Automatic Weighing Instruments

The EURAMET cg-18 guide details the calibration of non-automatic weighing instruments to ensure consistent and recognized results across laboratories. It includes calibration elements, test loads, measurement methods, uncertainty, and certificate preparation, with appendices on air buoyancy, convection effects, and minimum weight. Calibration is done over to maintain high standards in mass measurement.

Download this white paper to learn about the calibration guideline, measurements carried out as part of the calibration process and Sartorius specifications

Japanese Pharmacopeia Chapter 9.62 - Measuring Instruments, Appliances

Chapter 9.62 of the Japanese Pharmacopoeia has been extensively revised and published in June 2024to include detailed requirements for the calibration, repeatability, and accuracy of balances, emphasizing the importance of the smallest net weight. It mandates that balances be calibrated to ensure traceability to the SI and that repeatability checks confirm the minimum weight is smaller than the smallest net weight. Additionally, the chapter requires periodic accuracy checks to ensure sensitivity errors are within acceptable limits.

Download FAQ

Uniformity of dosage unit described in EP 2.9.40 - USP <905> - JP 6.02 and harmonized by ICH guidance Q4B annex 6

EP 2.9.40, USP <905>, and JP 6.02 describe the test for drug content uniformity in dosage units such as tablets and capsules in pharmaceutical or nutraceutical quality control. This test ensures that each individual unit of a drug product contains the intended amount of active ingredient within an acceptable range. Accurate weighing is crucial in these procedures, as it directly impacts the assessment of dosage uniformity, including criteria for acceptance based on statistical sampling and analysis.

Download the application highlight to learn how weight testing can be easily performed using the Cubis® II MCA balance and QApp tablet check.

Residue of ignition described in EP 2.4.14 - USP <281> - JP 2.44 and harmonized by ICH guidance Q4B annex 1

The residue on ignition - or sulfated ash - test described in EP 2.4.14, USP <281>, and JP 2.44 determines the amount of residual substance remaining after a sample is ignited, which is crucial for assessing the purity and quality of pharmaceutical substances. Accurate weighing by difference is essential in this procedure, as it is directly involved in the determination of the residue amount.

Download this informative application highlight to learn more about the role Cubis® II balances streamline the test procedure.

Loss on drying described in USP <731> - EP 2.2.32 - JP 2.41

The loss on drying (LOD) test, described in USP <731>, EP 2.2.32, and JP 2.41 measures the amount of volatile matter, such as water, in a sample. This test is crucial for determining the moisture content of pharmaceutical substances, which can affect their stability, efficacy, and shelf life. Accurate differential weighing is essential as it directly impacts the precise determination of the moisture content.

In the Cubis® II application, administrators can select USP or PhEur test procedures and choose the sample type—tablet or capsule. This determines how the software evaluates pass or fail based on weight differences. Download the application note to learn more.

Electronic records and data integrity as described in 21CFR Part 11, EU Annex 11 or ALCOA principle

21 CFR Part 11, EU Annex 11, and the ALCOA principles are essential for ensuring compliance in electronic data management within the pharmaceutical industry. These regulations outline Good Manufacturing Practice (GMP) protocols, including the use of electronic signatures, data integrity, and system validation, to ensure that electronic records are trustworthy and reliable.

Download the infographic for an overview of key terms and definitions, points of compliance, and ways to achieve quality control and data integrity.

Certified and accredited services for lab weighing instruments

Sartorius Services ensure lab balances meet GLP/GMP standards, providing audit security and comprehensive documentation. Our risk-based IQ/OQ qualification ensures compliance and peace of mind. Regular maintenance contracts enhance process safety, extend instrument life, and ensure reliable results. Calibration services guarantee accuracy, regulatory compliance, and traceability, with certificates meeting ISO/IEC 17025, USP, and European Pharmacopeia standards.

Find the lab weighing service you need.

Ensuring Data Integrity: Connected Solutions

Data Integrity is a necessity in scientific research and pharmaceutical manufacturing. It is essential for reliable results, ensures compliance, product quality, and patient safety. In order to stay compliant, modern lab equipment is designed to simplify data integrity compliance by automation. Explore this infographic to understand the importance of data integrity, the FDA’s focus on data integrity violations, and ultimately Sartorius connected solutions that help ensure compliance.

Get the Infographic Now

Audit Preparedness with Cubis® II Balances

Many analytical techniques involve weighing steps, where errors can occur. These mistakes can have significant and cumulative effects, potentially leading to invalidation of release tests, cross-contamination, or high analytical uncertainties. Recognizing the importance of accurate weighing, pharmacopoeias provide guidance on planning, verification, and protocol.

This guide helps you understand how the Cubis® II balances secure your daily weighing reliability and back you up for internal or external audits.

Access the Audit Preparedness with Cubis® II Balances eBook

Instrument Qualification in Regulated Industries

Watch this video to understand how compliance with GMP requirements necessitates equipment qualification (IQ | OQ). It provides general information on Design Qualification (DQ), Installation Qualification (IQ), Operational Qualification (OQ), and Performance Qualification (PQ), while discussing the Risk-Based Approach, digital IQ/OQ, and maintaining instruments in a qualified state.

Cubis® III and Cubis® II - Pharma Compliant by Design

Get the White Paper

Pharma Compliant Weighing Resources

 Cubis® III laboratory balance showcased in a modern lab environment - black background
Webinar

Beyond Digitization to AI-Ready Instruments

On-demand webinar on digital transformation, data integrity, connected workflows, and AI-ready lab instruments.

Cubis II laboratory balance showing USP41 and USP1251 - regulartory capabilities
eBook

USP 41 & 1251 Lab Balance Compliance Guide

Learn how QC labs meet USP weighing requirements with confidence, traceability, and audit-ready workflows.

Cubis® III laboratory balance showcased in a modern lab environment - gray background
eBook

Securing Accuracy in Pharma QC

The Strategic Role of Advanced Lab Balances

Lab Balance Powder Weighing Boat Application Image Close
Webinar

Weighing Masterclass: Understanding Measurement Uncertainty 

Weighing and Sample Management Solutions for Pharmaceutical Quality Control

Yellow rocket taking off from a laptop, startup and technology concept, black background.
Webinar

You're Now Connected: Prepare Your Lab for the Future

This webinar will explore the crucial roles of data integrity and laboratory connectivity in the lab.

Challenges In Testing of Dosing Accuracy According to IEC
Application Note

Dosing Accuracy Testing According to IEC 60601-2-24 And AAMI TIR-101

Discover the precision of Sartorius Cubis® II balances in ensuring accurate dosing rates for infusion pumps

Inspecting Cubis instrument
White Paper

Best Practices Guide: Lab Weighing

Discover practical guidance on weighing in the lab, including calibration, accreditation, legal metrology and correct weighing.

Sartorius Instrument Services
Technical Note

Lab Weighing: Generic Operating Procedures for Routine Testing

Our series of Generic Operating Procedures provides valuable information about routine testing of lab balances. Discover more!

eBook: Cubis® II MCA 21 CFR Part 11 Compliance Checklist
eBook

Cubis® II MCA 21 CFR Part 11 Compliance Checklist

Detailed insights into FDA’s 21 CFR Part 11 standards for electronic records and electronic signatures.

Use of Laboratory Balances in the Pharmaceutical Industry cover
White Paper

Use of Laboratory Balances in the Pharmaceutical Industry

Our white paper summarizes USP Chapters 41 and 1251 and the new European Pharmacopoeia Chapter 2.1.7.

Application Note

Formulation QApps Using a Database With Cubis®II

This is the use case description for the QApps Formulation in multiple vessels and Formulation in single vessel.

Application Note

Net Weight Control of Prepackaged Goods and Drugs

Learn more about Sartorius software packages for Cubis® II balances and how they can help you meet quality and safety regulations.

Measurement Inaccuracy of Rapid Moisture Analyzers as a Function of Sample Quantity
Application Note

Measurement Inaccuracy of Rapid Moisture Analyzers

Control of moisture content helps to prevent microbial growth and ensures that bulk powders flow properly.

Discover How Omnis and Cubis II Can Help You With Your Karl Fisher Titration Method!

Seamless Integration of Cubis® II into Metrohm OMNIS Analytical Software System

Discover OMNIS

View Webinar


Request a Quote, Demo, or More Information

What other areas are you interested in? (select all that apply)

Get in Touch With an Expert