Mixed Lymphocyte Reaction (MLR)

Immune checkpoints are regulatory signals that can act as ‘on and off-switches’ for T cells. Checkpoints are engaged when a T cell binds to an antigen presenting cell (APC), such as a tumor cell or dendritic cell (DC). Immunotherapies, termed checkpoint inhibitors, have been developed to target this synapse between T cells and APCs, specifically to block the immune checkpoints that usually ‘switch off’ T cells. This leads to enhanced T cell activation and increased anti-tumor response. Checkpoint inhibitor therapies currently approved for cancer treatment include anti-PD-1, anti-PD-L1 and anti-CTLA4 monoclonal antibodies, with more in active development.

MLR is an in vitro assay in which immune cells from two individuals are co-cultured together to trigger the ‘non-self’ recognition required for immune checkpoint regulation. The assay can be used to investigate the potential therapeutics by evaluating their ability to potentiate T cell response. Traditional techniques for measuring T cell response in MLR often:

  • Require a separate assay for cytokines (e.g. ELISA), proliferation and marker expression (e.g. traditional flow cytometry)
  • Use instrumentation with low-throughput acquisition that necessitate large sample volumes
  • Necessitate manual analysis of data which is compiled from multiple sources e.g. plate reader and ELISA
  • Are laborious and time-consuming, requiring steps such as protocol optimization, fixation and repetitive washes

Here we demonstrate a simple, robust workflow for measuring T cell response in MLR using the iQue® High-Throughput Screening (HTS) Cytometer and associated suite of validated reagents. The user can choose to combine one or more iQue® kits, including the iQue® Human T Cell Activation Kit and iQue Qbeads® Human Inflammation Panel Kit, to generate a range of outputs as desired. Enhance your screening and profiling studies by combining the power of the iQue® and the automated, integrated analysis for instantaneous pharmacological readouts for the effects of novel immunotherapies on T cell response

 

Request More Info

Application

Assay Concept

Figure 1. Illustration of the mixed lymphocyte reaction (MLR) assay principles

In one-way MLR, isolated CD4+ T cells from one donor are combined with DCs from another donor, resulting in uni-directional T cell activation. Two way MLR is a co-culture of PBMCs from two different donors, resulting in bi-directional activation of T cells from both donors. In both assay set ups, T cell activation is dependent on an allogenic reaction with the MHC molecules on the DCs recognized as ‘non-self’. This  relies on differences in the donors’ HLA haplotypes. The induction of T cell activation response by allogenic MHCs can be enhanced with addition of checkpoint inhibitor drugs, e.g. anti-PD-1 and anti-CTLA4 monoclonal antibodies. Analysis of T cell response from one or two-way MLR can be performed using the iQue® 3 and a range of associated kits, including the iQue® Human T Cell Activation Kit, the iQue Qbeads® Human Inflammation Panel Kit and a Custom iQue Qbeads® PlexScreen Kit. These kits can be used alone or in combination to measure proliferation, marker expression and cytokine release as required to suit user needs, all from a single assay plate.

Key Advantages

Quantify surface marker & cytokine expression simultaneously

Multiplexed immunophenotyping and effector cytokine concentration read from a single well


Figure 2.  Measure checkpoint inhibitor drug induced cytokine release and marker expression in a single well

DCs were thawed and activated overnight (with IL-4, granzyme B and LPS) prior to plating at 40K/well in a 96 well plate. CD4+ T cells labeled with B/Green Encoding Dye were added at a 3:1 T cell-to-DC  ratio. A range of concentrations of checkpoint inhibitor drug Pembrolizumab (an anti-PD-1 monoclonal antibody) were added to enhance T cell activation. Cytokine samples were analyzed on day 2 and 6.  Marker expression was analyzed at assay endpoint (day 6). Samples were analyzed for (A) IFNγ  release, (B) TNFα release and (C) CD25 expression using the iQue® Human T Cell Activation Kit and the iQue® 3 HTS platform.

Obtain quantitative data

Generate measurements of T cell response suitable for pharmacological analysis


Figure 3. Quantify drug induced T cell response with automatic EC50 calculation by iQue Forecyt®

DCs were seeded (40K/well) with encoded CD4+ T cells (3:1 T cell-to-DC  ratio) and treated with Pembrolizumab. 10 µL samples were analyzed on Days 2 and 6 using the iQue Qbeads® Human Inflammation Panel Kit.  (A) Heat map showing IL-2 (pg/mL) release per well. Control wells contained T cells and DCs in the absence of drug. (B-E) Curves highlight temporal and Pembrolizumab concentration dependent release of inflammatory cytokine. On Day 2, EC50 for IL-2 release in response to Pembrolizumab was 0.53 µg/mL, whilst by Day 6 all IL-2 production has ceased. IL-6, CCL2 and CCL3 levels all increased from day 2 to 6, with day 6 EC50 values for CCL2 and CCL3 release very similar at 0.98 and 1.0 µg/mL, respectively.

Perform high-throughput analysis

Facilitate screening and profiling studies with rapid quantification of markers and cytokines in 96 or 384-well plates.


Figure 4. Rapidly profile checkpoint inhibitor induced effects on cytokine release across multiple PBMC donor pairs using a 384 well assay format 

PBMCs (80K/well) from multiple donors were seeded alone (single donor controls) or in combination (8 donor pairs in total). Cells were treated with several concentrations of an anti-CTLA4 checkpoint inhibitor antibody. Mixed PBMCs with PHA and MMC were included as positive and negative controls, respectively. After 3 days, samples were analyzed for cytokine concentrations using IFNγ iQue Qbeads® and concentrations calculated using a standard curve. (A) Heat map highlights differences in anti-CTLA4 induced IFNγ release between PBMC donor pairs. (B) Bar chart shows mixed PBMCs consistently released more IFNγ than single donor controls. This was enhanced with addition of 17 ng/mL anti-CTLA4. (C) Representative concentration response curve showing donor pair 7 response to anti-CTLA4 (EC50 = 6.5 ng/mL)

Maximize your productivity

Reduce your time to answer with real time data analysis and novel visualization tools


Figure 5.  Pre-set gating and automated data analysis by iQue Forecyt® provides instantaneous readouts for T cell activation 

CD4+ T cells from two different donors were co-cultured separately with DCs from a single donor at a range of T:DC ratios. Each T cell donor had a different degree of mismatch with the DC donor’s HLA alleles. Donor 1 T cells were more similar in HLA profile to the DC donor with only 3/8 mismatched alleles (2 x HLA-A, -B, -C and -DR alleles) compared to the donor 2 T cells which had 7/8 mismatched alleles. Controls included T cells cultured alone (negative) or with Dynabeads or Immunocult (positive). Analysis was performed using the iQue® Human T Cell Activation Kit. (A) Plate view shows well by well differences in CD25 expression within the CD4+ population. T cell activation increases with decreasing T:DC ratio and is greater on donor 2 T cells. This is expected as the high mismatch in HLA alleles is promoting recognition of ‘non-self’ cells. (B) and (C) Contour plots show % CD25 positive T cells from donor 1 and donor 2 (3:1 T:DC ratio). (D) Bar chart quantifying % CD25 cells in the CD4+ population.

MLR Assay Workflow

Figure 6. Protocol for one-way and two-way MLR assay on iQue® 3 HTS platform

Choose from a range of cell and bead based kits to define analysis parameters based on user needs. This assay was validated using the iQue® Human T Cell Activation Kit, the iQue Qbeads® Human Inflammation Panel Kit and a Custom iQue Qbeads® PlexScreen Kit.

Ordering Information

iQue® Human T Cell Activation Kit
Platform: Compatible with iQue® 3/ iQue® Screener Plus - VBR Configuration
Available SizesCatalog Numbers
1 x 96 well90560
1 x 384 wells90562
iQue Qbeads® Human Inflammation Panel Kit
Platform: Compatible with iQue® 3/ iQue® Screener Plus – BR and VBR Configurations
Available SizesCatalog Numbers
1 x 384 wells97097
iQue Qbeads® PlexScreen: Human Secreted Proteins 
Cytokine 
ChemokineTNFInterleukin
CCL2 (MCP-1)TNF (TNFα)IL-1αIL-10
CCL3 (MIP-1α)sCD154 (sCD40 Ligand)IL-1βIL-11
CCL5 (RANTES)CD178 (Fas Ligand)IL-2IL-12/IL-23(p40)
CCL11 (Eotaxin)TNFβ (LT-α/TNFSF1)IL-3IL-12(p70)
CD14 IL-4IL-13
CXCL9 (MIG) IL-5IL-17A
CXCL10 (IP-10) IL-6IL-17F
CXCL11 (I-TAC) IL-7IL-21
CX3CL1 (Fractalkine) IL-8IFN-α
  IL-9IFN-γ
ReceptorAdhesion MoleculeGrowth FactorEnzyme
CD121a (IL-1 RI)CD54 (ICAM-1)AngiogeninGranzyme A
CD121b (IL-1 RII)CD62E (E-Selectin)Basic FGFGranzyme B
TNFRICD62L (L-Selectin)CSF2 (GM-CSF) 
TNFRIICD62P (P-Selectin)CSF3 (G-CSF) 
 CD106 (VCAM-1)VEGF 

 

Resources

Literature and Documentation

Brochure

iQue® High-Throughput Screening (HTS) by Cytometry

Truly Fast. Simply Effortless.  

Webinar

On-Demand Webinar: Evaluation of Checkpoint Inhibitor Therapies using...

Product Guide

Product Guide

T Cell Activation Cell and Cytokine Profiling Kit

Product Guide

Product Guide

Human QBeads Inflammation Panel Kit

Application Note

Application Note

Utilizing Mixed Lymphocyte Reaction (MLR) to Evaluate Checkpoint Inhibitor Therapies

Poster

Poster: Evaluation of checkpoint inhibitor therapies using a MLR assay

An assay for quantification of T cell response in MLR in 96- or 384-well plates using the iQue® Cytometry Platform.

Request a Quote, Demo, or More Information

What other areas are you interested in? (select all that apply)

Request a Demo, Literature, or More Information