On-Demand Webinar: Evaluation of Checkpoint Inhibitor Therapies using a Mixed Lymphocyte Reaction (MLR) Assay

Overview

Immune checkpoints are signaling molecules which control the synapse between T cells and antigen presenting cells (APCs).

Checkpoint inhibitor therapies target and inhibit the signals that ‘switch off’ T cells, leading to an upregulation of T cell activation and tumor cell killing.

The mixed lymphocyte reaction (MLR) mimics the T cell and APC synapse by co-culturing immune cells from two individuals. MLR is used as a model, to explore the effects of checkpoint inhibitor drugs in vitro; facilitating biological research applications and drug discovery processes.

Register to Watch On Demand

Key webinar discussion topics include:
   

  1. The impact of checkpoint inhibitor therapeutics on inflammatory cytokine release
  2. How the iQue® Advanced Flow Cytometry Platform and associated reagent kits can be used to quantify T cell response in MLR
  3. The use of the iQue® MLR assay to generate pharmacological outputs for checkpoint inhibitor induced T cell activation

Webinar Speaker

Kirsty McBain
Associate Scientist
iQue® Applications Group, Sartorius

Kirsty McBain is an Associate Scientist in the iQue® Applications Group, part of the European based BioAnalytics at Sartorius, where she is involved in the research and development of novel applications.

Kirsty’s efforts are focused on the iQue® 3 advanced flow cytometry platform where she has supported a number of the immuno-oncology campaigns that are used to exemplify how Sartorius technology can be applied to the drug discovery process. Kirsty obtained a master’s degree in Biochemistry at the University of Bristol before joining Sartorius in 2019.

Request a Quote, Demo, or More Information

What other areas are you interested in? (select all that apply)

Register to watch the on-demand webinar

icon-shopping-cart
Ready to Buy?