Are You Testing Your Medical Devices with Endotoxin-Free Pipette Tips?
Guarantee Consistently Reliable Endotoxin Testing Results with Purity-Certified Pipette Tips
Endotoxins can be a risk to patient safety. Even a low endotoxin concentration in the blood stream can produce inflammation in the human body; therefore, preventing endotoxin exposure to your patients is important.
To prevent patient exposure to endotoxins, frequent and reliable testing for endotoxin levels on medical devices is required. The LAL method, is one such reliable test method used to guarantee patient safety and the risk-free use of medical devices. An alternative method is the recombinant Factor C (rFC) assay that is completely animal-free.
Depending on the intended use, US Pharmacopeia (USP) chapter 161 states that all final sterilized products, such as medical devices, must be tested for endotoxin levels, usually by batch, and describes endotoxin release limits as follows for products that come into contact with
- the cardiovascular system or they lymphatic system -- 0.5 EU/mL or 20 EU/device
- the cerebrospinal fluid -- 0.06 EU/mL or 2.15 EU/device
New Application Note: Are You GLP/GMP Compliant When it Comes to pipetting?
Are you following methods for current Good Laboratory Practice (cGLP) or current Good Manufacturing Practice (cGMP)?
Our new application note introduces tools and principles that can help you with these demanding requirements, especially when it comes to your pipetting practices. A pipette is a precision measuring apparatus that has a significant influence on your lab results, but it can also be your companion in ensuring compliance.
Download Application Note
Application Note: How To Avoid Contamination in Pipetting
Preventing contamination in pipetting is paramount to achieving reliable results. It requires identification of the potential contamination mechanism in order that they can all be addressed. This paper addresses the three contamination types that originate from pipetting: Pipette-to-sample contamination, sample-to-pipette contamination, and sample-to-sample contamination.
Pipetting in Endotoxin Testing
The Effects of Endotoxin Contamination
Did you know that endotoxin contamination of lab consumables can influence your assay results?
Pipetting is an integral part of the endotoxin testing workflow for medical devices. To minimize potential sources of endotoxin contamination, use endotoxin-free consumables, such as pipette tips, within the testing workflow.
Pipette tips that are not manufactured in an automated process can contain endotoxins that cause false endotoxin test results and contaminate samples. Highly automated processes minimize human contact with the raw materials and the final product during the entire manufacturing process, thus minimize endotoxin contamination risk. Sartorius pipette tips are manufactured in a highly automated process and in a clean room environment, and go through a lot-specific testing with an endotoxin test limit of <0.005 EU/ml, which is 100 times lower than the regulatory requirement. All Sartorius endotoxin-free tips are supplied with purity certificates. Before purchasing endotoxin-free pipette tips, check the test limits for endotoxin-free certification of pipette tips to ensure they are low enough to match your test needs.
The Effects of Pipetting Technique
Pipetting errors are a common source of variance in testing procedures. For example, variance in endotoxin testing standard curves can have a deleterious effect on the reliability of test results.
The pre-programmable protocols of electronic pipettes can reduce user error in pipetting steps. Using the same manufacturer’s pipette tips with your pipettes ensures the perfect fit, thus reducing leakage, accuracy, and precision performance promised for the pipette.
To ensure the most reliable results, take care of your pipettes and calibrate them regularly. Sartorius also offers certified and accredited pipette calibration services.
Purity Certified Pipette Tips and Accurate and Precise Pipettes
Endotoxin-free Pipette Tips
Sartorius pipette tips are tested and certified to be endotoxin free, so they fit into workflows of medical device QC labs. Sartorius manufactures pipette tips according to ISO 14644-1 in a certified ISO 8 cleanroom environment to maintain the highest quality and purity standards. Only the best plastic materials are selected, and our automated manufacturing process is strictly controlled from beginning to end in line with GMP to reliably prevent contamination by human contact. An independent laboratory checks every tip lot to ensure the absence of DNase, RNase, and endotoxins with a test limit of 100 times lower than the regulatory requirement.
Optifit Pipette Tips
Sartorius Optifit tips ensure perfect fitting and leak-tight sealing on Sartorius pipettes for maximum pipetting accuracy and reproducibility. The color coding of the tip trays enable you to easily match them to their color-coded Sartorius pipette.
- Tips are packed in single tray racks with an air-tight wrapping to protect the tips from endotoxins
- DNase-, RNase-, and endotoxin-free production processes reliably protect your sample from contamination
- The highest quality pure polypropylene is used as raw material to ensure material purity
- A lot-specific purity certificate is supplied with tips
Tacta® Mechanical Pipette – Perfectly Balanced
Tacta® is the new premium mechanical pipette with superb comfort and reliability. Tacta® makes pipetting effortless and safe, while producing accurate and reliable results time after time.
Experience the benefits of Tacta®:
- Fully autoclavable pipette for best contamination control
- Reliable results, even over lengthy pipetting periods
- Controlled and smooth tip ejection with the new Sartorius Optiject technology
- Comfortable to hold due to the ergonomically designed handle
- The unique Sartorius Optilock system provides flexibility for volume adjustment and locking
- Calibration adjustment to provide accurate results for various liquid types
- Easy to clean, with only three parts to disassemble
Picus® Nxt Electronic Pipette – Highly Sophisticated and Ergonomic
Picus® Nxt is the lightest and smallest electronic pipette on the market. Its ergonomic design, fully electronic operation, and advanced functionalities ensure an easy and comfortable pipetting experience.
Experience the benefits of Picus® Nxt:
- Fully electronic operations guarantee accurate and precise pipetting results, regardless of user skill level
- The extensive range of pipetting modes, from diluting and titrating to serial dispensing, makes pipetting tasks quick and easy
- User-definable protocols speed up routine pipetting sequences and add reliability on standard curve pipetting
- Certificate of accredited 3-point calibration (ISO 17025 and ISO 8655) conforms to the strictest regulations
- Maintenance and calibration reminders alert you when service is required
- Possibility to lock the pipette and prevent the use, for instance, in case of contamination
- Uniquely lightweight (weighs only 100 grams) and streamlined design for effortless pipetting
Accurate and Precise Pipettes
Sartorius pipettes are a perfect choice for endotoxin testing of medical devices, as they have been designed with cleanliness, accuracy, and ease-of-use in mind. The pipettes are easy to clean with the lower parts of the pipette being easy to remove. They are also easy to calibrate and are equipped with a volume lock to ensure that your dispensing volume is as intended. In addition, the Picus® Nxt has a calibration reminder feature so that you don’t forget your next calibration expiry date.
Resources
Enjoy these resources to help you find information-rich solutions.
Practical Selection Guide
How to set up Pipetting Quality Control Program for Your Lab?