When Time Is the Most Critical Resource: How an Ambitious Dad and Sartorius Aim to Advance Gene Therapy for CDKL5 

Pioneers
Mar 05, 2026  |  5 min read

What if a single gene changes everything? For eight-year-old Reyna, a rare mutation means daily seizures and developmental challenges. Her father, Jainu Jogani, refused to wait for a cure. Instead, together with partners like Sartorius, he aims to advance a gene therapy for CDKL5 Deficiency Disorder. Explore how determination, innovation, and collaboration are creating hope for Reyna and children worldwide.

This article is posted on Sartorius Blog.

When Jainu Jogani’s daughter Reyna was 20 days old, she began showing unusual hand and eye movements. Within weeks, EEG and genetic testing confirmed a diagnosis: CDKL5 Deficiency Disorder (CDD) – a rare disease affecting roughly 1 in 40,000 children.

Reyna, now eight years old, lives with seizures, developmental delays and complex medical needs. “Some children have up to 40 seizures a day,” Jainu explains. “There is no cure. Most care is supportive.”

 

We chose to not take a backseat and wait for someone to deliver, but we are working on making this happen for our children.

 

 

Rather than waiting for traditional drug development timelines, Jainu, a biomedical engineer by training, co-founded Child’s Cure Genetic Research to pursue therapeutic approaches. “Programs initiated by large biotech companies were often deprioritized. We chose to not take a backseat and wait for someone to deliver, but we are working on making this happen for our children.” 

In April 2024, the organization launched its own lean gene therapy initiative together with a Contract Development and Manufacturing Organization in the United States, trying to target the root cause of CDD: the missing or dysfunctional CDKL5 protein.

Addressing the Disease at Its Origin

CDD is caused by mutations in the CDKL5 gene on the X chromosome. Without sufficient functional CDKL5 protein, neuronal signaling is disrupted, leading to early-onset, intractable epilepsy and profound developmental impairment.Existing care largely focuses on managing symptoms, particularly epilepsy, rather than correcting the underlying genetic defect.

Jainu’s ambition: Advancing an AAV9-based gene therapy designed to reintroduce a functional copy of the CDKL5 gene into brain cells. The viral vector — a modified, non-replicating capsid — delivers DNA into neurons, enabling cells to produce the missing protein.

 

Shruti and Jainu Jogani with their daughter Reyna

 

Preclinical studies are ongoing. The next milestone is IND submission in the U.S., following toxicology studies.

Parallel approaches, including antisense strategies, drug repurposing targeting CDKL2, enzyme replacement research, and a newly initiated mRNA program, complement the effort. But gene replacement remains central because it addresses the disorder at its genetic root.

“Time is of the essence,” Jainu says. “We are focused on delivering what is absolutely necessary to move to clinic — nothing exploratory that slows us down.”

From Mission to Manufacturing: A Collaborative Effort

Scaling AAV gene therapy from concept to clinical material requires advanced viral vector manufacturing – a field where Sartorius technologies can make a difference.

Mayra Mancia, Commercial Development Manager at Sartorius, recalls the first conversation with Jainu in early 2025. “It’s rare to see a parent this deeply involved in therapeutic development. We understood that in a parent-led program like this, resources are limited and timelines critical — not in abstract terms, but personally.” 

 

Sartorius understood the urgency from the very beginning and helped deliver the material that is needed to ensure that our timelines for material manufacturing are met.

 

The Sartorius team made sure to facilitate the orders as fast as possible, navigating administrative setup, aligning production schedules and ensuring that materials were delivered when the clinical programs depended on them. 

“We are very grateful to the team,” Jainu says, “Sartorius understood the urgency from the very beginning and helped deliver the material that is needed to ensure that our timelines for material manufacturing are met. They are playing a significant role in the project.”

Sartorius Products in use:

Sartocon® Hydrosart® cassettes

Tangential flow filtration for concentration and buffer exchange of AAV vectors

Sartoflow® Systems 

Scalable control platforms supporting filtration workflows

CIMmultus® Monolith Columns

Chromatography Enabling Efficient Capture and Polishing of Viral Particles

Sartoclear® Filters

Clarification of Harvest Material Prior to Purification

“Today, a wide variety of our filtration and purification portfolio for gene therapies is used in the process,” Mayra continues. “We are all in this together with Jainu and Reyna and proud to be part of the solution in accelerating the manufacture of this AAV therapy.”

Future upstream application in the process include:

Biostat STR® Generation 3

Flexsafe® 2D & 3D Single-Use Bags for Storage and Shipping

BioWelder TC  

The Biowelder® TC is an automated device for making sterile connections between thermoplastic elastomer tubing elements.

Making Progress One Milestone at a Time

For Jainu, progress is measured in milestones rather than endpoints — completing preclinical studies, preparing regulatory submissions, building partnerships that expand capability.

“We are in contact with the FDA and getting closer to submitting our work as an Investigational Drug and to the Institutional Review Board of the University of California in San Francisco. Once we get approval, we can start treating human patients,” he explains.

His objective remains direct and personal: Bring a treatment option to Reyna and other children affected by CDD. “We are open to collaboration with organizations that can accelerate this path,” he says. “If what we develop helps my daughter, we want it to become available to others. Every decision we make is guided by that urgency — and by the belief that meaningful progress comes when people across the ecosystem work together.”

Understanding AAV and CDKL5:

icon-virus-a

What Is an AAV?

Adeno-associated viruses (AAVs) are engineered, non-replicating viral shells used to deliver therapeutic genes into cells. In AAV9-based therapies, the vector carries a functional DNA sequence into target tissues — such as neurons — enabling production of a missing protein. The virus itself does not replicate and is modified to minimize safety risks.

icon-gene-modified-cell-therapy

What is CDKL5 Deficiency Disorder?

CDKL5 Deficiency Disorder is a rare genetic neurological condition that affects an estimated 1 in 40,000–60,000 births worldwide. It is caused by mutations in the CDKL5 gene on the X chromosome, which encodes a protein essential for neuronal development and signaling. Without functional CDKL5, infants can experience seizures and developmental delays affecting movement, cognition, communication, and vision as well as feeding difficulties, sleep disruption, and respiratory issues.

Related Stories

Pioneers
Nov 18, 2025 | 7 min read

“It’s just like Lego – but with molecules.” 

Meet Alengo, Segment Marketing Manager, at Sartorius' GMP facility in Illkirch. Together with her team she helps customers bring cell and gene therapies to life.  

Pioneers
Oct 08, 2024 | 5 min read

30 Years of Pioneering Work for Cell and Gene Therapies

Felicia Rosenthal is a true pioneer in the field of cell and gene therapies. In this interview, she shares insights from her journey in CGTs and talks about Sartorius' role in advancing new therapies.

Better Health
Aug 22, 2024 | 4 min read

The Rise of Biologics: From Early Milestones to Major Breakthroughs

Biologics are transforming the lives of millions of patients. Explore the rise of the most effective treatments of their time and the need for faster, more efficient drug discovery and manufacturing.

icon-e-mail
Media Contact