Vaccine Development Platforms

Strategies for vaccine manufacturing have evolved in the last couple of decades. Emerging methodologies such as recombinant production complement more traditional techniques. Traditional methods, such as the production of inactivated or live attenuated vaccines, have demonstrated efficiency for several diseases but can be limiting for others. Recombinant strategies have unlocked the potential to develop vaccines for unmet indications. At present, there are multiple different platforms available for vaccine developers:

  • A well-proven platform such as inactivated and live attenuated vaccines
  • Recombinant protein vaccines, or recombinant subunit vaccines, allowing the production of an antigen  
  • Viral vector vaccines and nucleic acid vaccines, including mRNA and DNA plasmids, allowing the transportation of a genetic sequence in the patient body for in vivo production of the antigen

As a partner of the vaccine industry, we at Sartorius are committed to providing solutions for developing vaccines using these platforms.

Webinar

Accelerating Viral Vector Characterization: An Industry Case Study

Explore how CDMOs can overcome process bottlenecks, improve efficiency, and support flexible, scalable manufacturing with proven technologies. 

Register Here

Viral Vaccines

Viral vaccines include inactivated viral vaccines and live-attenuated viral vaccines. Both rely on a traditional approach i.e.; the disease-causing virus is identified, produced in a bioreactor, and purified. This type of strategy has been used for many diseases with success, and most of the current vaccines against viral diseases use this strategy.

We, at Sartorius, understand the needs of vaccine developers and producers working with viral vaccines and have developed a dedicated toolbox of solutions to face the challenges viral vaccines production.

Learn More

Viral Vector Vaccines

Viral vector-based vaccines constitute a promising part of the biopharmaceutical pipeline, addressing many unmet indications. To leverage the full potential of viral vector-based vaccine development, many vaccine developers are looking to innovative technologies to support more productive, intensified, and flexible processes.

We invite you to discover the Sartorius toolbox of technologies dedicated to the production and purification of viral vectors. As you explore our generic process overviews for enveloped vectors, non-enveloped vectors, and commonly used vectors, you can click on each step to reveal the challenges that manufacturers face when working with viral vector-based vaccines.

Learn More

mRNA Vaccines and pDNA

Nucleic acid vaccines have the potential to disrupt the vaccine industry. These vaccines consist of a plasmid DNA or a messenger RNA molecule coding for a disease-specific antigen that is translated into a protein once injected into a patient.

Both processes are simple, cost-effective, and quick to develop and produce in comparison to traditional vaccine processes. However, mRNA vaccines are cell-free processes are relatively new, and this requires solutions tailored to the needs of this platform.

We invite you to discover Sartorius' range of solutions at each step of mRNA and pDNA production.

Learn More

Recombinant Protein Vaccines

Recombinant protein vaccines, also called recombinant subunit, consist of viral or bacterial antigen produced using recombinant DNA technology. This type of vaccine does not require the production of the entire pathogen and is therefore considered safe, and is well established in the industry.

The challenge to support recombinant protein vaccine manufacturing relies on the diversity of expression systems that can be used: bacteria, yeasts, insect cells, mammalian cells, or even plants. The antigen can be a simple protein or a more complex structure, such as a virus-like particle or a nanoparticle.

Learn More

icon-webcast

mRNA Production and Purification in the Aftermath of Pandemic

This webinar features an exclusive panel discussion where the speakers lay out their vision for truly optimized next-gen mRNA processes.

Watch Webinar Online
icon-webcast

Integrated Production Process of Highly Purified mRNA

Learn how a new, optimized purification approach for mRNA provides higher yields and lower costs

Watch Webinar Online

Consult Our Experts

Consult Our Experts

Discover further Sartorius Platforms for Biomanufacturing

Scalable Single-Use Toolbox for Your mAb Process Platform

Regenerative Medicine

Antibody Drug Conjugates

Streamline your ADC processes with scalable solutions addressing key challenges in cytotoxicity, chemical compatibility, and process control.