Cell Line Characterization Services

Generating master and working cell banks in compliance with GMP requires specialized expertise in manufacturing, biosafety, and characterization testing to ensure a robust, safe supply of cells for manufacturing processes.

Sartorius provides comprehensive services to characterize mammalian cell banks in line with ICH guidelines. All testing follows global pharmacopeial standards and is conducted in facilities accredited by the U.S. FDA, EMA, and MHRA.

Ready-to-use quality control plans support testing and release of:

  • Research cell banks (RCBs)
  • Master cell banks (MCBs)
  • Working cell banks (WCBs)
  • End-of-production cell banks (EoPCBs)

Consult Our Experts

icon-industrial-microbiology

Integrated cGMP biosafety and cell characterization services

Sartorius has extensive experience in the characterization of cell banks used to produce biologic drugs, including protein-based and viral-based therapies. Our quality control testing plans meet requirements for mammalian cell bank release and are designed to align with ICH Q5A regulations, using assays validated to GMP standards. Ready-to-use testing schemes may be added to existing drug development risk strategies or customized to meet the needs of specific programs.

Biosafety testing and cell line characterization packages

Stringent cGMP biosafety testing is required for all cell banks to confirm the absence of contaminants, including bacteria, mycoplasma, and viruses.

Cell bank testing regulations can be extensive. Sartorius has developed cGMP platform methods for cell bank testing that align with ICH Q5 guidelines.

 

Research cell bank testing

The process of cell banking begins with a research cell bank (RCB), which is used to generate a master cell bank (MCB).

Before this step, the RCB must be certified, at a minimum, as sterile, mycoplasma-free, and identity-assured. The manufacturer may also request a broad-spectrum cell-based in vitro test for potential viral contaminants.

To expedite RCB release, options include rapid testing by polymerase chain reaction (PCR), interim-read in vitro strategies, and identity testing by DNA barcoding.

Master cell bank testing

The master cell bank (MCB) is the primary, well‑characterized cell source from which all working cell banks (WCBs) are derived. It is generated from a single, clonally derived cell line, expanded under controlled conditions, aliquoted, and stored (e.g., in the vapor phase of liquid nitrogen) to support consistent manufacturing over the product lifecycle. Extensive testing is performed on the MCB, typically including:

Genetic identity and stability

  • Assessment of the transgene and integration profile (e.g., Southern blotting, mRNA sequencing, and | or transgene copy number).
  • Confirmation of identity (e.g., DNA barcoding or equivalent methods).

The extensive qualification of the MCB supports reduced, risk‑based testing of derived WCBs.

Microbial and adventitious agent safety

  • Testing for bacteria, fungi, mycoplasma, and mycobacteria (e.g., sterility, mycoplasma, and mycobacterium assays).
  • Comprehensive virus safety testing in line with the cell line’s risk profile and regulatory expectations.

Working cell bank testing

Working cell banks (WCBs) are prepared from the MCB. Biosafety testing requirements for the WCB depend on the level of testing conducted on the MCB.

Where extensive characterization has already been completed on the MCB, minimal testing is required on the WCB. Depending on the regulatory authority, this is typically limited to assessment of identity, stability, and microbial contamination. Virus testing is recommended only where a recognized risk occurs.

To characterize genetic stability, the transgene is assessed using techniques such as Southern blotting, mRNA sequencing, and | or transgene copy number. Identity can be measured using DNA barcoding. The presence of microbes is determined using sterility, mycoplasma, and mycobacterium assays.

Test methodologies used to characterize working cell banks originating from different species include:

  • Sterility testing
  • Mycoplasma testing
  • In vitro assays

Genetic stability assays may be requested using these methods:

  • Nucleic acid sequencing
  • Southern blotting
  • Identity testing
  • Gene copy number

End-of-production cell bank testing

An end-of-production cell bank (EoPCB) is sometimes referred to as a post-production cell bank (PPCB) or as cells at the limit of in vitro cultivation. These cells are tested to validate the production system to ensure cell stability and identify any contamination issues.

The timing of EoPCB sampling will vary by product and is performed on a case-by-case basis.

For cell lines used in the manufacture of protein-based therapies, testing typically covers two areas: stability and contamination (biosafety). Testing schemes for cell lines used in viral vaccines or viral vectors may not require the same genetic stability assessments, depending on the MCB generation process.

Requirements for the EoPCB are very similar to those of the MCB. The EoPCB requires genetic stability testing and direct comparison with the MCB. Tests used include genetic analysis of the transgene using techniques such as Southern blotting, mRNA sequencing, or transgene copy number. A number of methods are used to test for potential contaminants, including those for microbes (sterility and mycoplasma), adventitious viruses (in vitro and in vivo tests and transmission electron microscopy), and specific virus tests, as determined by the process.

Test methodology used to characterize EoPCBs originating from different species include:

  • Sterility testing
  • Mycoplasma testing
  • In vivo testing
  • In vitro testing
  • Retrovirus testing
  • Bovine and porcine assays
  • Electron microscopy
  • Species-specific assays

Genetic stability assays provided by Sartorius include the following:

  • Nucleic acid sequencing
  • Southern blotting
  • Identity testing
  • Gene copy number

Regulatory requirements for cell line characterization

With a safety profile established over 20 years, CHO cells are by far the most widely used production cell lines in the pharmaceutical industry. Sartorius has performed biosafety and characterization testing on more than 200 CHO cell banks. Our scientists have extensive experience to advise on the most appropriate and cost-effective testing strategy to meet regulatory requirements. This recommendation takes into consideration both the history of the cell line and the raw materials used during the cell bank manufacturing. Below is a standard QC testing plan for CHO cell line characterization.  While this plan may be modified for cells of human and simian origin, the basic principles apply.

 

Biosafety testing 
Microbiological safety
  • Sterility
  • Mycoplasma
Viral safety
  • Species-specific viruses (vesiviruses, bovine and porcine viruses, MVM, MAP, and HAP)
  • Retroviruses (transmission electron microscopy and S+L assay)
  • Adventitious agents (in vitro assays)
Characterization 
Genetic analysisTransgene confirmation (gene copy number and sequencing)
IdentityDNA barcoding

With a well-established safety profile, HEK cells are widely used as host cell lines in biopharmaceutical research and production, particularly for viral vectors and recombinant proteins. Sartorius has extensive experience performing biosafety and characterization testing on HEK cell banks and can recommend appropriate, cost-effective testing strategies to meet regulatory expectations, considering both cell line history and raw materials used. The table below provides an overview of a standard QC testing package for HEK cell line characterization.

 

Biosafety testing 
Microbiological safety
  • Sterility
  • Mycoplasma and mycobacterium
Viral safety
  • Species-specific viruses (human and simian viruses, bovine and porcine viruses; optional: SARS-CoV-2 and MVM)
  • Retroviruses (transmission electron microscopy, PERT)
  • Adventitious agents (in vitro assays)
Characterization 
Genetic analysisSequencing and gene copy number (custom development)
IdentityMorphology (if adherent) and DNA barcoding

With a well-established safety profile, MDCK cells are widely used as host cell lines in biopharmaceutical research and vaccine production, particularly for influenza virus manufacturing. Sartorius has extensive experience performing biosafety and characterization testing on MDCK cell banks and can recommend appropriate, cost-effective testing strategies to meet regulatory expectations, considering both cell line history and raw materials used. The table below provides an overview of a standard QC testing package for MDCK cell line characterization.

 

Biosafety testing 
Microbiological safety
  • Sterility
  • Mycoplasma
Viral safety
  • Species-specific viruses (bovine and porcine; optional: MVM)
  • Retrovirus (transmission electron microscopy and PERT)
  • Adventitious agents (in vitro and in vivo assays)
Characterization 
Genetic analysisTransgene confirmation (gene copy number and Southern blot)
Appearance and identityMorphology (if adherent) and DNA barcoding

With a well-established use in advanced therapies, stem and immune cells are increasingly used as starting materials for cell and gene therapy products. Sartorius has extensive experience performing biosafety and characterization testing on stem and immune cell banks and can recommend appropriate testing strategies to meet regulatory expectations, considering both cell source | history and raw materials used. The table below provides an overview of a standard QC testing package for stem and immune cell bank characterization.

 

Biosafety testing (standard package)
Microbiological safety
  • Sterility
  • Mycoplasma and mycobacterium
Viral safety
  • Species-specific viruses (human virus panel by PCR; optional: SARS-CoV-2)
  • Retroviruses (transmission electron microscopy)
  • Adventitious viruses (in vitro assays)
Identity
  • DNA barcoding
  • Finger printing
Additional testing (based on product risk assessment)
Additional adventitious virusesNext-generation sequencing 
Species-specific virusesSimian virus panel, bovine and porcine viruses, sexually transmitted disease (STD) panel by PCR or next-generation sequencing
Replication competencyReplication-competent retrovirus (if retroviral vectors were used to induce gene editing)
ImpuritiesResidual plasmids and viruses (for induced pluripotent stem cells induced using plasmid or viral vectors); custom testing design
TumorigenicityNot required for continuous cell lines or irradiated cells. For highly expanded cells, testing may be considered in specific circumstances, as described by FDA guidance
Other speciesAs required

Learn more about cell line characterization

Related Assets

Brochure

cGMP Cell Bank Manufacturing and Characterization

icon-blog

What is Mycoplasma?

Mycoplasmas are the smallest self-replicating organisms currently known to science.

Read Blog Article

Frequently Asked Questions

Regulatory process per ICH Q5D confirming identity, purity, genetic stability and freedom from adventitious agents for MCB, WCB and EoPCB. Required by FDA and EMA before clinical or commercial manufacture.

MCB is the primary, extensively characterised stock stored long-term. WCB is derived from the MCB for routine production. MCB requires the most extensive ICH Q5D testing; WCB testing is more limited where MCB characterization is complete.

Mycoplasma (PCR and culture), sterility, adventitious virus (in vitro and in vivo), species identity (DNA barcoding), genetic stability (sequencing, copy number), endogenous retrovirus testing.

CHO, HEK293, MRC-5, Vero, MDCK, NS0 and others. DNA barcoding validated for CHO-K1, HeLa, HEK-293, Vero, MDBK, MRC-5, A9 and MA104.

In vivo adventitious virus studies typically 28 days. Full MCB package ranges 8–16 weeks depending on scope. Ready-to-use QC plans accelerate scheduling.

Cell line characterization is essential to confirm the identity, genetic stability, and purity of the mammalian cell banks used to produce your biologic. It proves that your cell line is free from adventitious agents (like bacteria, fungi, mycoplasma, and viruses) and guarantees reproducible manufacturing across the lifecycle of your drug.

Consult Our Experts

Consult Our Experts