Picus-2 Single Channel 300-µL Pippette on a stand

Pipetting ergonomics

Pipetting ergonomics: Reduce strain and improve pipetting performance

Ergonomic pipetting practices can help reduce hand, wrist, arm and shoulder strain during repetitive laboratory work. Pipetting for extended periods, using excessive force, maintaining awkward postures or performing repetitive movements can increase the risk of discomfort and repetitive strain injuries (RSIs).

Learn how to improve pipetting ergonomics with practical guidance on pipette handling, posture, posture, work habits and workflow design. By identifying and addressing ergonomic risk factors, laboratory professionals can create more comfortable pipetting workflows while supporting consistent, reliable results.

Browse Our Ergonomic Pipettes

What to consider for ergonomic pipetting

Picus 2 120 µL electronic pipette, Tacta 200 µL mechanical pipette side-by-side in gloved hands

Choosing ergonomic liquid handling tools

Selecting the right pipette can help reduce hand and arm strain during repetitive liquid handling tasks. Factors such as operating force, pipette weight, grip design, tip attachment and ejection force can have a significant impact on user comfort and workflow efficiency.

When selecting an ergonomic pipette, consider the following:

  • Choose electronic pipettes with electronic tip ejection to minimize the manual force required to eject tips.
  • Select mechanical pipettes with low operating forces, particularly for tip attachment and ejection.
  • Choose a lightweight, well-balanced pipette to help reduce the effort required to hold and operate the instrument.
  • Look for an ergonomic grip and finger hook that provide support and minimize the force needed to maintain a secure grip.
  • Use multichannel pipettes when appropriate to process multiple samples simultaneously, reducing repetitive motions and helping increase workflow efficiency.

Reduce pipetting strain with low-force tools

The operating force required to complete a pipetting cycle can vary considerably between pipettes. While the force required for an individual aspiration, dispense, blow-out or tip-ejection step may seem small, these forces can accumulate over hundreds or thousands of pipetting cycles.

Tip ejection is often one of the most force-intensive steps in manual pipetting. Choosing an electronic pipette with electronic tip ejection, or a mechanical pipette designed for low-force tip ejection, can help reduce the physical effort associated with repetitive liquid handling.

Choosing a pipette that combines ergonomic design, low operating forces and consistent performance can help create a more comfortable and efficient liquid handling workflow.

Improve pipetting consistency with ergonomic tools

Ergonomics can influence more than user comfort. Fatigue and inconsistent pipetting technique can affect how consistently a liquid handling task is performed, particularly during long or repetitive workflows.

Lightweight, well-balanced pipettes can help reduce fatigue during extended use, while electronic pipettes can provide consistent, controlled operation with minimal manual force. Multichannel pipettes can also help streamline repetitive workflows by allowing multiple samples to be processed at the same time.

Sartorius pipettes designed with ergonomics in mind

Sartorius considers ergonomics, ease of use, accuracy and efficiency when developing pipetting solutions. Our pipettes are designed to help minimize the physical effort associated with repetitive liquid handling while supporting accurate and precise results.

Ergonomic design features include lightweight and balanced handles, comfortable grip options, low operating forces and designs that accommodate different hand sizes and holding positions. These features can help reduce the physical demands of repetitive pipetting and support more comfortable laboratory workflows.

  • Picus® 2 electronic pipettes feature electronic pipetting and electronic tip ejection to minimize manual operating forces and a lightweight ergonomic design to  support comfortable operation during repetitive liquid handling tasks.
    Explore Picus® 2
  • Tacta® mechanical pipettes combine a lightweight, ergonomic design with low operating forces. The Optiload system uses spring-loaded tip cones to help make tip attachment and ejection smoother. 
    Explore Tacta®

Sartorius pipette tips are available in easy-to-open racks designed for convenient access, while compatibility with the Optiload system supports low-force tip loading and ejection.

Sartorius ergonomic pipettes

Both electronic and mechanical pipettes have their advantages dependent on your pipetting applications and workflows. Read more about choosing the right pipette for your laboratory from our selection guide. 

Picus 2 pipettes on stand - 01

Picus® 2 Electronic Pipette

Tacta® Mechanical Pipette

Pipette resources

View All Resources
Benefits of an Ergonomic and Electronic Pipette for RT-PCR

Benefits of an Ergonomic and Electronic Pipette for RT-PCR

Ergonomic pipettes have been proven to reduce pipetting error in long pipetting series. The ergonomic benefits go even further with an electronic pipe...

Pipetting Ergonomics White Paper

Good pipetting ergonomics requires proper tool selection and optimized working environment.

infographic thumbnail

Strategies to Improve Lab Ergonomics by Using the Right Pipette

Get expert tips on how to improve your well-being in the lab and discover strategies to optimize lab ergonomics by using the right pipettes.

Frequently asked questions

Repetitive pipetting exposes the user to musculoskeletal disorders (MSD) and repetitive strain injury (RSI) and can cause carpal tunnel syndrome (CTS). The common symptoms are pain in hands and arm, especially in the wrists. This can lead to long absences from work and of course inconvenience into your everyday life. There is no threshold value of safe level of pipetting so everyone regardless of amount of pipetting should consider work ergonomics.

  • Frequency of pipetting​
  • Speed of your movements​
  • The time of continuous pipetting​
  • Working posture and how much it deviates from a neutral posture​
  • Time reserved between sessions for rest and recovery

Using ergonomic tools and especially the use of fully electronic pipettes reduces ergonomic risk. Spread repetitive work throughout the day and allow enough time for your hand and body to rest. Be aware of your working posture and work in as neutral position as possible. Alternate your pipetting hand and where possible share pipetting responsibilities with multiple persons

Request a Quote, Demo, or More Information

What other areas are you interested in? (select all that apply)

Request a Quote, Demo, or More Information

icon-shopping-cart
Ready to Buy?