Accelerating Discoveries for Viral Biology and Host Immunity with Advanced Cell Analysis Solutions - White Paper
In the wake of global pandemics such as COVID-19, MERS-CoV, and Ebola, virology studies have taken center stage. This increased awareness is accompanied by an urgent need to characterize viral biology and the host immune response for the identification of therapeutics and development of vaccines.
Addressing these needs requires the use of experimental approaches that are high throughput, yet properly balanced with thorough analysis for scientific rigor, leading to reproducible results. Traditional endpoint analysis can be limited, utilizing time-consuming, tedious “hands-on” workflows with multiple instruments, which also presents safety concerns through increased exposure to pathogens.
This publication review highlights how the Incucyte® Live-Cell Analysis System and iQue® 3 Advanced High-Throughput Flow Cytometry addresses these challenges to derive deeper insights into the host pathogen interaction through the course of viral infection.