Integrated Applications — Video

Whether you need to perform common weighing procedures or run dedicated laboratory applications, Quintix® and Secura® will give you the best of both. They provide built-in applications as standard features and offer the widest array of accessories and options to choose from.

Weighing

Would you like to measure the weight of a sample with high accuracy? Easy. Just select the Weighing function on your Sartorius balance.

Mixing

Say you have a formula and need to weigh in various components quickly with 100% traceability, without losing track of the total weight. Just use the Mixing application.

Statistics

Would you like to save statistics on an entire group of different samples? Your Sartorius balance will transfer the readings to its statistics memory and generate a report on the key statistical parameters.

Components

Do you need to compound components according to a formula, but don’t want to mix them immediately? The Components application enables you to weigh your individual ingredients into different containers and to retrieve the total amount weighed-in – anytime at the touch of a key.

Density

Let’s suppose you have a solid, irregularly-shaped object and want to precisely determine its density. Just use the Density application along with the Sartorius density determination kit to calculate the quality of, for example, precious metals and plastic parts with high accuracy.

Percentage

Do you want to compare different samples and determine how much they vary from a reference sample in percent? The Percentage application will show you the difference in percent.

Conversion

Do you need to convert a unit of mass using a defined factor e.g. in order to calculate the weight per unit area, such as gsm? This application will show you the converted weight at the touch of a key.

Unstable conditions

Do you have to weigh in an extremely unstable environment or measure the weight of an inquisitive little mouse that just won’t sit still? No problem. This application lets you determine the weight reliably, giving you peace of mind about the accuracy and traceability of your results.

Checkweighing

Would you like to quickly check whether different samples are within a specific tolerance range? This application will enable you to see at just one glance whether a sample “gets the green light” so to speak.

Peak hold

Say you want to measure the release force or you have a large object on the pan that hides the display. This application “locks in” the maximum weight, or peak, of a measurement so that you can read it off for 15 sec.

Counting

Familiarize yourself with the capabilities of your Sartorius balance and start off by counting identical parts. The balance will show you the quantity and the total weight.

Request a Quote, Demo, or More Information

What other areas are you interested in? (select all that apply)

Request a Live, Virtual Secura®️ & Quintix®️ Demo Today!