Principales preguntas frecuentes
A continuación, encontrará respuestas a las preguntas más frecuentes. Si no encuentra una respuesta aquí, visite también nuestra Base de conocimientos para conocer más temas.
There are two solution to this problem
Solution a: Start the command prompt as an administrator and thereafter do the installation in the command prompt.
Solution b: Install SIMCA®/MODDE® as an silent installation, for details on how to do that see this link.
Send an email to umetrics_support@sartorius.com and we will deactivate the old activation. In this email please make sure the following information is available, your full name, company/university, activation and that you have change to a new computer.
Unfortunately the demo will not work on a MAC with a virtual windows installed.
To get a license file for the demo version that will work on a MAC with a virtual machine installed, please contact the Sales Manager of your region.
Answer 1: The incorrect version of the licenser server is installed (for example the license server for SIMCA® 13 is installed while you have a license file for SIMCA® 12 or the other way around.) Make sure you have the correct license server installed
Answer 2: You have received an incorrect license file (for example you have received a license file for MODDE® 9.1.1 while you should have a license file for MODDE® 9.1.) Please contact Umetrics_delivery@sartorius.com to get the correct license file. In this email please make sure the following information is available; your name, company/department, site, activation key/product key, registration key and information about the error.
Products from SIMCA® 13 and MODDE® 9.1.1 can use the newest version of Umetrics License Server.
SIMCA®
SIMCA® 16 uses UmLicenseServer 4.9.6 or newer
SIMCA® 13, 14.x, 15 uses UmLicenseServer 4.5.7 or newer.
MODDE®
MODDE® 9.1.1, MODDE® 10, MODDE® 11, MODDE® 12.x uses UmLicenseServer 4.5.7 or newer.
MODDE® 9.0 and MODDE® 9.1 uses UmLicenseServer 2.4.0
Make sure that you have downloaded the correct version of SIMCA®/MODDE®, if you have a product key you should use the following links
For MODDE® 9.1, SIMCA® 13.0/MODDE® 9.0 and older versions contact support to get the installation files at umetrics_support@sartorius.com