Application Note: Impact of the Claristep® Filtration System on Recovery and Adsorption of Various Therapeutic Proteins at Low Sample Volumes 

We tested the novel filter device Claristep® for the preparation of protein samples containing one of four different target molecules: an anti-malaria vaccine candidate, aviscuminum, interferon alfa-2B, or monoclonal antibody (mAb) P2G12. In comparison to the standard protocols for sample preparation prior to analysis by either reversed-phase or SEC HPLC, the Claristep® filter did not exhibit a significant difference in protein concentration if the target molecules were present with at least 1.0 g L-1. A significantly reduced product concentration was observed in the Claristep® filtered samples compared to the standard protocol for mAb P2G12 if the concentrations were lower. The protein adsorption to the filter material was well described by a Langmuir adsorption isotherm. Additionally, the Claristep® filters facilitated a rapid sample preparation with minimal volume losses.

Discover More About Cannabis Testing

Request a Quote, Demo, or More Information

What other areas are you interested in? (select all that apply)

Complete the Form Below to Download Your Copy