ATP Assay

The Incucyte® ATP Assay is an end-to-end solution consisting of instrumentation, software, and reagents that enables direct analysis of ATP facilitating the understanding of metabolic change in cancer cells. Evaluate metabolic changes like never before!


Request More Info

Probing cell metabolism using live-cell imaging and analysis

Cancer cells exhibit metabolic rewiring to support increased rates of proliferation and survival in the tumor microenvironment. This phenomenon is recognized as a hallmark of cancer. Recent studies also point to the importance of understanding the complex relationship between cancer cells and cancer-associated stromal cells, specifically evaluating how metabolic symbiosis promotes drug resistance. Researchers employ a wide-variety of biological techniques in order to expand their knowledge of cancer-associated metabolic changes and for the development of anti-cancer therapies. However, evaluation of metabolic changes in complex cancer cell models as they proliferate and interact with their environment are limited by current techniques.

Traditional techniques for measuring metabolic changes often:

  • Cannot distinguish cell-type-specific metabolic changes in complex co-culture models
  • Use indirect, byproduct measurements of metabolism as opposed to directly measuring metabolic ATP output
  • Do not integrate confirmation of cell morphology
  • Analyze an endpoint, rather than perform kinetic evaluation
  • Do not incorporate physiologically relevant environment conditions, thus introducing potential artifacts

Watch the Incucyte® ATP Assay for Live-Cell Analysis video

Incucyte ATP Assay

It Is Now Possible to Distinguish Cell-Type-Specific, Long-Term Metabolic Changes in Advanced Cell Models With Direct ATP Measurements

Gain unprecedented access to cell-type specific metabolic changes in advanced models with continuous imaging and analysis. The Incucyte® ATP Assay allows for direct measurements of cytosolic ATP for the characterization of tumor cell models in physiologically relevant conditions. Distinguish cell-type specific changes in ATP with integrated qualitative confirmation of cell morphology in real time with the Incucyte® SX5 Live-Cell Analysis System configured with an SX5 Metabolism Optical Module, Incucyte® ATP Analysis Software Module, and Incucyte® CytoATP Lentivirus Reagent Kit.

Key Advantages

Novel, Non-perturbing Reagent

Express Incucyte® CytoATP Lentivirus Reagent in a variety of cell types for direct measurements of cytosolic ATP in live cells.

Figure 1. Efficient, non-perturbing labeling of living cells enables direct measurement of cytosolic ATP. HeLa cells were infected with Incucyte® CytoATP Lentivirus and subjected to puromycin selection to generate a stably expressing population. Morphology (A) and proliferation (B) of CytoATP-expressing cells were unchanged compared to parental cells. (C) HeLa cells stably expressing CytoATP seeded at 4,000 cells/well in a 96-well microplate were exposed to a combined treatment of 2-deoxy-D-glucose (2DG) and potassium cyanide (KCN). Quantification of CytoATP fluorescence images captured over 3 hours reveals a rapid, concentration-dependent depletion of ATP resulting from concurrent glycolysis and oxidative phosphorylation blockade.

Analyze cell-type specific ATP changes

Automatically measure and visualize cell-type-specific changes in cytosolic ATP for greater insight into the dynamic tumor environment.

Figure 2. Distinguish impacts on ATP in a specific cell type in monoculture or advanced cell models. The triple negative breast cancer (TNBC) cell line HCC1806 and receptor-positive breast cancer cell line MCF7 stably expressing CytoATP or CytoATP Non-binding Control were seeded in the presence or absence of CCD14086SK fibroblasts (8K cells/well). Identification of cellular changes in ATP (color scaled masking) is performed using the integrated Incucyte® ATP Analysis Software Module. Masked images (A) provide visualization  ATP in HCC1806 cells treated with 1 µM CB-839 in monoculture and in co-culture with CCD14086SK cells. Kinetic data shows a more sustained depletion of ATP in TNBC lines (B) following CB-839 treatment compared to MCF-7 (receptor-positive cell line) grown in monoculture (C). However, co-culture with stromal cells mediated resistance to CB-839 in TNBC cells, while receptor-positive cell lines displayed no differential effect. IC50 curves depict 72 h (B) and 15 h (C) time point data.

Conduct Temporal Studies of ATP Dynamics

Generate real-time metabolic data for greater biological insight into both short-term and long-term ATP dynamics in response to treatments.

Figure 3. Discriminate mitotoxic vs cytotoxic compounds with nondestructive, repeated measurements of ATP. NIH 3T3 cells stably expressing CytoATP or Non-binding Control were grown in standard conditions (Glucose) or growth medium containing galactose substituted for glucose (Galactose) to drive dependence on oxidative phosphorylation for energy metabolism. Cells seeded at 12K cells/well in a 96-well microplate and fluorescent images (10X) were treated with nontoxic (Ambrisentan), cytotoxic (Chlorpromazine) or mitotoxic (Nefazodone) compounds. Kinetic data reveal a rapid depletion of ATP in cells treated with cytotoxic or mitotoxic compounds. While the response to cyotoxic compounds is similar in both media conditions, the leftward shift in IC50 of Nefazodone in cells grown in galactose is indicative of mitochondrial toxicity. A greater degree of separation is observed at early time points, demonstrating that kinetic CytoATP data can provide additional insight for evaluating compound profiles.

Confirm changes in cell morphology

Associate changes in cell morphology with ATP metabolism to reveal informative, temporal changes in cell behavior..

Figure 4. Enable qualitative inspection of cell morphology with HD phase images. HeLa cells stably expressing CytoATP or Non-binding Control seeded at 2K – 8K cells/well in 96-well microplates were treated with Chlorpromazine (60 µM), Etoposide (100 µM), or 2DG (20 mM) + KCN (2 mM), compounds that deplete ATP with variable time of effect highlighted by kinetic analysis (insets). HD phase images of cells (10x) acquired during depletion reveal drastic changes in morphology of cells treated with Chlorpromazine (21 h) and Etoposide (75 h), whereas cells treated with 2DG +KCN (60 min) show no significant morphological change compared to vehicle control.

Request More Information

Ordering Information

Resources

Protocols

Incucyte® CytoATP Lentivirus Reagent Kit (EF1α, Puro)

Posters

Direct measurements of cellular ATP levels using automated, quantitati...

Kinetic measurements of intracellular ATP levels in co-culture models...

Related Reagents and Applications

Brochure

Incucyte® Reagents, Consumables and Software

Cell Movement & Morphology - Spheroids

Spheroid Assays

Cell Migration and Invasion

Incucyte® ATP Assay Enables Direct, Live-Cell Measurement of ATP

Frequently Asked Questions

The ATP assay uses the Incucyte® SX5 configured with the Metabolism Optical Module, in conjuncation with the Incuctye® ATP Software Analysis Module and Incucyte® CytoATP Lentivirus Kit for real-time detection and evaluation of changes in cytoplasmic ATP in mono- and co-culture models. The Inuccyte® CytoATP is a lentiviral based live-cell labeling reagent that results in stable expression of a dual fluorescent ATP indicator, that we are then able to image on the Incucyte® SX5 using a dual passband emission filter.

The Incucyte® data is a direct readout of cystolic ATP generated over time in a physiologically relevant environment with the added capability of evaluating cell type-specific metabolic changes, unlike other assays that measure metabolic end products at single point in time without full environmental control in mono-culture cell models.

The Incucyte® ATP Assay is designed to study dynamic changes in ATP utilizing a reagent that requires distinct signal separation between ATP bound and free states. The acquisition and analysis tools are designed for use with our Incucyte® SX5 and the Incucyte® Metabolism Optical Module that allows us to study the changes in these states using dual excitation and single emission image acquisition which is not possible on Incucyte® S3 with Green/Red Optical Module, or the Incucyte® SX5 with the Green/Orange/NIR Optical Module.

We have not been able to introduce our genetically-modified fluorescent ATP indicator into immune cell models. As of now, this application has only been validated with cancer cell lines.

No. Due to different acquisition methods (metabolism using using dual excitation/ single emission), and that both the Incucyte® MMP and Incucyte® CytoATP are read in the orange channel, these two assays cannot be multiplexed.

Request a Quote, Demo, or More Information

What other areas are you interested in? (select all that apply)

Request a Demo, Literature, or More Information