Major Investment in Capacities for Production and Innovation
Sartorius is constantly investing in its Göttingen Campus, located at the heart of Germany. The current milestones of the expansion are:
- New Building for Research & Development (2023)
- New Building for Membrane Manufacturing (2023)
- New Building for Filter Production (2026)
- 100% renewable energy supply (2030)
Facts & Figures: Extension of the Campus
New R&D Building
~11,300 m²
Gross Floor Area
New Membrane Production Building
~21,100 m²
Gross Floor Area
New Filter Production Building
~21,600 m²
Gross Floor Area
Our Ambition: 100% Renewable Energy Supply on Campus Until 2030
Electricity
- Campus obtains electricity from wind energy
- Basic electricity supply is emission-free
- Additional operation of PV systems
Geothermal Energy
- Own geothermal field (90 boreholes, each 160m deep)
- Heating capacity 1,550 MWh/a (corresponds to ~80 SFH)
- Cooling capacity 1,020 MWh/a
District Heating
- Northern Campus heated with district heating from early 2024
- Connection to Göttingen district heating network planned by 2030 at the latest
Impressions from the Göttingen Expansion
Supporting Customer Growth
Explore Our Solutions, Products and Services
Facility Contact Details
Sartorius AG
Otto-Brenner-Straße 20
37079 Göttingen
Germany
Media Relations:
Send Email