Practical Tips for Choosing the Bottle-top Dispenser for Your Lab

Bottle-top dispensers are commonly used in various laboratories to measure liquid (typically between 1 and 60 ml) from a reagent bottle. Because they are used in so many different lab settings, there can be many factors to consider when choosing the right bottle-top dispenser for a particular set of needs.  

A few questions to consider when shopping for the right bottle-top dispenser:  

  • Which chemicals will this bottle-top dispenser be used for – and will it be durable enough to tolerate them?  
  • Is this bottle-top dispenser easy to clean and calibrate?  
  • What is the nominal volume for this unit?  
  • Does this bottle-top dispenser have ergonomic controls to allow for ease of use? 

A bottle-top dispenser is a long-term investment, so it is a good idea to consider all factors when choosing the unit to best suit your laboratory needs. 

Download Application Note

Commonly Asked Questions

  • Do I need a bottle-top dispenser in my lab? - If you work in a laboratory environment where it is common to need to measure larger volumes that would be inconvenient using a pipette.
  • How can bottle-top dispensers improve performance in the laboratory? - Properly calibrated bottle-top dispensers dispense reagents more quickly and with a higher degree of accuracy than when using a measuring cylinder or volumetric flask, so there is a smaller likelihood of error. And because they are designed to reduce spillage, they help to keep the workspace clean and free of contaminants.

This application note presents criteria to consider when evaluating dispenser models.

Request a Quote, Demo, or More Information

What other areas are you interested in? (select all that apply)

Complete the Form Below to Download Your Copy