Wetland Biotope in Göttingen
An Ecologically Diverse Habitat
In an initiative launched by Sartorius and in cooperation with the Heinz Sielmann Foundation and the city of Göttingen, a diverse wetland is being created on a 16 hectare tract located along the Leine River. Most of the area developed in the project was once heavily farmed.
The Leine River divides the site into two parcels of land that have evolved into an ecologically diverse haven for rare and endangered animals like amphibians and birds. For this purpose, a softwood alluvial forest, flood channels, hollows, and depressions were developed as elements of floodplain relief. Additionally, shallow pools, standing bodies of water, and extensive grasslands were created.
Renaturation is progressing faster than expected. Experts have recently spotted large numbers of partridges, tree hawks, whinchats. The most spectacular discovery: a resting ruff and a eurasian stone-curlew, an endangered species. The flora is also recovering. Where thistles grew a year ago, grasses and herbs now thrive. Visitors can explore the site via an observation tower and an explorers' trail.
Sartorius funded the entire project, which costs more than one million Euros.
From farmland to haven for plants and animals
Move the slider to see the renaturation progress
Idea and Realization
Map of the Area
Download
- Map Wetland at Lake "Kiessee" PDF | 137.7 KB
Areas of the Wetland
Shallow water ponds
Shallow water ponds are bodies of water that are not deep. Amphibians feel right at home in them thanks to the fluctuating levels of water that occur in these pools. The prevailing conditions of wet and dry create the perfect habitat for amphibians. Flora and fauna have adapted perfectly to the fluctuating water levels of the respective seasons. To settle in such a place, amphibians need something else as well: extensive grasslands to which no fertilizer has been applied. It is the exact conditions that the biotope offers. Another important aspect of this habitat is the opportunity to seek refuge back on land.
Still water bodies
Water does not flow into and out of these shallow ponds. Sunlight reaches all the way to the bottom, creating the conditions that green plants need to grow and that a range of aquatic animals need to live. Amphibians benefit from the conditions as well, as evidenced by their habit of laying their spawn in the shallow bodies of water. Sunlight also facilitates the development of larvae. But they have to watch out for hungry fish that prowl the area.
Softwood alluvial forest
Alluvial forests are found in the floodplains of bodies of flowing water and are located directly along the banks of streams and rivers. Shaped by the movement and power of the water, they provide a habitat for the widest range of flora and fauna. Softwood trees near rivers — in particular willows, alders and poplars — grow extremely fast. As a result of river regulation, softwood floodplains are increasingly turning into hardwood floodplains with shorter flooding periods. The objective of the project area is to create a natural forest whose developmental phases from young forest to decomposition are closely aligned. If a tree dies, it is allowed to remain standing or to lie on the ground as dead wood. The development of alluvial forests promotes biodiversity.
Extensive grasslands
Extensive grasslands facilitate sustainable uses while providing a way to unwind and experience the world. They also do an excellent job in helping protect groundwater. Their role in nature sanctuaries is primarily to provide a habitat and a place to procreate for ground-breeding birds. These areas are utilized for extensive grazing with miniature zebus and also offer a habitat for rabbits and deer to graze.
Flood channels with hollows
The flood channels created in the biotope are occasionally filled with water during high tides. The flooded hollows serve as an ideal spawn and growth area for endangered fish species in the floodplains. Young fish make their way to the river as the water recedes. A wide range of plants typically seen in a floodplain will appear depending on the length of time that the area was flooded.
Observation tower
The biotope has to meet two seemingly contradictory needs: It must provide nature with the tranquility that such a sanctuary requires and give people an opportunity to experience this world for themselves. The biotope achieves both with the observation tower that has been erected on the western edge of the area and with a boardwalk that is part of the eastern explorers’ trail. The official trails immerse visitors in the biotope without disturbing the world of animals.
Explorers’ trail
The biotope includes an explorers’ trail that enables visitors to experience the wonders of the biotope to the greatest degree possible while still respecting the needs of the flora and fauna that make their homes there. It provides visitors with direct insights into the life of the area. Dogs on a leash are welcome, too.