Back to News Overview
Date
Sartorius AG
Product News

The Fastest Stabilization Time Meets Everyday Analytical Weighing

Göttingen, February 27, 2024

  • Fastest stabilization time in its class for analytical weighing; results in under 2 seconds
  • Low minimum sample weight starting at 4.1 mg sets new benchmark for semi-microbalances
  • Innovative Cleaning QApp and tool-free assembly simplify compliance and routine maintenance
  • Advanced ionizing technology fully eliminates static electricity, optimizing accuracy
Cubis Ultra-High Resolution lab balance MCA 50mm

The Life Science Group Sartorius introduces the Cubis® II Ultra-High Resolution Semi-Micro balance, a perfect addition to the Cubis® II portfolio of premium laboratory balances. Designed for a wide range of weighing applications, this balance is the quintessential instrument for everyday use, offering impressive speed, precision, and ease-of-use.

Equipped with five-digit readability and a 220g capacity, the balance integrates cutting-edge weighing technology and a low minimum sample weight of 4.1 mg (or 8.2 mg for some models), surpassing typical requirements. Additionally, its industry-leading stabilization time of less than 2 seconds significantly enhances efficiency in the field.

Automatic compensation for environmental changes, such as temperature, humidity, air drafts, and air pressure, ensures consistent performance under real-world conditions. Crucial to this achievement is an innovative ionization technology that effectively neutralizes static electricity.

Recognizing the importance of cleanability, the new Cleaning QApp dramatically simplifies routine maintenance with clear, step-by-step instructions. Tool-free disassembly and reassembly of balance components further facilitate the cleaning processes, enabling compliance with standard operating procedures.

"The Cubis® II Semi-Micro balance is a game-changer for labs looking for a balance that excels in everyday weighing tasks," says Eszter Paldy, Manager of Product Management Premium Weighing Solutions at Sartorius. "With its fast stabilization time, low minimum sample weight, and ease of cleaning, this balance is a real solution that adapts to the dynamic needs of modern labs."

The new balance is fully equipped with the Cubis® II family's standard features, including modularity, compliance, connectivity, and digital data management.

For more information, please visit:

icon-e-mail
Media Contact