Part of The Solution: To Patch A Failing Heart

heart-shaped globe icon with happy face
Better Health
Jul 04, 2024  |  3 min read

The biotech company Repairon has developed an innovative form of therapy for the treatment of heart failure. Find out how Sartorius and its Göttingen-based neighbor are "in this together," exploring the full potential for commercial production and paving the way for groundbreaking therapeutic applications in the life sciences.

This article is posted on Sartorius Blog.

Shortly after birth, our heart muscle cells lose their ability to divide. This means that damage such as a heart attack leads to an irreversible loss of these cells. As a result, the heart's ability to pump effectively decreases, which can lead to cardiac insufficiency, also known as heart failure.

Heart failure affects an estimated 40 to 60 million individuals globally. They often suffer from shortness of breath, edema, and fatigue; the mortality rate is high. While medications and surgical procedures can mitigate symptoms, the condition remains incurable.

The problem: lost heart muscle cells cannot be restored. Sartorius’ partner Repairon is working on a therapy that directly targets this challenge.

The Idea: Heart Tissue From the Lab

For over two decades, the Repairon team has been researching to develop the so-called heart patch. It consists of new heart tissue, which is artificially grown from stem cells in the lab and then sewn onto special membranes that are compatible with the body. A surgeon can implant the patch, which is several square centimeters in size, onto the patient’s damaged heart tissue. The goal of the patch is to strengthen the heart muscle and permanently improve its pumping capacity.



A Collaborative Effort for a Cure: Sartorius Is Part of the Solution

It’s a highly complex process to produce the stem cells for the heart patches in the required quantities. It is, however, a crucial step to get closer to bringing them to market. Sartorius is providing expertise and support to Repairon in establishing industrial-scale patch production. Sartorius technologies, including bioreactor systems, cytokines, as well as freezing media, are integral to the process.


The project is a great example of how scientific findings from the life sciences can be translated into therapeutic applications.

Dr. Sven Wagner, Head of Business Development


Dr. Sven Wagner, Head of Business Development, ©Sartorius


Promising Results

The heart patch has already passed its first qualitative test. Within phase I of clinical trials, the maximum safe dosage of heart muscle cells per patch was determined in ten patients. The next phase aims to treat a higher number of patients.



The ongoing development and the encouraging results of the clinical trials give hope that the heart patch could pave a new way of treatment in the future and significantly improve the quality of life of those affected. “We are eager to continue our partnership with Repairon on this transformative project,” Sven remarks. “Plans for an even more collaborative future are already underway.”


Related Stories

Oscar-Werner Reif on How Sartorius Drives Innovation

Read the Interview with Oscar-Werner Reif, Head of Corporate Research, on the Sartorius Blog.

Life Science Factory Opens its Doors to Startups

The non-profit Life Science Factory initiated by Sartorius celebrated its official virtual soft opening on January 19, 2022.

The Opportunities to Collaborate with Sartorius are Virtually Endless

Read the Interview with Dr. Sven Wagner, Sartorius' Head of Business Development.

Part of the Solution: How Recombinant Albumin Supports the World’s Fir...

Helping to realize the promises of biologics, Sartorius is part of the solution in the fight against hepatitis.

Part of the Solution: How Freight Experts Keep Medical Production Runn...

Learn how Sartorius' Freight and Distribution Management Team makes sure biopharmaceutical companies have everything they need to produce medicines.

Part of the Solution: How Software Experts Help Digitize Bioprocesses

Around 50 software experts in Bangalore work in close collaboration with their manufacturing colleagues to digitize bioprocessing.

How Biopharmaceuticals Help to Protect Against Hepatitis

Helping to realize the promises of biologics, Sartorius is part of the solution in the fight against hepatitis.

Part of the Solution:  How Digital Customer Experience Simplifies...

At Sartorius IT, software engineers foster fast-paced digital solutions in an agile environment. 

Related Content

Research and Innovation at Sartorius

With innovative tools and technologies, we support life science research and the biopharmaceutical industry.

Partnerships

Sartorius supports creative technologies and businesses to foster entrepreneurship and cultivate innovation.

Repairon

Development, manufacturing and commercialization of induced pluripotent stem cell (iPSC) based tissues for organ repair.

icon-e-mail
Media Contact