Magali, let’s start at the beginning. Not all plastics used in the biotech industry are the same, can you give us an overview?
Indeed, the generic term “plastics” covers many materials designed to meet very different needs. Plastics are made from a wide range of polymers which are mixed with chemical compounds that protect them and improve material performance, for example regarding resistance to oxidation and UV light, fire-retardancy, and physical properties. The different types of plastics add complexity to recycling concepts.
Which special requirements must plastics fulfill in our industry? What are the challenges?
In the biopharma industry, single-use product designers face a complex set of demands when selecting materials, particularly to ensure both process efficiency and patient safety. These technologies must meet stringent requirements throughout their lifecycle, such as withstanding sterilization, maintaining structural integrity during transportation and storage, reliably serving their function in bioprocessing, and ultimately being manageable as process waste.
In addition, materials that get in contact with our customers’ products must be designed with minimized extractables for patient safety. And finally, the demand for extended shelf life imposes additional challenges. Our material engineers’ task is to integrate all these requirements across diverse process applications – which requires meticulous material selection and engineering.
When talking about recycling, what are the main challenges of plastics recycling in the biopharmaceutical industry?
There is a two-fold challenge, covering end and beginning of life of a plastic product: First, to recycle plastic products which are very often considered as “contaminated” and second to incorporate recycled plastic in new plastic products, because recycling is perceived as unsuitable for high-quality-applications – in some cases even forbidden.
Additionally, recycling is expected to have a better environmental impact. And on top of that, recycling should not cost more.
All in all, this is why retaining the value of our plastics, which are of excellent quality, is one of our goals.