Application Note: Pipette Calibration and Standards
Pipetting results are critically depending on the maintenance and calibration of the pipette. The most important International Standardization Organization (ISO) standards related to pipetting are ISO8655 and ISO17025 and these standards set the guidelines how and in which conditions calibration should be performed. Regular cleaning and maintenance according to guidelines also prolongs the lifetime of the pipette.