A Metrological White Paper Bundle
In addition to its wealth of technological experience accumulated over the years, the Sartorius Group also has decades of metrological expertise to offer. With its series of white papers that will gradually be compiled into a Best Practice Guide: Lab Weighing, Sartorius provides practical answers to the most important questions and issues revolving around the subject of weighing in the laboratory. Among the topics discussed in these white papers are calibration, accreditation, legal metrology and correct weighing. As a result, these white papers will give users all the knowledge needed to obtain accurate and reliable weighing results.
English
Framework Paper - Best Practice Guide: Lab Weighing
In the framework paper, the various topics of the White Paper Bundle "Best Practice Guide: Lab Weighing" are presented.
Reliable Weighing Results - Proper Handling of Laboratory Balances and Correct Handling of Samples
The most important influencing factors on the weighing result are presented and options are described how the disturbance variables can be minimized.
Weighing in Legal Metrology - Use and Testing of Laboratory Balances in Legally Regulated Environments Weighing
The requirements and limits of legal metrology are described. Measures are shown that help to ensure that the quality requirements of weighing applications are reliably met.
Calibration guideline EURAMET cg-18 - specifications, options and implementation of the guideline by Sartorius
In most countries, Sartorius follows the EURAMET cg-18 calibration guideline for accredited and non-accredited calibrations.
Download Now
Sartorius Balance Test Report - Testing and Evaluating Balances Against Different Tolerance Requirements
Sartorius balance test reports can be used to test balances against previously defined tolerances. The white paper describes the various tests and presents the test protocols.
Download Now
Minimum Sample Weights According to USP <41>, OIML R76 and EURAMET cg-18
The smaller the weight of the sample, the larger the relative measurement uncertainty that the weighing is subject to. What should a sample weigh at least to obtain a reliable weighing result?
Download Now
Use of Laboratory Balances in the Pharmaceutical Industry
The aim of this white paper is to present the testing requirements for laboratory balances as described in the relevant chapters of the pharmacopoeias.
Calibration Certificates From Accredited Providers - What Benefits Do Our Accreditations Offer the User?
This white paper explains the advantage of certificates from accredited providers.
Handling Test Weights - Sensible Selection and Correct Handling of Test Weights
Recommendations are given for the correct handling of test weights and for testing balances with test weights.
Sartorius Calibration Certificate for Weighing Instruments According to EURAMET cg-18 Explained Step-by-Step
The calibration certificate is explained step-by-step. Meaningful information is provided on how results can be used in the day-to-day work.
German
Rahmenpapier - Best Practice Guide: Lab Weighing
In dem Rahmenpapier werden die verschiedenen Themen des White Paper Bundles "Best Practice Guide: Lab Weighing" vorgestellt.
Verlässliche Wägeergebnisse - Der richtige Umgang mit Laborwaagen und korrektes Probenhandling
Die wichtigsten Einflussfaktoren auf das Wägeergebnis werden vorgestellt und es werden Möglichkeiten beschrieben wie die Störgrößen minimiert werden können.
Arbeiten im gesetzlichen Messwesen - Einsatz und Prüfung von Laborwaagen im gesetzlich regulierten Umfeld
Die Anforderungen und Grenzen des gesetzlichen Messwesens beschrieben. Es werden Maßnahmen aufgezeigt, die dabei helfen, die Qualitätsanforderungen von Wägeanwendungen sicher zu erfüllen..
Kalibrierrichtlinie EURAMET cg-18 - Vorgaben, Optionen und Umsetzung der Richtlinie durch Sartorius
Sartorius folgt in den meisten Ländern bei akkreditierten und nicht akkreditierten Kalibrierungen der Kalibrierrichtlinie EURAMET cg-18.
Sartorius Waagenprüfprotokoll - Prüfen und bewerten von Waagen gegen Unterschiedliche Toleranzanforderungen
Mit Waagenprüfprotokollen (Balance Test Reports) können Waagen gegen vorher festgelegte Toleranzen geprüft werden. Das White Paper beschreibt die verschiedenen Prüfungen und stellt die Prüfprotokolle vor.
Mindesteinwaagen nach USP <41>, OIML R76 und EURAMET cg-18
Je kleiner eine Einwaage ist, desto größer ist die relative Messunsicherheit mit der ein Wägeergebnis behaftet ist. Wie groß sollte eine Einwaage mindestens sein, um ein sicheres Wägeergebnis zu erhalten?
Einsatz Von Laborwaagen in Der Pharmazeutischen Industrie?
Ziel dieses White Paper ist es, die Testanforderungen an Laborwaagen, wie sie in den betreffenden Kapiteln der Pharmakopöen beschrieben sind, vorzustellen.
Kalibrierscheine von akkreditierten Anbietern - Welche Vorteile bieten unsere Akkreditierungen dem Anwender?
In diesem White Paper wird der Vorteil von Zertifikaten akkreditierter Anbieter wird erläutert.
Umgang mit Prüfgewichten - Sinnvolle Auswahl und korrekte Handhabung von Gewichten
Es werden Empfehlungen zum richtigen Umgang mit Prüfgewichten und zur Prüfung von Waagen mit Prüfgewichten gegeben.
Der Sartorius Kalibrierschein - Erklärungen und Hinweise für akkreditierte und nicht akkreditierte Kalibrierscheine nach EURAMET cg-18
Die verschiedenen Teile des Kalibrierscheins werden Schritt für Schritt erklärt. Es werden Hinweise gegeben wie die Ergebnisse in der täglichen Arbeit genutzt werden können.