Inspecting Cubis instrument

Best Practice Guide: Lab Weighing

A Metrological White Paper Bundle

In addition to its wealth of technological experience accumulated over the years, the Sartorius Group also has decades of metrological expertise to offer. With its series of white papers that will gradually be compiled into a Best Practice Guide: Lab Weighing, Sartorius provides practical answers to the most important questions and issues revolving around the subject of weighing in the laboratory. Among the topics discussed in these white papers are calibration, accreditation, legal metrology and correct weighing. As a result, these white papers will give users all the knowledge needed to obtain accurate and reliable weighing results.

Framework Paper - Best Practice Guide: Lab Weighing

In the framework paper, the various topics of the White Paper Bundle "Best Practice Guide: Lab Weighing" are presented.

Download Now

Reliable Weighing Results - Proper Handling of Laboratory Balances and Correct Handling of Samples

The most important influencing factors on the weighing result are presented and options are described how the disturbance variables can be minimized.

Download Now
 

Weighing in Legal Metrology - Use and Testing of Laboratory Balances in Legally Regulated Environments Weighing

The requirements and limits of legal metrology are described. Measures are shown that help to ensure that the quality requirements of weighing applications are reliably met.

Download Now
 

Calibration guideline EURAMET cg-18 - specifications, options and implementation of the guideline by Sartorius

In most countries, Sartorius follows the EURAMET cg-18 calibration guideline for accredited and non-accredited calibrations.

Download Now

Sartorius Balance Test Report - Testing and Evaluating Balances Against Different Tolerance Requirements

Sartorius balance test reports can be used to test balances against previously defined tolerances. The white paper describes the various tests and presents the test protocols.

Download Now

Minimum Sample Weights According to USP <41>, OIML R76 and EURAMET cg-18

The smaller the weight of the sample, the larger the relative measurement uncertainty that the weighing is subject to. What should a sample weigh at least to obtain a reliable weighing result?

Download Now

Use of Laboratory Balances in the Pharmaceutical Industry

The aim of this white paper is to present the testing requirements for laboratory balances as described in the relevant chapters of the pharmacopoeias.

Download Now

Calibration Certificates From Accredited Providers - What Benefits Do Our Accreditations Offer the User?

This white paper explains the advantage of certificates from accredited providers.

Download Now

Handling Test Weights - Sensible Selection and Correct Handling of Test Weights

Recommendations are given for the correct handling of test weights and for testing balances with test weights.

Download Now

Sartorius Calibration Certificate for Weighing Instruments According to EURAMET cg-18 Explained Step-by-Step

The calibration certificate is explained step-by-step. Meaningful information is provided on how results can be used in the day-to-day work.

Download Now

Rahmenpapier - Best Practice Guide: Lab Weighing

In dem Rahmenpapier werden die verschiedenen Themen des White Paper Bundles "Best Practice Guide: Lab Weighing" vorgestellt.

Jetzt downloaden

Verlässliche Wägeergebnisse - Der richtige Umgang mit Laborwaagen und korrektes Probenhandling

Die wichtigsten Einflussfaktoren auf das Wägeergebnis werden vorgestellt und es werden Möglichkeiten beschrieben wie die Störgrößen minimiert werden können. 

Jetzt downloaden

Arbeiten im gesetzlichen Messwesen - Einsatz und Prüfung von Laborwaagen im gesetzlich regulierten Umfeld

Die Anforderungen und Grenzen des gesetzlichen Messwesens beschrieben. Es werden Maßnahmen aufgezeigt, die dabei helfen,  die Qualitätsanforderungen von Wägeanwendungen sicher zu erfüllen..

Jetzt downloaden

Kalibrierrichtlinie EURAMET cg-18 - Vorgaben, Optionen und Umsetzung der Richtlinie durch Sartorius

Sartorius folgt in den meisten Ländern bei akkreditierten und nicht akkreditierten Kalibrierungen der Kalibrierrichtlinie EURAMET cg-18. 

Jetzt downloaden

Sartorius Waagenprüfprotokoll - Prüfen und bewerten von Waagen gegen Unterschiedliche Toleranzanforderungen

Mit Waagenprüfprotokollen (Balance Test Reports) können Waagen gegen vorher festgelegte Toleranzen geprüft werden. Das White Paper beschreibt die verschiedenen Prüfungen und stellt die Prüfprotokolle vor.

Jetzt downloaden

Mindesteinwaagen nach USP <41>, OIML R76 und EURAMET cg-18

Je kleiner eine Einwaage ist, desto größer ist die relative Messunsicherheit mit der ein Wägeergebnis behaftet ist. Wie groß sollte eine Einwaage mindestens sein, um ein sicheres Wägeergebnis zu erhalten?

Jetzt downloaden

Einsatz Von Laborwaagen in Der Pharmazeutischen Industrie?

Ziel dieses White Paper ist es, die Testanforderungen an Laborwaagen, wie sie in den betreffenden Kapiteln der Pharmakopöen beschrieben sind, vorzustellen.

Jetzt downloaden

Kalibrierscheine von akkreditierten Anbietern - Welche Vorteile bieten unsere Akkreditierungen dem Anwender?

In diesem White Paper wird der Vorteil von Zertifikaten akkreditierter Anbieter wird erläutert.

Jetzt downloaden

Umgang mit Prüfgewichten - Sinnvolle Auswahl und korrekte Handhabung von Gewichten

Es werden Empfehlungen zum richtigen Umgang mit Prüfgewichten und zur Prüfung von Waagen mit Prüfgewichten gegeben.

Jetzt downloaden

Der Sartorius Kalibrierschein - Erklärungen und Hinweise für akkreditierte und nicht akkreditierte Kalibrierscheine nach EURAMET cg-18

Die verschiedenen Teile des Kalibrierscheins werden Schritt für Schritt erklärt. Es werden Hinweise gegeben wie die Ergebnisse in der täglichen Arbeit genutzt werden können.

Jetzt downloaden