Pipettes and Pipette Tips by Sartorius

Three key factors – ergonomics, design and reliability – form the cornerstone of our products. Sartorius pipettes and pipette tips raise your pipetting to a whole new level ensuring repeatable and reliable results. Enjoy the experience with Sartorius products and feel the new standard of pipetting in your hand.

Ready to Buy?

Quickly find Pipetting and Dispensing products by searching by category or filtering by attributes.

Shop over 140 Pipettes and Pipette Tips Now

Sartorius Pipette Promotions

Pipette Trade-In Program | Up to 40% Discount on Pipette Products

Trade in your old pipettes for the most ergonomic electronic or mechanical pipettes available – all while receiving up to 40% off.

Find Out More

Pipette Tips in Stock

Explore various Pipette tips that are currently available in our local warehouses for immediate deliveries. Order today!

Find Out More

Pipette Quick Ship Program

Mechanical Pipettes are available for Quick Shipment in the United States and Canada. 

Find Out More

Pipette Product Categories

Picus Electronic Pipette

Electronic Pipettes

Picus® Nxt and Picus® are Sartorius’ user-friendliest and most sophisticated electronic pipettes.

Explore More
Mechanical Pipette

Mechanical Pipettes

Sartorius mechanical pipettes are appreciated for their ergonomics, ease of use and reliability.

Explore More
Pipette Tips

Pipette Tips

Our Optifit and Safetyspace® Filter Tips are designed to perfectly match our pipettes, permitting maximum accuracy, precision and ergonomics.

Explore More

Bottle-Top Dispensers

Sartorius bottle-top dispensers and burettes are safe. convenient and customizable. They fit perfectly to a wide range of dispensing needs.

Explore More
Pipette Controllers

Pipette Controllers

Midi Plus is a lightweight and easy-to-use pipette controller for large volumes.

Explore More

Pipette Accessories

Sartorius pipette accessories keep your laboratory clean, in good order and make your pipetting more comfortable.

Explore More

See What Sartorius Has to Offer

Pipetting

Pipetting Ergonomics

Learn how ergonomics can improve your well-being and results while protecting yourself from repetitive strain injuries (RSI).

Explore More
Pipetting

Pipette Training Academy ​

When did you last have formal pipetting training? 9 out of 10 Sartorius Pipetting Academy participants say they learned new skills.

Discover More

Pipette Services​

Sartorius offers comprehensive calibration, maintenance, and repair services to ensure your pipette’s everyday performance.

Explore More
Image of a pipette tip purity certificate

Certificates

To search for pipette certificates, lot specific pipette tip certificates and quality certificates, click on the download now button below.

Download Now

Applications for Pipetting

View Applications

Drug Discovery

Boost your productivity and find the most promising candidates sooner with pipettes that increase throughput and reduce errors. Your everyday multiwell plate setup can be sped up with modern pipetting tools that will also help maintain your high standard of quality. Our electronic pipettes help to harmonize lab practices to a new level, so you have one less variable to worry about. 

Sample Preparation

From easiest to most difficult samples, we offer pipetting that ensures the reliability of your results. Our pipettes can be easily adjusted for the non-aqueous reagents and standards in your work so even the smallest volumes are accurate. Ensure that you get the most out of your expensive liquids by choosing our high-quality and inert consumables.

Cell Biology

Pipettes that enable you to spend less time seeding cells and worrying about contamination and more time on making discoveries. Your cells will be back in the comfy warmth of their incubator in no time and you can concentrate on the analysis of your results. Lab work and cleanup will become something you are looking forward to - now that the hassle is gone.

Frequently Asked Questions

To achieve the highest level of accuracy, you should choose the smallest volume pipette capable of handling the volume in question. This is important because pipette is most accurate at nominal (maximum) volume. It is a well-recognized fact that even slight muscle fatigue reduces the output when performing work that requires precision. Therefore, in order to maintain the performance, pipettes which require high forces should be avoided. Moreover, heavy pipettes fatigue the user, selecting an ergonomic pipette allows precise operation. Electronic pipettes can be considered when number of samples is high or when reducing variance in pipetting is important. A multichannel pipette can significantly speed up working with 96 and 384 well plates.

There is two principles of how pipettes work, air displacement and positive displacement. The majority of pipettes used in laboratories work according to air displacement principle due to their wide applicability and lower costs of consumables. Positive displacement pipettes are sometimes used with problematic liquids, but air displacement pipettes can be used as well with correct techniques. An electronic pipette can eliminate a lot of the variance from pipetting and also variance between users. With an electronic pipette the piston movement is controlled automatically regardless of the user.

Different pipettes can fit different application, for example when working only with few samples a mechanical pipette is good choice, but when working with 96 microwell plates multichannel pipette is a better option. But in general lighter pipettes are better ergonomically, electronic pipettes can reduce the variance, and using tips and pipettes from the same manufacturer creates the most accurate system. Remember that choosing the right tip is as important as choosing the right pipette!

Pipette will be accurate when you use correct pipetting technique considering liquid properties, use proper fitting tips, and keep it well maintained and calibrated.

Pipettes transfer liquid using piston system whereas burettes are graduated glass tubes. Pipettes are used when moving known amount of liquid and burettes are often used to determine unknown amounts.

Pipettes are precision measuring instruments designed to reliably and repeatably transfer small amounts of liquid. Well maintained pipettes will last for a long time.

People often use calibration stickers with the last calibration date. Also you should have a calibration certificate with a date stating that the pipette has passed calibration.

Pipettes are used to transfer accurately small amounts of liquid. Disposable pipette tips are used in conjunction with pipettes to hold the liquid.

Pipettes are often calibrated according to ISO 8655-2 in an ISO 17025 accredited calibration laboratory by trained service personnel. The technician tests and adjusts the pipettes, usually in a 3-point calibration (100% - 50% - 10% of nominal volume). Commonly a balance with moisture trap and distilled water are used, along with environmentally controlled room.

There are two main factors, accuracy and precision. Accuracy describes the ability of an instrument to give responses close to the true value. It expresses the difference between the mean volume of actual measurements and the true value. Precision describes the ability to produce closely similar measurements. It tells how close a set of repetitive measurements are to each another. 

1. Plan the pipetting steps, especially with applications where contamination can be an issue.
2. Select a pipette that covers the volume you desire to transfer.
3. Select tips that fit the pipette.
4. Adjust and lock the volume to prevent accidental volume changes.
5. Select technique according to liquid.
6. Operate plunger slowly and smoothly, or with an electronic pipette select correct speed.
7. Remember good ergonomics, to protect yourself from accumulating strain.
8. Store pipettes in stand and make sure they are maintained and calibrated regularly.

Pipettes with air displacement principle have a piston-cylinder -combination which manipulates an air column between the piston and liquid. Pressure changes in air column move the liquid in and out.

According to Oxford dictionary pipette and pipet are synonyms.

Check that the position of the multichannel pipette lower part can be rotated 360 degrees to ensure that pipetting can be performed ergonomically. Make sure that the multichannel pipette provides fast, secure, and simultaneous tip loading for all tips. It should be possible to mount the tips evenly without excessive force. Check also that the tips can be easily ejected.

Professional training is a very good option to improve pipetting skills. Especially when working with viscous, volatile, or liquids with low surface tension proper technique will increase the quality of results significantly. Ask your pipette provider if they offer training courses.


In addition to being able to pipette more accurately and precisely, proper training can save you time and promotes ergonomical working habits. See our training offering at https://www.sartorius.com/en/knowledge/trainings/pipetting-academy

Pipettes can be used with many different techniques, especially the electronic pipettes. Choose the technique according to the liquid you are pipetting. For more infromation ask your pipette provider for training. See our Pipetting Academy offering at https://www.sartorius.com/en/knowledge/trainings/pipetting-academy

1. Winding above or below the marked volume range.
2. Dropping or hitting, or othervice physically damaging pipette.
3. Using tips that do not properly fit to the pipette or that that the pipette is not calibrated for.
4. Using wrong pipetting technique, especially with viscous or volatile liquids.
5. Forgetting to calibrate your pipettes, calibration is the only way to ensure pipette will deliver reliable results.

Pipette Resources

View All Resources

Pipetting Resources

Product Guide

Pipetting Made Simple with the Ultimate Pipette Buyers Guide for 2023

Pipette selection, pipetting techniques and more - it's all right here in our buyers guide. This page is a one-stop shop for everything you need.

Read More
Poster

How to Clean Your Pipette?

Cleaning pipettes can be easy! Download our quick guide on how to clean your pipette.

Read More
application note cover
Application Note

Pipette Calibration and Standards

The most import International Stardardization Organization (ISO) standards related to pipetting are ISO8655 and ISO17025 and these standards set the g...

Read More

Request a Quote, Demo, or More Information

What other areas are you interested in? (select all that apply)

Request More Information

Ready to Buy?