• Homepage
  • Octet® BLI Resource Library
  • Bio-Layer Interferometry as a Strategic Platform to Validate Covalent Proximity Inducing Small Molecules With Synthetic Tumor Immunotherapeutic Applications

Bio-Layer Interferometry as a Strategic Platform to Validate Covalent Proximity Inducing Small Molecules With Synthetic Tumor Immunotherapeutic Applications

On Demand Webinar

Abstract

The host immune "recognition" of cancer forms the basis of modern tumor immmunotherapy, a highly targeted treatment option with the demonstrated ability to "cure" previously lethal blood cancers. Immune recognition is mimimally governed by the proximity of "active" phagocytic and cytotoxic immune cells to the site of target cancer cells. To probe mechanistic aspects of the recognition process, generate useful immunotherapeutic design principles, and design potentially new classes of "reactive" synthetic tumor immunotherapeutics, our lab develops chemical tools that modulate the proximity of host immune cells with cancer cells. One class of these chemical tools we call "covalent immune recruiters" or CIRs, function by binding and forming selective irreversible linkages to tumor antigens highly expressed on the cancer cell surface, and or natural immune machinery e.g. serum antibodies, Fc receptors. In vitro validation of CIR function is thus highly non-trivial as both binding affinities and covalent reaction kinetics must be characterized and differentiated in the context of two different proteins. This seminar focuses on the unique suitability and application of BLI for the characterization of CIR function at the molecular level. We demonstrate BLI can be employed to efficiently characterize CIR binding affinities against both prostate tumor antigen and human serum antibody proteins, and selective covalent recruitment of these antibodies to the tumor antigen. The elucidation of these highly relevant physical parameters via other conventional techniques such as ITC and fluorescent polarization is difficult if not impossible largely due to higher sample concentration and time requirements, in addition to aggregation induced artifacts. Taken together, BLI validation of CIRs can accelerate lead compound advancement to in vivo validation studies with additional utility in characterizing emerging classes of covalent inhibitor drugs and ABPP chemical tools.


Complete the Form to Watch

Presenter

Anthony F. Rullo, Ph.D.

Assistant Professor-Chemical Immunology, Department of Pathology and Molecular Medicine, McMaster Immunology Research Center, Department of Chemistry and Chemical Biology, McMaster University


Learning Objectives:

  • How to design, optimize, and validate a novel trifunctional chemical tool named covalent immune recruiters (CIRs) that can selectively label serum antibodies and direct immune responses to specific target proteins.
  • Use of Octet label-free binding analysis platforms to obtain kinetic information to quantify covalent labeling of antibodies and evaluate selectivity, also providing a 1 step solution to simultaneously monitor target protein binding and antibody recruitment under relevant equilibrium conditions.
  • Validation of CIRs specificity and selectively in vivo conditions

Request a Quote, Demo, or More Information

What other areas are you interested in? (select all that apply)

Please Complete the Form and Watch the Webinar