Pipette Check to Standard DIN with Cubis II
Application Highlight
According to Standard DIN EN ISO 8655-2 volumetric measuring instruments such as piston pipettes must be checked at regular intervals but at least once per year. Shorter time intervals may be specified by the users depending upon the frequency of use, number of users, aggressive nature of the pipetted liquids and the acceptable maximum permissible errors established by the user. In consequence for all laboratories that have to work in compliance to standard DIN EN ISO 8655 the regular check is mandatory.
Explore Cubis® II