Effects of Static Electricity on Analytical Weighing
Application Article
Among the various options for eliminating static electricity during analytical weighing, there are simple, low-cost measures available. However, due to the current metrological and practical limitations, many of these measures are difficult and timeconsuming to use and are not universally applicable. On the other hand, there are methods that are both powerful and spacesaving, particularly when they are integrated directly into the balance.
Learn how these effects can be eliminated with a Cubis®️ II balance.
Explore Cubis® II