White Paper: Balance-Testing for Quality Assurance
Sartorius balance test reports can be used to test balances against previously defined tolerances, both manufacturer and user specified. Compliance with up to four key parameters (repeatability, deviation in case of eccentric loading, adjustment accuracy, linearity) is tested and evaluated.
In this white paper, learn about testing within the defined tolerances, and how test equipment is required to operate within specified tolerance ranges to achieve successful quality assurance. Sartorius offers a variety of tests to ensure all tolerance specifications are met.
Commonly Asked Questions:
- What is the best way to keep your balance functioning properly?
- There are several things to keep in mind when it comes to analytical balances: Handle the equipment properly, keep the balance calibrated according to current guidelines, ensure a proper environment free of contaminants and static electricity and always store the equipment safely and securely when not in use.
- How often should my lab balance be calibrated?
- It is usually recommended a balance be calibrated prior to initial use. After that, calibration frequency depends on factors such as how often the unit is used and the degree of accuracy required for tasks.