Biologics Discovery and Development Resources
Expert insight and knowledge to further the discovery and development of breakthrough therapeutics at your fingertips.
Featured Resources
- How to Work Faster, Smarter, and Pain-Free With Electronic Pipettes
- From Molecule to Market: Simplifying the Characterization of Antibody-Drug Conjugates (ADCs) Webinar
- Characterizing Anti-HER2 Antibodies with Advanced Flow Cytometry & BLI Label-Free Detection
- Accelerating Drug Discovery with High-throughput Biomolecular Interaction Analysis
- Rapid Antibody Discovery Strategies to Support Optimized Next Generation Modalities
- Quantitation and Characterization of mAbs Using Octet® Bio-Layer Interferometry
- Securing the Antibody Supply Chain Through Recombinant Antibody Technology: A COVID-19 Case Study
- Detailed Antibody Characterization Enabled by High Throughput Flow Cytometry
- DNA as Medicine: Encoding Cancer Therapeutic Antibodies
- Body Feed Filtration – the Novel Method for Rapid Harvesting of Mammalian Cell Cultures
- Accelerating Nanobody Discovery Workflows with High-Throughput Flow Cytometry
- High Throughput Antibody Discovery Targeting Glycoproteins for Apoptosis Induction in Cancer
- High-Throughput Antibody Discovery Targeting Cell Surface Receptors for Signaling Blocking in Cancer
- Gain deeper insights into the mechanisms of immune cell killing of tumor cells
- Disrupting the Immunotherapy Field - A Novel Platform for Targeting Chronic Diseases
- Combining Binding and Functional Analyses for Comparison of Anti-TNFα Monoclonal Antibody Biosimilars
- iPSC Pluripotency During Cell Line Selection and Differentiation
- Characterization of Trastuzumab ADC Using Bio-layer Interferometry and Advanced Flow Cytometry
- Characterization of Anti-HER2 Antibodies Using iQue® & Octet® Platforms
- The Essential Role of Cell Culture Techniques and Lab Consumables in Ensuring Cell Health
- Fast and Full-Scale Multipass Membrane Protein-Specific Antibody Optimization Workflow at ImmunoPrecise Antibodies
- A Rapid Method to Quantitatively Screen Bispecific Antibody Using Protein A and His1K Biosensors
- Rapid Mammalian Cell Harvest without Centrifugation for Antibody Purification Using the Sartoclear Dynamics Lab Filtration System
- The Mouse IgG Type and Titer Kit is a single, multiplexed assay that simultaneously quantifies IgG isotype, IgG quantity per isotype, total IgG secretion, cell count and cell health
- From Mammalian Cell Cultures to Pure Proteins: Sartoclear Dynamics® Lab Significantly Reduces Cell Harvest Time
- Minimizing Syringe Filter Usage in harvesting Monoclonal Antibodies from CHO Cell Culture Supernatants
- Vivaflow® 200: A Critical Sample Preparation Tool for Concentrating Hybridoma Supernatants
- Concentration of Mammalian Cell Culture Supernatants with Vivaspin® Turbo 15 and Amicon® Ultra-15 Devices
- Cell Culture Expansion in Fully Closed Erlenmeyer Shake Flasks Outside the Biosafety Cabinet with Mycap® CCX
- Application Highlight: Safe-Lock Tube Holders for Cubis®️ Balances
- Application Highlight: Vial and Flask Holders for Cubis®️ Balances
- The Sterisart® Septum Enables Reliable Sampling from a Closed System Sterility Testing Unit
- Cubis® II in the Context of Therapeutic Antibodies
- Cross-Platform Analysis of the Binding and Function of Anti-HER2 Antibody-Drug Conjugates (ADCs)
- Antibody Internalization: Advanced Flow Cytometry and Live-Cell Analysis Give Rich Insights During Antibody Profiling
- Analytical Power Tools Open Upstream Bioprocessing Bottlenecks
- Advanced Therapeutic Antibody Discovery with Multiplexed Screening
- Reliable Results from Cell-based Bioassays with Leachable-free Sartorius Pipette Tips
- Lab Essentials for Successful Cell Line Development eBook
- Bioanalytical Techniques to Advance Biosimilars Development
- Article Collection: Next-Generation Therapeutic Antibody Discovery
- Development of Next-Generation Antibodies for Therapeutics
- Cell Press Research Arc: New Targets for Cancer Immunotherapy
- Importance of mAb Discovery and Development in Immunotherapy
- Compendium - Accelerated Antibody Discovery
- Overcoming Challenges in High Density Cell Culture Harvesting During Antibody Development
- Neutralizing Antibodies Making Their Mark in Next Wave of Biologics
- Beyond Monoclonal Antibodies: Exploring the Next Generation of Antibody Therapeutics
- Idea-to-Lead: Advances in Discovery & Characterization of Therapeutic Antibodies eBook
- Biologics Molecule Development Workflow
- Supporting The Development of Nanomedicines with Ultrafiltration & BLI
- Challenges and Solutions in Developing Biosimilars
- Role of Neutralizing Antibodies in Viral Infection Research Infographic
- Challenges and Solutions for Developing New Monoclonal Antibodies
- Developing Next Generation Therapeutic Antibodies