Why measure neuronal activity?

The generation and maturation of neuronal networks are necessary characteristics of neurogenesis, providing confirmation that the cellular processes required for proper neuronal function have been developed. Recent advances in human induced pluripotent stem cell (hiPSC)-derived neurons offer promise as a powerful in vitro model strategy for the study of both the basic mechanisms of development as well as complex disorders of the human nervous system. A wide array of research areas, including molecular and developmental neuroscience, drug development and neurotoxicology, employ hiPSC-derived cell models to gain functional insight into relevant neuronal networks and disease states. However, characterization and optimization of these models as they differentiate, mature, and become functionally active are limited by current techniques.

Traditional techniques for measuring activity often:

  • derive measurement of activity from a limited number of cells, lacking context of a true network
  • cannot confirm cell morphology, spatial resolution, or evaluate functional connectivity
  • analyze a single endpoint rather than repeated, kinetic evaluation throughout the duration of neuronal maturation
  • increase the chance of damaging sensitive cells or altering neuronal function as they require transferring culture plates from incubator to instrument  for analysis
  • do not incorporate physiologically relevant environmental conditions, further limiting longitudinal studies

The Incucyte® Neuronal Activity Assay is an end-to-end solution consisting of instrumentation, software, and reagent that enables unprecedented access to complex, neuronal activity measurements enabling functional insight into neuronal cell models. A new era of discovery awaits....

Application

Introducing Incucyte® Neuronal Activity Assay

Determine if your neurons are active, when they become active, and how their activity changes over time

Gain insight into the activity and connectivity of neuronal networks with continuous imaging and analysis. The Incucyte® Neuronal Activity Assay allows for direct, long-term measurements of synaptic activity for the characterization of neuronal cell models in physiologically relevant conditions. Visualize and analyze spontaneous neuronal activity for weeks or months with the Incucyte Live-Cell Analysis System, Incucyte Neuronal Activity Analysis Software, and Incucyte Neuroburst Orange Lentivirus.

Key Advantages

Key Advantages of Incucyte® Neuronal Activity Assay

  • Novel, Non-perturbing Reagent - Express a genetically-encoded fluorescent calcium sensor using Incucyte® Neuroburst Orange Lentivirus in a variety of neuronal cell types
  • Analyze Thousands of Cells - Automatically capture and analyze short-term, calcium-flux kinetics from thousands of cells while qualitatively monitoring cell morphology
  • Conduct Chronic Studies of Activity - Quantify longitudinal changes for every active object within every well of a 96-well plate while cells sit undisturbed inside your incubator
  • Built for Every Scientist - Gain unprecedented access to phenotypic information using a lab-tested live-cell reagent, established protocol and purpose-built software – enabling even first time users

Request More Information

Novel, Non-perturbing Reagent

Express Incucyte® Neuroburst Orange Lentivirus in a variety of neuronal cell types, including iPSC-derived models, to gain insight into the dynamic changes in activity via measurements of calcium oscillations.

Figure 1. Efficient, non-perturbing labeling of living cells enables chronic, long-term neuronal activity analysis during network development. CNS.4U iPSC-derived neurons (Ncardia) seeded at 20,000 cells/well in a 96-well microplate were infected with Incucyte® Neuroburst Orange Reagent to monitor neuronal activity over time. Movies (3 minute duration) captured on Day 15 and day 44 reveal spontaneous development of neuronal activity (calcium oscillations) while phase images enable qualitative inspection of cell morphology. Movies were taken for 3 minutes every 24 hours over the course of 45 days, reveal maintained expression of Incucyte® Neuroburst Orange Reagent. Quantification of the orange fluorescent signal kinetics shows an increase in active object count over the course of the experiment along with a corresponding increase in mean correlation (connectivity) at later time points, signifying development of a functional, mature network.


Analyze Thousands of Cells

Automatically capture and analyze short-term, calcium-flux kinetics for every active cell within each well of a 96-well plate using Incucyte® Stare Mode Movie acquisition. Easily generate correlation metrics to reveal the extent of connections in a network.

Figure 2. Analyze calcium dynamics for every active neuron in a 96-well plate. Incucyte® rCortical Neurons primary neurons seeded at 15,000 cells/well in a co-culture model with Incucyte® rAstrocytes were subsequently infected with the Incucyte® Neuroburst Orange Lentivirus. Vessel View (A) displays a summary of active objects (range image) in each well of a 96-well plate acquired during movie acquisition on day 8, revealing differences in activity across the microplate. Identification of each active object via masking (shown in purple) of the range image (B) is performed using the integrated Incucyte® Neuronal Activity Analysis Software Module. 96-well Summary Traces for movies acquired at a given timepoint (C) provide a full 96-well view of burst intensity, active object count (left inset value) and mean correlation (right inset value).


Conduct Chronic Studies of Activity

Quantify longitudinal changes of activity for the characterization of neuronal cell models in physiologically relevant conditions

Figure 3. Identify changes in activity patterns over weeks or months to characterize neuronal cell models. iCell GlutaNeurons (Cellular Dynamics International) were seeded at 30K cells/well with a co-culture of rat astrocytes (15K cells/well) on PEI/laminin coated 96-well culture plates. Neurons were transduced with Incucyte® Neuroburst Orange Lentivirus at DIV 2, and spontaneous neuronal activity was analyzed over a period of 20 days. Kinetic quantification (center graph) of longitudinal, dynamic changes in neuronal activity of mean burst rate and mean correlation over time shows that during neuronal network maturation, an increase in burst rate occurs, peaking at day 5. Time course data also shows an increase in neuronal synaptic connections, as noted in an increase in correlation. Active object traces (corner traces) provide detailed insight into the dynamic changes in neuronal activity and connectivity for every acquired movie and are qualitatively confirmed with movie viewing tools.


Built for Every Scientist

Enable scientific discovery with an end-to-end solution – reagent, protocol, purpose-built acquisition and analysis software

Figure 4. Make the complex simple. Combine the power of automated acquisition and analysis with our novel reagent and lab-tested protocol to gain unprecedented access to phenotypic information. Guided interface enables rapid experimental set up and analysis, making data and images readily accessible for the entire research team.


Request More Information

Neuronal Activity Assay Testimonials

Michael Uhler, PhDb | Professor, Biological Chemistry
Research Professor, Molecular and Behavioral Neuroscience Institute, University of Michigan

“The Incucyte Neuronal Activity Assay is particularly useful in comparing the network activity of neuronal cultures from different genotypes and we have found it indispensable for optimizing culture conditions for the generation of mature neurons from human stem cells.”

Krishna Vadodaria, PhD | Research Associate
Rusty Gage Lab, Salk Institute

“The Incucyte Neuronal Activity Assay allows for testing multiple culture conditions across multiple neuronal lines.  The assay let us assess the impact of co-culture between different cell types, multiplexed with different treatment conditions at a semi high-throughput scale in a manner previously not possible."

Louis Dang, MD, PhD | Clinical Lecturer
Jack Parent Lab, University of Michigan

“The Incucyte Neuronal Activity Assay allowed me to perform a longitudinal analysis of calcium transients in stem cell-derived neurons. The 96-well plate format allows multiple concurrent comparisons from different cell lines and growth conditions. The burst rate, burst duration, and network formation was highly reproducible with minimal well-to-well variability. The ability to concurrently view cell morphology with phase contrast was highly advantageous to eliminate outliers.”

Ordering Information

Ordering Information

Product

Qty.

Cat. No.

Incucyte® SX5 Live-Cell Analysis System

1 instrument

4816

Incucyte® Neuronal Activity Analysis Software Module

1 Module

9600-0032

Incucyte® Neuroburst Orange Lentivirus

2 mL

4736

Incucyte® Neuroactive Orange Kit

1 Kit

4761


Request a Quote

Resources

Literature and Documentation

Brochure

Incucyte® Reagents, Consumables and Software

Download Now

Incucyte® Neuroburst Orange Lentivirus

For Detection of Neuronal Activity in Live Cells

Download Now
icon-article

Application Note

Long-Term Live Cell Visualization and Quantification of Neuronal Activity

Download Now
icon-article

One-Sheet

Incucyte® Neuronal Activity Assay

Download Now
icon-article

Protocol

Incucyte® Neuroburst Orange Lentivirus

Download Now
icon-download

Poster: SFN 2017

Long-term live cell visualization and quantification of spontaneous neuronal activity and pharmacological response from human induced pluripotent stem...

Download Now

Request a Quote, Demo, or More Information

What other areas are you interested in? (select all that apply)

Request a Demo, Literature, or More Information