Sartocheck® – The Multiunit Concept
Increasing Production Efficiency by Parallel Testing
- The Multiunit consists of the pneumatic components (Test Unit) and the software algorithms to perform an integrity test
- Up to 4 Mulitunits can be connected to one Sartocheck® 4 via a RS 485 interface
- Real time saving - up to 5 tests in parallel
- All kinds of test combinations possible for highest flexibility
- Integrity test to be performed is selected and started via the Sartocheck® 4 user interface
- Sartocheck® 4 generates the test printout and stores the test result in his data base
- Almost no relevant distance limitations between units (100 m)